SEL Time-Domain Link (TiDL) Process Bus Solutions

SEL TiDL technology enables robust process bus solutions using time-deterministic data exchange and simplified configuration.

Elements of a TiDL-Based Process Bus System

Merging Units

SEL-TMU TiDL Merging Units are installed close to primary equipment, such as within breaker control cabinets, to perform A/D signal conversion. They transmit digitized current and voltage measurements as well as breaker status and other binary signals using SEL T-Protocol over fiber-optic cable to TiDL-enabled relays. Each SEL-TMU supports direct fiber-optic connections to as many as four TiDL-enabled relays with no need for Ethernet networking.

Protective Relays

Relays perform protective functions and other control actions based on the T-Protocol data streams from connected SEL-TMU devices as well as direct communications from other devices. They send communications-assisted protection signals, interlock signals, and control signals to SEL-TMU units via T-Protocol messages.Each SEL TiDL-enabled relay has eight 100BASE-FX fiber-optic ports for acquiring digitized analog and binary data from SEL-TMU units to perform protective functions and other control actions. If a fault is detected, relays send a trip signal to the merging unit using the SEL T-Protocol over fiber-optic cable.

Communications

SEL TiDL merging units and TiDL-enabled relays communicate using the SEL T-Protocol, which maintains data synchronization among all connected merging units. The SEL T-Protocol combines several communication functions, which streamlines message encoding, transport, and decoding tasks and simplifies process bus configuration.SEL TiDL-enabled relays communicate with other devices using common protocols, such as GOOSE, Mirrored Bits communications, synchrophasors, and SEL-2600 RTD Module communications.

Time Synchronization

TiDL relays measure the path delay between the relay and the merging unit on each connected port to align current and voltage measurements acquired from different merging units. This aligning procedure eliminates the need for external time sources, such as GPS clocks, for data synchronization.TiDL relays can be time-synchronized with other devices in station bus networks via the Precision Time Protocol (PTP) or IRIG-B.

Ancillary Data

A TiDL system often needs to collect more than current and voltage measurements and binary statuses to perform protection actions. Many SEL protection, control, and monitoring devices collect and digitize ancillary data, such as temperature, alarms, control actions, and more, to supplement the protection data digitized by merging units. SEL offers devices that support traditional CT/PT, Rogowski coil, and digital message inputs and connect to a wide variety of protection, control, and monitoring sensors.

Design Considerations for TiDL Solutions

In addition to its protective functions, there are other important factors that must be considered when designing and implementing a process bus system.

Interoperability

Device protocols allow communication between digital devices and between process bus and station bus networks. Communications between SEL-TMU units and TiDL-enabled relays use the SEL T-Protocol exclusively.SEL TiDL-enabled relays also communicate with non-TiDL relays and other devices using common protocols. This capability allows substations to integrate process bus systems with a variety of station bus protocols, such as DNP3, FTP, Telnet, HTTP, IEC 61850 MMS and GOOSE, IEC 61158 EtherCAT, synchrophasors, Mirrored Bits communications, and SEL-2600 communications. (EtherCAT® is a registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany.)

Cybersecurity

Cybersecurity is a vital consideration in process bus systems. However, because operational technology (OT) and IT systems have different purposes, the cybersecurity solutions for one system may not be the most appropriate for another.

Preserve Availability with Privacy Methods

TiDL-based process bus solutions use privacy methods to preserve the availability of data and restrict access.Direct connections provide privacy by physically isolating communications paths. Private links between devices enable immediate detection of intentional or unintentional disturbances to data flows, so that devices issue alarms and perform automatic corrective action to maintain security.TiDL communications are inherently private through direct, point-to-point connections between SEL-TMU units and TiDL-enabled relays. Physically isolated communications paths prevent the capture or misdirection of SEL T-Protocol messages without detection. The T-Protocol cannot be encoded or decoded by conventional protocol analyzers to perform malicious or accidental insertion of simulated messages.

Secrecy Methods Reduce Availability

Network connections that are not engineered to maintain privacy often require coordinated secrecy methods like TLS within each device to obscure data, generally by encryption, making them unreadable to other devices and unauthorized users. This solution is undesirable in secondary systems because the additional processing load and time required to encrypt and decrypt data can slow protective action. Encryption also makes data unavailable to engineers, technicians, other devices, and systems that lack the appropriate decryption capabilities. In addition, the increased frequency of firmware updates required to stay current with secrecy technologies poses a serious obstacle for maintaining system availability, requires that devices be updated simultaneously, and introduces new supply chain and personnel vulnerabilities. Unintended consequences that affect protection reliability include device down time during firmware upgrades to address security vulnerabilities and a lack of communications among devices until they are all upgraded to the same firmware version. From our knowledge base:

Engineering Services

As part of a digital secondary system implementation, TiDL-based process bus systems are as simple or sophisticated as an application demands, but many important factors must be considered in designing the system. Partner with SEL Engineering Services to create a turnkey solution that addresses the needs of your system and puts you in control. Our expert engineers provide thorough training in all products applied in a solution, ensuring that you can achieve your operational goals once a system is in place.

Our Support

We’ve collaborated closely with our customers since the company was founded nearly 40 years ago—a major reason why we’re North America’s most trusted provider of protective relays and ranked #1 by international utilities in price, service, and support.
SEL devices are designed for a working life of at least 20 years, and every SEL-manufactured device comes with a ten-year warranty—the best in the electric power industry. If it fails under warranty, repair and replacement are free.We always do all that we can to repair any returned product, whether it meets our warranty or not.

Rugged and Reliable—Guaranteed

SEL products are designed and manufactured for the world’s most challenging environments, exceeding all industry standards for temperature, shock, and electric stress. An optional conformal coating for circuit boards adds an extra level of protection against contaminants in extreme environments.Our products have a mean time between failures (MTBF) of more than 700 years, based on observed field performance. This means that if you have 700 SEL products installed in your systems, you can expect to have less than one fail per year for any reason, whether it’s a defect or an external factor such as overvoltage, overcurrent, wildlife damage, or environmental exposure.
Every device we manufacture comes with free lifetime technical support.SEL support teams are stationed in regional offices around the world and staffed with application engineers who are experts in our products and in power system applications.No matter how often you need to call or how long your SEL products have been in service, our customer service and technical support professionals are ready to help. 

Security Bulletins and Updates

We notify product owners of updates and security patches for the full life of the product. Software and firmware updates are distributed directly to our customers via secure file transfer, and their authenticity and integrity are verifiable through digital signatures and cryptographic hashes.More About Security Notifications
SEL offers complete cybersecurity support for every solution, system, and product we provide.We also practice secure supply chain management and help our customers comply with applicable supply chain and cybersecurity standards.

Security Bulletins and Updates

We thoroughly review and test the code in our products, which allows us greater control over their quality, security, and functionality. Customers are notified of updates and security patches for the full life of every SEL product.

Cybersecurity Services and Support

From system assessment and baselining to cyber-defense solution development and ongoing system management, our full suite of security services can help strengthen your defenses and streamline the demands of maintenance and compliance.Cyber services support contracts can include incident response, audits, system hardening, patch/update management, and more, depending on your anticipated needs.Contact SEL Cyber Services
SEL meets your workforce training and continuing-education needs through seminars, conference and tradeshow presentations, and SEL University courses.SEL University courses and many of our seminars provide Professional Development Hours (PDHs) for maintaining Professional Engineering (P.E.) licenses. Courses and seminars can be delivered in various formats, including self-paced online learning, virtual classrooms, live and recorded webinars, and in person.We can also work with you to develop training that is customized to the specific needs of your workforce.

Training and Education offerings

Questions? Contact Us!

If you have any questions about SEL products, services, solutions, or support, please contact us. Our service and support professionals are ready to provide the answers you need.

Unbeatable Support

SEL support teams are stationed in regional offices around the world and staffed with application engineers who are experts in our products and in power system applications.

Technical support for SEL-manufactured devices is always complimentary. No matter how often you need to call or how long your SEL products have been in service, you’ll reach an SEL expert who can provide the service and support you need.

Our cybersecurity team is always ready with the information and resources needed to keep your OT networks and critical systems secure and working effectively. Cyber services support contracts can include incident response, audits, system hardening, and more, depending on your anticipated needs.

More about SEL warranty and support