Productos
Soluciones
Servicios de ingeniería
Educación
Soporte
Empresa
Iniciar sesión
SEL-2240
Presentación
Documentos
Soporte
SEL-2240
Toggle Dropdown
Presentación
Documentos
Soporte
Documentos
Destacados
Manual de instrucciones
SEL-2240 Axion and
acSELerator
RTAC SEL-5033 Software
Hoja de datos
SEL-2240 Axion
Folleto
Axion SEL-2240 Controlador de automatización en tiempo real modular
Folleto
SEL Axion Bay Controller
Hoja de datos
SEL-2240 Axion Bay Controller
Literatura
Los documentos más nuevos se muestran primero.
Incluir la literatura en inglés
Literatura
Folletos
Axion SEL-2240 Controlador de automatización en tiempo real modular
Inglés
Capture Every Disturbance With Continuous Waveform Recording
Hojas de datos
Inglés
SEL-2241-2 Data Sheet
SEL-2240 Axion
SEL-2240 Axion Bay Controller
SEL-2242 Chassis/Backplane
SEL-2244 Digital I/O Module
SEL-2245-2 Analog Input Module
SEL-2245-4 AC Metering Module
SEL-2245-411 Standard Current and Low-Voltage (LEA) Monitoring Module
SEL-2245-42 AC Protection Module
SEL-2241 Real-Time Automation Controller (RTAC)
SEL-2243 Power Coupler
SEL-2245-22 Analog Input Extended Range Module
SEL-2245-221 Low-Voltage Monitoring Module
SEL-2245-3 Analog Output Module
Manuales de instrucción
Inglés
SEL-2240 Axion and
acSELerator
RTAC SEL-5033 Software
Información para ordenar
Inglés
SEL-2242 I/O Chassis/Backplane for the SEL-2240 Axion System
SEL-2245-221 Low-Voltage (LEA) Monitoring Module
SEL-2245-411 Standard Current and Low-Voltage (LEA) Monitoring Module
SEL-2243 Power Coupler for the SEL-2240 Axion System
SEL-2245-22 DC Analog Input Extended Range Module For the SEL-2240 Axion System
SEL-2245-42 AC Protection Module
SEL-2245-4 AC Analog Input Module for the SEL-2240 Axion System
SEL-2244-2 Digital Input Module
SEL-2244-3 Digital Output Module
SEL-2244-5 Fast High-Current Digital Output Module
SEL-2245-2 DC Analog Input Module for the SEL-2240 Axion System
SEL-2245-3 DC Analog Output Module for the SEL-2240 Axion System
SEL-WA2244 DIN Rail Adapter and Wiring Harness
Certificaciones
Inglés
Destacados
RTAC Axion IEC 61850 Edition 2 Certificate
Notas técnicas de firmware
Inglés
RTAC R155-R201 Technical Note
RTAC R154-R200 Technical Note
RTAC R153 Technical Note
RTAC R152 Technical Note
RTAC R151 Technical Note
Publicaciones
Guías de aplicación
Inglés
Deploying Custom Alarm Screens in an SEL-2240 Axion Bay Controller
View Streamed Axion Wave Server Time-Series Data in Synchrowave Monitoring and Calculate Energy Packets in RTAC Logic Engine
Related Material
XML Files
Modbus Configuration for SEL-700 Series Relays and RTAC Devices
Creating a Warning Screen in Bay Screen Builder for the SEL-700 Series Relays
Managing IED Passwords With the SEL-3620 Ethernet Security Gateway and SEL RTAC Using SEL Server Connections
Understanding and Using Functions and Function Blocks in the RTAC
Configuring the SEL RTAC to Exchange Data With SEL IEDs Over IEC 61850 GOOSE
RTAC–IEC 61850 MMS Client-Server
Using SEL Fast Message Protocol Between the SEL-3530 RTAC and the SEL-2032
Configure the RTAC to Obtain Temperature Measurements From SEL Relays Via Flex Parse Messaging
Detecting a Loss of Communication Between an RTAC and a Relay
Configuring the SEL-3530 RTAC to Obtain Temperature Measured Using the SEL-2600
Using Shared Tags to Optimize an RTAC HMI
Related Material
Demo Shared Tags
Defining DCE and DTE: Null Modem Cable and Straight-Through Cable Applications
Converting SEL-651R Event Type ASCII Character Strings to DNP3 Analog Inputs in the RTAC
Tiered Communication Between Remote Locations Using Multiple SEL-3530 RTACs
Automating Common RTAC Maintenance Tasks Using Python Scripts and SEL Software
Related Material
Python Scripts-AG2020-08
Using the DateTime Triggers Extension to Simplify Time-Based Triggering of Standard IEC 61131-3 Logic in the SEL RTAC
Related Material
DateTime Triggers extension
Using Wireshark to Troubleshoot Protocol Communications Issues on an RTAC
Using an RTAC to Get Three-Phase Fault Currents From SEL-400 Series Relays
Understanding and Effectively Using the SEL
Mirrored Bits
Protocol
Event Collection From SEL-3530 RTAC Using Team
SEL RTAC Axion Batch Sequencing With HMI for Industrial Automation Using Ladder Logic
SEL-2240 Axion Retrofit Cables for GE D20
Implement Serial DF1 Client Protocol in an RTAC By Using an
acSELerator
RTAC Extension
Related Material
DF1 Client
Configuring the SEL RTAC as a Single Source for Substation Event Data: Job Done Examples of Various Methods for Collecting and Retrieving Digital and Oscillographic Records
Using an RTAC to Monitor Network Status With SNMP
RTAC Commissioning Assistant
Related Material
Commissioning_Assistant
Commissioning Assistant
Maximizing RTAC Performance
Integrating Fast Controls With SCADA Operations in the RTAC
How to Fix the HTTPS Untrusted Server Error on an SEL Web-Enabled Device
Related Material
Make A Cert
Sample Console Session
Proportional Integral Derivative Controller Tuning for the Real-Time Automation Controller (RTAC) Platform
Convert SEL Fast Message Synchrophasor Messages to IEEE C37.118 Using the RTAC
Using Wireshark to Decode RTAC Serial Line Messages and SEL Protocols
Managing Time in the RTAC
Setting Up an RTAC HMI for an SEL-700 Series Relay Using Various Protocols
Using an RTAC to Read and Write Analog Data Values to an SEL-2411 Using SEL Fast Message Protocol
Basic and Advanced Applications of the SEL-3530 RTAC Access Point Router
Using an RTAC to Automatically Manage the Date and Time in Legacy Relays
Notas de aplicación
Capture datos vitales de la subestación utilizando el sistema de registro digital de fallas (DFR) de SEL
SEL-3530 - Lógicas para pruebas en campo
SEL-3530 - Como programar pulsos en la tarjeta de salidas digitales
Inglés
Wiring SEL-2400, SEL-2200, and SEL-700 Series Devices
IEC 61131-3 Variable Usage and Initialization in the RTAC
Overcome Wetting Voltage and Current Limitations With an External Wetting Power Supply
Interface HMI Touchscreens to SEL Devices Using Modbus Protocols
Using Network Global Variable List Communications in Decentralized Control Solutions
Using the RTAC as a Modern Serial Data Line Analyzer
Open Channel Flow Control Using the SEL-2411, SEL-3031, and RTAC
Distributed Data Acquisition Using the SEL-2411 PAC and SEL-2440 DPAC
Power Plant - Steam Control
Adding Radio Pilot Channels and Backing Up SCADA Communications
Use Synchrophasors in SCADA/EMS
Control Rotary Assembly Table Systems With SEL Automation Products
Casos de estudio
Inglés
Improving System Performance Using SEL’s Distribution Network Automation (DNA)
Artículos técnicos
Inglés
Locating Faults by Using Incremental Quantities: Introduction, Application Considerations, and Performance
Megahertz-Sampled Observations of AC Level 2 Onboard Electric Vehicle Charging
Ushering in a New Era of Power Management for a Centenarian Oil Field
Hardware-in-the-Loop Simulation, Control, and Validation of Battery Inverter Characteristics Through the IBR Control Hardware
Wind Farm Volt/VAR Control Using a Real-Time Automation Controller
Diagramas