This paper describes the Chess Master project, sponsored by the U.S. Department of Energy, which will apply software-defined networking to advance energy sector network cybersecurity.
This white paper addresses the two main reliability concerns in NAND flash storage, what type of NAND flash memory is best suited for embedded computer systems, and how to optimize computer systems for maximum reliability of NAND flash storage.
The falling conductor protection (FCP) application developed by Schweitzer Engineering Laboratories, Inc. (SEL) depends upon reliable, low-latency broadband communications to de-energize broken distribution power line as they fall, eliminating the risk of wildfire caused by arcing of live wires on the ground. This paper describes the test bed operation of the FCP application enabled by a private Long-Term Evolution (LTE) network usin Anterix’s 900 MHz band spectrum. It reports that, in a range of network congestion and signal strength scenarios, the 900 MHz private LTE network successfully supports the FCP application to de-energize the affecte circuit section within one second. This is less than the time it takes for a broken conductor to fall to the ground, typically a distance of 25 feet.
The goal of this paper is to provide insight and guidance on what is involved in a network migration so the appropriate balance between risk and cost can be found. This discussion focuses on upgrading to an operational technology (OT) software-defined networking (SDN) solution. The paper addresses the challenges of this upgrade process and explores what must be considered and done along the way to make the upgrade as successful as possible.
This white paper describes the application of Schweitzer Engineering Laboratories dynamic disturbance and fault clearing technology associated with a utility’s nuclear plants and how they benefitted from the SEL solution on costs, convenience, and reliability.
This white paper provides a comprehensive review of distribution protection technologies available today for wildfire mitigation. The solutions outlined in this paper focus on enhanced system protection and system hardening, and they are designed to minimize risk in the areas most susceptible to wildfire ignition.
This white paper provides both theoretical and real-world examples with questions and solutions that can be used to gain experience with symmetrical components.
This paper discusses how the SEL-735 Power Quality and Revenue Meter exceeds the nonsinusoidal test requirements for ANSI 0.1 accuracy class compliance. It also illustrates why the SEL-735 is highly qualified for revenue metering applications in today’s challenging power system conditions.
This paper describes the function of capacitor banks in the distribution system and describes common methods for controlling capacitor banks, including their benefits and challenges. It also introduces a new method for controlling capacitor banks by using wireless current sensors in place of traditional line post sensors.
This paper describes how SEL software-defined networking (SDN) can significantly reduce the time and effort required to collect data and provide evidence for CIP-007-6 R1.1 and CIP-010-2 R1.1.4 compliance. It also describes how SEL SDN can assist with meeting NERC CIP-005-5 R1.1–3 requirements [3].
This paper explores how touchscreen technology has evolved, compares popular touchscreen technologies, and discusses common misconceptions about touchscreen technology for power system applications.
Improving how your power system is monitored and controlled can provide operational and maintenance benefits greater than the initial capital investment. This paper examines the financial and non-monetary benefits provided by relay replacement programs.
This white paper examines the benefits of using software-defined networking (SDN) technology
to easily interconnect and manage traffic on OT Ethernet networks that communicate using
IEC 61850 technology. A case study from the Itaipu Dam in South America, one of the world’s
largest hydroelectric facilities, is used to illustrate these benefits.
This document explains the functionality of the SEL Underground AutoRANGER Fault Indicator (AR-URD). It defines the AR-URD AutoRANGER trip logic, principles of operation, fault indication options, inrush restraint, and testing and reset functions.
This paper provides an overview of single event upsets (SEUs), including their causes, mitigation methods, and effects on SEL relays. It quantifies the impact that SEUs have on system protection and provides best practices for ensuring reliability.
This paper explores the implementation of PTP on various Ethernet architectures, including enhancements to provide PTP redundancy. In addition, the paper provides reasons to use PTP clocks and recommendations on the types of PTP clocks to select.
By using a defense-in-depth approach, you can provide read-only SCADA data and Syslog messages to corporate or other networks. The layered defense includes adding a perimeter network, read-only HMI and Syslog server, and a one-way data sending mechanism through SDN and unidirectional firewall rules.
This paper discusses the benefits of applying the new SEL-FT50/SEL-FR12 Fault Transmitter and Receiver System to enhance distribution system protection.
The principles of software-defined networking (SDN) offer significant benefits for operational technology (OT) networking by addressing the limitations of traditional Ethernet. Read more in this white paper.
This white paper describes the early days of programmable logic controllers (PLCs), the introduction of Modbus protocol, and some of the challenges involved today with device interoperability, specifically challenges related to register addressing and data type formatting.
This white paper describes how to use the SEL Real-Time Automation Controller (RTAC) to build an automated system to continuously monitor and validate many of the components identified in the NERC PRC-005 standard.
This white paper discusses SEL Real-Time Automation Controller (RTAC) security concepts and provides configuration examples to empower engineers, technicians, and security personnel to protect critical cyberassets.
This white paper addresses the design considerations for modifying transformer protection at an existing nuclear station and the SEL equipment that can be used to implement that design.
This paper provides recommendations for testing SEL relays and guidance for developing a test program that is compliant with NERC PRC-005-2.
This document defines AutoRANGER® trip logic, inrush restraint (IR), installation considerations, fault indication modes, principles of operation, battery conservation, and test/reset methods.
Event reports continue to be an invaluable feature in microprocessor-based relays. Some events are relatively straightforward to analyze, and others require experience and considerable knowledge of the power system and protective relay system in order to find root cause. This session provides several advanced real-world event examples, time to evaluate them, and solutions.
Event reports continue to be an invaluable feature in microprocessor-based relays. Some events are relatively straightforward to analyze, and others require experience and considerable knowledge of the power system and protective relay system in order to find root cause. This session provides several advanced real-world event examples, time to evaluate them, and solutions.
This white paper provides both theoretical and real-world examples with questions that can be used to gain experience with symmetrical components. The full solutions to these questions can be found in the white paper "Tutorial on Symmetrical Components, Part 2: Solutions."
Event reports have been an invaluable feature in microprocessor-based relays since the initial introduction of the technology. The days of unknown root cause for an operation, lengthy outages, or unexplained test results are largely over due to this tool and the ability of engineers and technicians to use it. We must practice to become proficient at analyzing event reports. This session provides real-world event examples, time to evaluate them, and solutions.
Event reports have been an invaluable feature in microprocessor-based relays since the initial introduction of the technology. The days of unknown root cause for an operation, lengthy outages, or unexplained test results are largely over due to this tool and the ability of engineers and technicians to use it. We must practice to become proficient at analyzing event reports. This session provides real-world event examples, time to evaluate them, and solutions.
The SEL-3530, SEL-3530-4, and SEL-2241 Real-Time Automation Controllers (RTACs) are ultrarugged remote terminal unit (RTU) and programmable logic controller (PLC) systems. An RTAC can operate as the controller for the SEL-2240 Axion, which is a modular I/O system where up to 60 modules can connect to a high-speed, deterministic EtherCAT network. We performed processing analysis and testing to determine the performance of the RTAC with the Axion I/O system. This paper summarizes these tests results and provides recommendations to determine an optimal processing cycle time for any particular application.
This white paper addresses another method of increasing the reliability of substation computers designing them to use error-correcting code (ECC) memory. The use of ECC memory minimizes the specific memory error class of single bit flips. Almost all server-class computers use ECC memory, but very few substation computers use ECC memory.
A minimal synchrophasor system consists of phasor measurement units (PMUs) and integrates the collected data into centralized operator displays. This approach, while providing an immediate benefit over existing supervisory control and data acquisition (SCADA) systems, misses many opportunities for additional power system improvements.
This white paper discusses how the versatile SEL-2505 Remote I/O Module can move contact information and control and monitor remote equipment safely, reliably, and economically.
This paper shows that the specific considerations of using ISM band spread-spectrum radio impact the protection scheme and give Mirrored Bits® communications a significant advantage over IEC 61850 GOOSE messages.
In this paper, the basic concepts of reliability are investigated, and the reliable use of two SEL devices as primary and backup protective relays is promoted.
This paper reviews ground fault protection and detection methods for distribution systems.
The SEL-421 has the unique ability to provide both line protection and Synchrophasor measurement. A frequent question is: how does this dual functionality affect relay performance?
Several people asked SEL what this supposed breach of the algorithm means to users of the SEL-3021 Serial Encrypting Transceiver. The short answer is that the reported SHA-1 compromise does not impact the SEL-3021.
The Facilities Department at Schweitzer Engineering Laboratories, Inc. (SEL) oversees and maintains the power system for seven buildings totaling over 250,000 square feet. This facility in Pullman, Washington, is the world headquarters of SEL. As a result of the company’s growing need for power, the Facilities and Property Manager initiated an investigation of the power system for the Manufacturing building.
Multifunction protective relays include comprehensive monitoring capabilities that can detect the alert and emergency states, minimize system disturbance and prevent system collapse.
As part of our overall mission to make electric power safer, more reliable, and more economical, SEL develops and provides innovative, simple to use, robust technologies to protect, automate, control, monitor, and analyze power systems. An essential element of this strategy is the development of appropriate communications technologies and protocols.
Communications processors, RTUs, and PLCs are used as integration and automation controllers around the world. In order to appreciate the differences, it is appropriate to consider all aspects of integration and automation needs within the power system.
Case study and description of Commonwealth Edison Jefferson 138 kV/69 kV substation instrumentation and control design using SEL protection, control, automation and communications products and technology to provide substation SCADA, monitoring, and automation.
This paper describes a solution for the “last foot” problem, which is a well-known cybersecurity vulnerability
that worldwide electric distribution system owners and operators often confront and ask manufacturers to
mitigate via a cryptographic solution. Here the authors investigate the central concept of the “last foot”
problem, examine the trade-offs and requirements for selecting the best approach to solving that problem, and
introduce a long-lived solution in the form of IEEE 802.1AE Media Access Control Security (MACsec) and the
MACsec Key Agreement (MKA) portion of 802.1X Port-Based Network Access Control.