The SEL-3354 requires device drivers and software to be installed on the operating system in order for the devices, such as Ethernet, video, and audio devices, and the system Watchdog to function. Products shipped from the factory with an operating system installed already include all necessary drivers and software. Use the downloads below when installing your own operating system or to update existing software and drivers on your SEL-3354.
This package contains all SEL-3354 device drivers and software. Windows XP, 7, and Server 2008R2 are fully supported, and some versions of Linux are also supported. Contact SEL if you have questions about support for a specific operating system.
This package contains the installation files for the SEL-3354 IRIG Driver.
These updates provide enhancements, bug fixes, and security updates to the firmware embedded in the SEL-3354 system. Please see the instruction manual Appendix A for release notes.
This file updates the SEL-3354 firmware to the latest release for use with Microsoft Windows operating systems.
This file updates the SEL-3354 firmware to the latest release for use with Linux operating systems.
This package configures the rear ethernet ports to enable Intel Advanced Network Services (ANS) functionality, such as Teaming. This is only applicable to systems manufactured after May 2011 (serial number 1111350000 and higher). See the included readme.txt file for more information.
This package configures the rear ethernet ports to force 100 Mbps full-duplex operation. This should be applied to systems that have fiber-optic rear Ethernet ports or when connected to network devices that do not support autonegotiation of speed and duplex.
This package configures the rear ethernet ports to force 100 Mbps full-duplex operation. This should be applied to systems that have fiber-optic rear Ethernet ports or when connected to network devices that do not support autonegotiation of speed and duplex.
Contains updates and modifications to the operating system environment. Please install any missing updates in the order in which they were released and carefully follow instructions if included with the update you download.
Updates all Windows Embedded Standard SEL-3354 with Microsoft's Remote Desktop Security Update KB4500331 (CVE-2019-0708)
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Security Update 2018). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2018 through January 2019.
Microsoft announced on January 8, 2019, that it discontinued support for the Windows Embedded Standard operating system. This is the final Microsoft Windows Security Update for the SEL-3354. To receive future security updates, customers must upgrade to a newer operating system.
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2017). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from June 2017 through December 2017.
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2017). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2016 through June 2017 and includes the MS17-010 (KB4012598) Security Update previously released for the SEL-3354.
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2016). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from June 2016 through December 2016.
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2016). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2016 through June 2016.
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2015). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from July 2015 through December 2015.
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2015). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2015 through June 2015. This update also includes a security update from Adobe.
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2014). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from May 2014 through December 2014. This update also includes security updates for Adobe Reader and Silverlight.
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2014). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from October 2013 through May 2014. This update also includes security updates for Adobe Reader and Silverlight.
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2013). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from May 2013 through October 2013. We have also included relevant Security Updates from Adobe® Systems Incorporated.
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable executable covering primarily July 2012 through May 2013. This update also includes security updates for Adobe Reader and Silverlight.
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable executable covering primarily November 2011 through June 2012. This update includes security updates for a few non-Operating System supporting software such as Adobe Reader and Silverlight.
Updates all Windows Embedded Standard SEL-3354 with KB2621440.
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable executable covering primarily May 2011 through October 2011 as well as some older, lower priority Microsoft Security Updates. We have also included relevant Security Updates from Adobe Systems and the new .NET 4 Framework for Windows Embedded Standard.
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable DUA covering primarily August 2010 through April 2011 as well as some older, lower priority Microsoft Security Updates. We have also included two relevant Security Updates from Adobe Systems Incorporated.
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable installer covering January 2010 through August 2010. This update addresses the vulnerability discussed in NERC R-2010-09-13-01 (MS10-046).
This version of Silverlight for Windows Embedded Standard will update your current Silverlight 4.X version to 4.0.60531.0.
Use SEL BaRT to quickly and easily create a complete drive backup to capture your computing platform’s operating system and applications. Backups can be used for disaster recovery or to deploy a configured image across many similar systems. SEL BaRT was designed specifically for SEL’s computing platform line to ensure ease of use and compatibility with each platform’s features, including the system watchdog which is responsible for monitoring system availability.
SEL BaRT is custom-developed by SEL using open-source technology to be fast, portable, and free of charge. Back up a system drive in as little as 15 minutes, then, when needed, you can restore the backup image in even less time. Easily install SEL BaRT onto a USB drive using the included make_bart Windows and Linux installation tools. See the included README.TXT file for installation instructions. The included application guide AG2012-05 (also available for download) provides detailed installation and usage instructions.
The download will be in the form of a self-extracting executable with an .exe extension. From a Windows OS, click on the file once downloaded and the files will extract similar to a .zip file.
The Windows SysMon is a front-end graphical user interface (GUI) and back-end Windows service (SEL Service).
Copy the setup.exe file to your SEL-3354 and as an administrator user run the setup program with the following arguments, depending on your Microsoft® operating system version.
| Operating System | Installation Arguments |
|---|---|
| Windows XP Pro | setup.exe /product=3354 |
| Windows Embedded Standard | setup.exe /product=3354WES |
| Windows 2008 Server | setup.exe /Product=3354 /D=C:\Windows\SysWOW64\SELShell |