html{display:none} Software Downloads | Schweitzer Engineering Laboratories

Software Downloads


Filter
Model
Operating System
Categories
4 Results Found Current Page: 1 of 1

SEL USB Driver

This driver enables USB communication between Windows computers and SEL USB ports for the following devices:

  • SEL-2440
  • SEL-3031
  • SEL-C662
  • SEL-C667
  • SEL-3021
  • SEL-9192
  • SEL-T4287

Installation Instructions

  1. Download the driver that corresponds to your version of Windows.
  2. Run the installer, if present, or follow the driver instructions.
  3. To see new COM port assignment, open Device Manager and expand Ports.
For Windows 11 operating systems.

Version R11.1.0.53
Size 1.88 MB
Date Code 20221007

Verifying SEL Software Downloads

For 32-bit and 64-bit Windows 10 operating systems. (Multi-language support)

Version R6.7.5
Size 3.58 MB
Date Code 20180515

Verifying SEL Software Downloads

For 32-bit and 64-bit Windows 8, Windows 7, Vista, and XP operating systems. (Multi-language Support)

Version R6.6.0.0
Size 3.56 MB
Date Code 20130215

Verifying SEL Software Downloads

USB Port Driver and Installation Instructions

This driver enables USB communication between Windows computers and SEL USB ports for the following devices:

  • SEL-311C
  • SEL-351
  • SEL-351A
  • SEL-351RS Kestrel
  • SEL-351S
  • SEL-651R
  • SEL-651RA
  • SEL-T400L
  • SEL-T401L
  • SEL-TWFL

Installation Instructions

  1. Download zip directory and extract files.
  2. Open and follow installation instructions.
For Microsoft Windows operating systems.

Size 580.00 kB
Date Code 20240424

Verifying SEL Software Downloads

SEL-3600 USB Driver

Use the built-in front USB Port to connect locally with the Ethernet Security Gateway.

Installation Instructions

  1. Unzip the archive to a location on your computer.
  2. Connect the USB A-to-B cable to your computer and an SEL-36XX.
  3. Go to the Device Manager and find the device. Right click and select "Update Driver Software."
  4. Choose "Browse my computer for driver software in the pop-up window.
  5. Browse to the folder that you saved the archive contents to and select that folder. Click "Next."
  6. Click "Install" when prompted.
  7. Once the installer finishes you will see "SEL USB Ethernet/RNDIS Gadget" under Network Adapters in the Device Manager.
For Windows 7, and Windows 10 operating systems.

Version 1.0
Size 8.00 kB
Date Code 20170228

Verifying SEL Software Downloads

SEL Backup and Recovery Tool (BaRT)

Use SEL BaRT to quickly and easily create a complete drive backup to capture your computing platform’s operating system and applications. Backups can be used for disaster recovery or to deploy a configured image across many similar systems. SEL BaRT was designed specifically for SEL’s computing platform line to ensure ease of use and compatibility with each platform’s features, including the system watchdog which is responsible for monitoring system availability.

SEL BaRT is custom-developed by SEL using open-source technology to be fast, portable, and free of charge. Back up a system drive in as little as 15 minutes, then, when needed, you can restore the backup image in even less time. Easily install SEL BaRT onto a USB drive using the included make_bart Windows and Linux installation tools. See the included README.TXT file for installation instructions. The included application guide AG2012-05 (also available for download) provides detailed installation and usage instructions.

SEL BaRT

Version 5.0.1.1
Size 139.64 MB
Date Code 20240328

Notes

The download will be in the form of a self-extracting executable with an .exe extension.  From a Windows OS, click on the file once downloaded and the files will extract similar to a .zip file.

Verifying SEL Software Downloads