SEL has released the SEL-2742S Software-Defined Network Switch, a 12-port software-defined networking (SDN) Ethernet switch. This addition to our SDN portfolio provides utilities and industrial operations with a choice of surface or DIN-rail mounting.
Key features of the SEL-2742S include the following:
*Note: At first release, the SEL-2742S will be available with all copper ports. A second configuration with two 1 Gbps multimode fiber ports and the rest copper is scheduled to release in early 2021, and more configurations will follow.
We have also released a new version of the SEL-5056 Software-Defined Network Flow Controller, Version 2.3.0, to support the SEL-2742S.
For more details, visit the SEL-2742S product page.