ICON News

34 results

Nov 12, 2025

The SEL ICON team is releasing redesigned Nx64F Multimode and Single-Mode submodules and is discontinuing the Module (PLM) due to component obsolescence. Learn about the recommended replacement and read the updated documentation.

Jun 25, 2025

With Version 4.6.0.0, we released many new enhancements to the SEL-5051/5052 Client/Server Network Management System (NMS) Software.

Nov 25, 2024

The ICON is receiving a new submodule that provides an interface for channelized, synchronous E1 traffic transported by SDH-based WANs and E1 channel banks.

Nov 4, 2024

ICON supports Ethernet Layer 2 802.1Q bridge and allows the transmission of non-critical Ethernet services in the same channel as VSN.

Jun 7, 2024

The SEL-5051 Client and SEL-5052 Server Software are receiving many enhancements requested by users.

Jan 19, 2024

SEL recently released Version 4.4.0.1 of the SEL-5051/5052 Client/Server Network Management System (NMS) Software. The latest release provides some significant enhancements, many of which were in response to User Group requests.

Aug 11, 2023

Firmware R104 for the FXS submodule resolves issues with On-/Off-Hook indication, DS1 hot-standby operation, and physical port disabling from software. As an additional cybersecurity enhancement, R104 update disables the onboard serial port.

May 26, 2023

SEL recently released version 4.3.0.0 of the SEL-5051/5052 Client/Server Network Management System (NMS) Software. The latest release provides some significant enhancements, many of which were implemented in response to customer requests.

Feb 13, 2023

SEL University will be offering training courses for the SEL ICON in spring and fall 2023.

Feb 1, 2023

New firmware has been released that addresses recently identified issues with the SEL ICON’s time synchronization subsystem. These issues have the potential to impact the stability of the network under certain timing reference conditions. The new firmware also provides enhancements that improve the resiliency of the network during time interruption events.

Sep 27, 2022

The latest versions of DS1 Sync and Server Module firmware introduced two new features. Users can define the severity of Loss of Signal alarms as Minor or Major, depending on whether the port is a line or access port. Interoperability with third-party voice modules has been improved with Robbed Bit Signaling.

Sep 27, 2022

SEL has released a full set of DS1 Async and DS1 Sync submodules, functionally equivalent to and hot-swappable with installed counterparts. These alternatives will help address a supply chain issue with an FPGA part used in ICON submodules.

Sep 13, 2022

SEL has released several new enhancements for the SEL ICON platform and SEL-5051 Client and SEL-5052 Server Network Management System (NMS) software. Many of these enhancements were developed in response to User Group requests.

Feb 15, 2022

SEL has released a new version of the SEL 5051/5052 Client/Server Network Management System Software and Server Module Firmware R127. These updates address a supply chain issue with a field-programmable gate array device used in various ICON modules.

Oct 22, 2021

SEL offers significant enhancements in its newly released version of the SEL-5051/5052 Client/Server Network Management System Software.

Oct 22, 2021

A new firmware release adds DS1 line timing support for the Enhanced Protected Line Module (EPLM), Firmware R101-V1, and the DS1 Sync Submodule, Firmware R102-V1. This timing support enables the SEL ICON to synchronize to an external DS1 reference or BITS clock.

Oct 22, 2021

A new firmware release for the Transfer Trip Module (TTM), Firmware R105, provides an increase in the latency alarm threshold from 2–15 ms to 2–30 ms.

Apr 21, 2021

SEL’s newly released line module, the Enhanced Protected Line Module (EPLM), is fully backwards compatible with the existing Protected Line Module (PLM) and provides significant new capabilities to the SEL ICON platform.

Apr 21, 2021

SEL released a new access module to provide support for EIA-232, EIA-422, and EIA-485 circuits when operating as a DS1 channel bank.

Apr 21, 2021

SEL’s recent release of Version 4.0.0.0 of the SEL-5051/5052 Client/Server Network Management System (NMS) Software provides support for the Enhanced Protected Line Module (EPLM) and Async Data CB Submodule.

Page 1 of 2