html{display:none} SEL-710 Motor Protection Relay—Thermal Model Elements and Settings | Schweitzer Engineering Laboratories
Recorded Webinar

SEL-710 Motor Protection Relay—Thermal Model Elements and Settings

Date held: December 16, 2020
Duration: 2 hours

During this recorded technical presentation SEL presenters Derrick Haas and Krithika Bhuvaneshwaran discuss the thermal element in the SEL-710 Motor Protection Relay. The thermal element is used to provide locked rotor, running overload, and negative-sequence current unbalance protection.

During the webinar, you will:

  • Learn about the first-order thermal model.
  • Understand the different methods to set the thermal element.
  • Develop settings using the rating method and check coordination.

You can use the knowledge gained from this webinar to set the thermal element and understand how the motor is protected.

Learn From the Experts

Krithika Bhuvaneshwaran
Presenter

Krithika Bhuvaneshwaran (KB)

Application Engineer I—Protection
Derrick Haas
Presenter

Derrick Haas