Schweitzer Engineering Laboratories

Newsroom

Jan 26, 2023

Secure and Reliable Stator Ground Protection, 100 Percent of the Time

The SEL-2664S Stator Ground Protection Relay is a robust option for generator stator ground protection. The relay uses neutral-overvoltage-based protection and multisine frequency injection to protect 100 percent of the stator winding, even when the generator is at a standstill. The unique multisine frequency injection function injects and measures impedances at four different frequencies to determine any losses in stator winding capacitance—regardless of whether the generator is at a standstill, starting up or running. Calibration processes performed during commissioning provide an accurate measurement of all wire impedances, allowing the relay to be highly sensitive to overvoltage in a specific system.The SEL-2664S now ships with the SEL-4664 Calibration Module. This module supports a new calibration process in the relay by automatically cycling through several impedance levels, which the SEL-2664S tests to create an accurate model of system impedances. This fully automated process takes approximately 10 minutes and requires no interaction from the engineer commissioning the device. For more information, please see the SEL-2664S product page.
Back to Newsroom 
Featured Stories

Press Release

SEL Advances Development of Investigational Autism Screening Device, Launches Clinical Trial

Press Release

SEL Names New VP of Marketing and SEL University

Press Release

SEL Completes Purchase of New Post Falls Manufacturing Site

  • SEL Invests More Than $500 Million to Expand U.S. Manufacturing Capacity
  • SEL Releases Two New Solutions for High-Density Serial-to-Ethernet Communications

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow