Belgium Integrates Offshore Wind Power Into European Grid

Many People Were Counting On It

Despite its compact size, Belgium is a major exporter of products, from automobiles and computers to fine chocolates and beer, which contributes to its highly developed economy. Not long ago, the nation faced a headwind. Heavily dependent on nuclear power for more than a half century, the federal government ordered the country’s seven aging reactors to be phased out by 2025. Officials also set a goal of gaining energy independence and lowering carbon emissions by reducing fossil fuel imports and deploying renewable sources. “It was part of a wider move to shift toward renewable energy across all of the European Union,” said Hanuise of Elia, which owns and operates the Belgian transmission grid and is responsible for importing and exporting electricity with neighboring countries. How would Belgium ensure clean, reliable energy for its future? Enter the strong, steady winds blowing off its coast.

From Sea to Belgium and the UK

How does energy produced by the wind turbines get miles to land where it’s needed? First, it’s transported through cables buried along the ocean floor to an offshore switchyard platform owned and operated by Elia. From there, it travels through another network of subsea cables to a substation on the Belgian coast. From there, Elia’s new 380 kV transmission corridor carries the power into Belgium’s mainland. And in a second major role, the corridor facilitates the exchange of up to 1,000 MW of electricity between Belgium and the United Kingdom through a high-voltage direct current (HVdc) link. The joint project by Elia and UK’s National Grid includes a submarine cable that runs 81 miles along the seabed.
But even though the link was finished and tested late last year, engineers would not energize it until the SPS was in place.“The amount of power capable of being transported through the transmission corridor—both from the offshore windfarms and from the HVdc link—is equivalent of up to three nuclear reactors,” Hanuise explained. Meaning that if a severe storm were to trigger a fault, power stability could be compromised. To avoid blackouts, an SPS was needed to detect abnormal conditions along the corridor and quickly respond. Ultimately, Elia selected a company outside Europe to provide it. “We picked Schweitzer Engineering for two main reasons,” said Hanuise. “They proposed the best solution with very technologically advanced relays. We also took into account that they had done comparable SPS projects in other countries, such as Georgia and Uruguay, with very good results.”

Ticking Clock

Not only did the SPS project require a perfect alignment of expertise and technology—it demanded haste. Teaming up with Elia, SEL’s Engineering Services division faced a finish date in less than 10 months.“Normally, a project like this would probably take a year and a half or even longer,” said SEL’s Milind Malichkar, the SPS project’s technical lead. “So a group of us sat in a room, looked at the schedule, and broke it down week by week, day to day. We analyzed each stage to see how we could save time without cutting back on quality, with the goal of employing fast and innovative methods for solution delivery.”
Inside Elia’s national dispatching, or control room, Rodolphe Hanuise and SEL’s Milind Malichkar examine a wind production forecast graph. Belgium’s electric grid is illuminated to their right.
The strict deadline was necessary to protect the Belgian grid from instability once the HVdc link became operational in late January 2019. But it was also needed to avert a possible energy shortfall during Belgium’s coldest time of year. With several nuclear reactors taken offline for maintenance, “it was critical that our country have the additional power-importing capacity in case of a prolonged cold spell,” said Hanuise.At SEL branches in Spain, Mexico, and the United States, SEL workers strove to complete their SPS tasks on time, on budget, and with high quality. To meet the January 31 deadline, Malichkar and the engineering team spent weeks in Belgium commissioning the SPS.“A lot was riding on the project,” said Malichkar. “There was a sense of urgency, and we all understood this.”

Software-defined networking (SDN) was integrated into the SPS project to increase cybersecurity.

Surprising Results

As leaves turned to gold and red across Belgium, the panels were finished at SEL’s Mexico branch and then quality-tested. Next, they were shipped to headquarters in Pullman, Washington, for two weeks of rigorous hardware-in-the-loop testing. “This is where we put all the equipment through simulation scenarios to verify how the SPS would react as if it were in a real field setting,” said Malichkar. For example, real-time digital simulation was used to model the wind farms, the HVdc link, and the transmission corridor so engineers could see how quickly the SPS would respond during different power system contingencies. During testing, the SPS was expected to detect abnormal conditions and initiate corrective action in 40 milliseconds, as required by Elia. But the outcome couldn't have been better. It took only 20 milliseconds. “It was faster than what Elia expected—faster than we expected,” said Malichkar. “The testing gave us the proof and the renewed confidence to move the project forward.” Now certain that the SPS was proven, deployable, and within cost, each fully equipped panel was carefully packaged at SEL’s Solution Delivery Center for air transport to Belgium.
Meanwhile, it wouldn’t be long before the season’s first snowflakes fell over the high hills of the Belgian Ardennes region. Winter approached—as did the January deadline. Following installation and further testing in Belgium, the protection system was successfully energized on January 25. When the clock struck midnight on January 31, the HVdc link started commercial operation. The next day, the international news agency Reuters published a story about the achievement. John Pettigrew, chief executive of the UK’s National Grid, was quoted as saying: “Interconnectors like the HVdc link are the perfect tool to move renewable energy from where it is produced to where it is needed most.”

Rise of the Wind Turbines

Today, when someone flips on a light switch in Brugge, Belgium, or in Kent, England, the electricity powering the bulb was probably channeled through Elia’s transmission corridor. With the SPS in place, Elia is able to track signs of disturbances and respond rapidly before a problem escalates into a power failure.Multiple SEL devices are working together to keep the power system stable and secure, said SEL’s DeWald. “We helped to integrate and stabilize delivery of a new source of renewable power that’s been brought into the European grid,” he said. “That’s something we’re very proud of.” When two additional wind farms go online by 2020, offshore wind energy will make up more than 10 percent of the total Belgian energy mix, said Hanuise. “This is only a first step,” he said. “The SPS allowed us to dream bigger by opening the path to even more green energy integration in the future.” With the addition of more turbines by 2024, the wind farms will be capable of generating 14 terawatt-hours each year, “enough to power 85 percent of all Belgian households,” he explained.And the next time a severe storm rolls through, the SPS could mean that end customers—whether a chocolatier, car manufacturer, or potato farmer—will experience a mere flicker of lights instead of a blackout.