Productos
Soluciones
Servicios de ingeniería
Educación
Soporte
Empresa
Iniciar sesión
SEL-3530-4
Presentación
Documentos
Soporte
SEL-3530-4
Toggle Dropdown
Presentación
Documentos
Soporte
Documentos
Destacados
Manual de instrucciones
SEL-3530-4 Real-Time Automation Controller (RTAC) and
acSELerator
RTAC SEL-5033 Software
Hoja de datos
SEL-3530-4 Real-Time Automation Controller (RTAC)
Folleto
Control de estación, IHM web e ingreso integrados SEL-3530
Literatura
Los documentos más nuevos se muestran primero.
Incluir la literatura en inglés
Literatura
Folletos
Control de estación, IHM web e ingreso integrados SEL-3530
Inglés
SEL Real-Time Automation Controller (RTAC) Product Family
Human-Machine Interface (HMI) for SEL Real-Time Automation Controllers (RTACs)
Automated NERC PRC-005 Maintenance and Testing
Secure Communications and Control Solutions
Grid Connect
Example Secure Control System Diagram
Hojas de datos
Inglés
SEL-3530-4 Real-Time Automation Controller (RTAC)
Guías de especificación
Inglés
SEL RTAC (3505, 3530, 3530-4, 3532, 3555, 2240) Guideform Specification
SEL RTAC (3505, 3530, 3530-4, 3532, 3555, 2240) Guideform Specification
Guías de instalación
Inglés
SEL-3530 RTAC HMI and Diagram Builder Setup Guide
Getting Started With RTAC
Manuales de instrucción
Inglés
SEL-3530-4 Real-Time Automation Controller (RTAC) and
acSELerator
RTAC SEL-5033 Software
Notas técnicas de firmware
Inglés
RTAC R155-R201 Technical Note
RTAC R154-R200 Technical Note
RTAC R153 Technical Note
RTAC R152 Technical Note
RTAC R151 Technical Note
Publicaciones
Guías de aplicación
Inglés
Configuring
acSELerator Team
for SEL-3620 and RTAC Tiered Communications Architectures: Password Changes, Event Collection, and SOE Collection
SEL Fiber-Optic Device Compatibility Guide
Parsing the GPS Location in GPS NMEA Data From a Sierra Wireless RV55 Cellular Modem by Using RTAC Flex Parsing
Understanding and Using Static Routes in the SEL RTAC
Implementing Communication Redundancy in the RTAC
Related Material
RTAC Redundancy Projects
RTAC Redundancy Appendix A Projects
Using IEC 60870-5-103 Protocol Between the SEL Real-Time Automation Controller and SEL-751 Relays and Siemens SIPROTEC 7SJ80 Relays
Double-Ended Traveling-Wave Fault Locating Using the SEL RTAC as a DNP3 Client
Related Material
fb_TWFaultLocation.xml
Monitor IEEE 519 and 1547 Harmonic Distortion Levels With an SEL-735 and RTAC
Related Material
XML_Files
Modbus Configuration for SEL-700 Series Relays and RTAC Devices
Retrieving Event Files From the RTAC by Using File Transfer Protocol
Managing IED Passwords With the SEL-3620 Ethernet Security Gateway and SEL RTAC Using SEL Server Connections
Understanding and Using Functions and Function Blocks in the RTAC
Configuring the SEL RTAC to Exchange Data With SEL IEDs Over IEC 61850 GOOSE
RTAC–IEC 61850 MMS Client-Server
Configuring the SEL-2488 to Distribute PTP to an SEL-3530 by Using SEL-2740S
Using SEL Fast Message Protocol Between the SEL-3530 RTAC and the SEL-2032
Using Flex Parsing in the RTAC With SEL Protocol to Obtain Energy Metering Data
SEL Fiber-Optic Communications Device Specifications
Configure the RTAC to Obtain Temperature Measurements From SEL Relays Via Flex Parse Messaging
Detecting a Loss of Communication Between an RTAC and a Relay
Configuring the SEL-3530 RTAC to Obtain Temperature Measured Using the SEL-2600
Using Shared Tags to Optimize an RTAC HMI
Related Material
Demo Shared Tags
Defining DCE and DTE: Null Modem Cable and Straight-Through Cable Applications
Converting SEL-651R Event Type ASCII Character Strings to DNP3 Analog Inputs in the RTAC
Tiered Communication Between Remote Locations Using Multiple SEL-3530 RTACs
Automating Common RTAC Maintenance Tasks Using Python Scripts and SEL Software
Related Material
Python Scripts-AG2020-08
Using the DateTime Triggers Extension to Simplify Time-Based Triggering of Standard IEC 61131-3 Logic in the SEL RTAC
Related Material
DateTime Triggers extension
Using Wireshark to Troubleshoot Protocol Communications Issues on an RTAC
Programming a Phase Angle Difference Monitor in the SEL RTAC
Using an RTAC to Get Three-Phase Fault Currents From SEL-400 Series Relays
Conversion Tips and Important Differences Between the SEL-3530 RTAC and the SEL-3555 RTAC
Understanding and Effectively Using the SEL
Mirrored Bits
Protocol
Event Collection From SEL-3530 RTAC Using Team
SEL RTAC Axion Batch Sequencing With HMI for Industrial Automation Using Ladder Logic
Implement Serial DF1 Client Protocol in an RTAC By Using an
acSELerator
RTAC Extension
Related Material
DF1 Client
Configuring the SEL RTAC as a Single Source for Substation Event Data: Job Done Examples of Various Methods for Collecting and Retrieving Digital and Oscillographic Records
Using Breaker and Remote Bits to Implement Controls Through DNP3 From an RTAC HMI
Configure the SEL-3530 and SEL-3610 to Collect Temperature Data Using the SEL-2600
Creating a Syslog Heartbeat in an SEL RTAC, SEL-3610, and SEL-3620
Using an RTAC to Monitor Network Status With SNMP
RTAC Commissioning Assistant
Related Material
Commissioning_Assistant
Commissioning Assistant
Using an RTAC to Monitor and Report Firmware and Settings Changes in SEL Relays
Using Syslog to Report SEL Relay Security Status
Using an RTAC to Monitor GOOSE Statistics on SEL Relays
Applying a Universal Expression in the RTAC to Parse RTD Data From SEL Devices
Using an SEL RTAC to Integrate the SEL-T400L Relay With SCADA
Maximizing RTAC Performance
Configuring an RTAC for a Typical SCADA Application
Setting the Modbus User Map on the SEL-734 and SEL-735 Meters Using the RTAC and FileIO Library
Related Material
UserMap
UserMap Spreadsheet
Integrating Fast Controls With SCADA Operations in the RTAC
Configure an SEL-3530 RTAC to Communicate With a Davis Weather Station
Proportional Integral Derivative Controller Tuning for the Real-Time Automation Controller (RTAC) Platform
Convert SEL Fast Message Synchrophasor Messages to IEEE C37.118 Using the RTAC
Using Wireshark to Decode RTAC Serial Line Messages and SEL Protocols
Managing Time in the RTAC
Setting Up an RTAC HMI for an SEL-700 Series Relay Using Various Protocols
Using an RTAC to Read and Write Analog Data Values to an SEL-2411 Using SEL Fast Message Protocol
Basic and Advanced Applications of the SEL-3530 RTAC Access Point Router
Using an RTAC to Automatically Manage the Date and Time in Legacy Relays
Notas de aplicación
Registro de eventos analógicos en base de datos a través de los RTAC de SEL
Inglés
IEC 61131-3 Variable Usage and Initialization in the RTAC
Using Network Global Variable List Communications in Decentralized Control Solutions
Using the RTAC as a Modern Serial Data Line Analyzer
Open Channel Flow Control Using the SEL-2411, SEL-3031, and RTAC
Distributed Data Acquisition Using the SEL-2411 PAC and SEL-2440 DPAC
Power Plant - Steam Control
Adding Radio Pilot Channels and Backing Up SCADA Communications
Solar Tracking Using the SEL-2411 PAC and SEL-3530 RTAC
Use Synchrophasors in SCADA/EMS
Control Rotary Assembly Table Systems With SEL Automation Products
Casos de estudio
Inglés
NREL Selects SEL Microgrid Controller for the Energy Systems Integration Facility
Artículos técnicos
Inglés
Wind Farm Volt/VAR Control Using a Real-Time Automation Controller
Libros blancos
Inglés
Best Practices for Implementing PTP in the Power Industry
Using Defense in Depth to Safely Present SCADA Data for Read-Only and Corporate Reporting
Automating Protection System Monitoring and Verification With the SEL RTAC
Leveraging Security – Using the SEL RTAC's Built-In Security Features
Diagramas