Schweitzer Engineering Laboratories

Newsroom

May 17, 2023

SEL-3350 3U Joins the SEL Automation Family

SEL recently released a 3U form factor for the versatile and rugged SEL-3350 computing platform.The SEL-3350 can be configured—and easily reconfigured—as a Real-Time Automation Controller (RTAC), an SEL Blueframe application platform or a Linux- or Microsoft Windows-based computer. As an RTAC, the SEL-3350 represents the next generation of the popular SEL-3530. Like the SEL-3530, the SEL-3350 offers 1U and 3U form factors, an operating temperature range of –⁠40° to +85°C (–⁠40° to +185°F) and a similar price point. But it improves upon the SEL-3530 with: 
  • Five times the processing power. 
  • The addition of a DisplayPort connection. 
  • The addition of a digital input/battery monitor with 0.5 percent dc accuracy. 
  • 8 GB of memory. 
  • Up to 2 TB of storage. 
  • Five 10/100/1000BASE-T Ethernet ports. 
Additionally, the SEL-3350 3U form factor is an ideal replacement for SEL-2030 and SEL-2032 Communications Processors and legacy remote terminal units (RTUs) from other manufacturers. The new 3U form factor offers the following options: 
  • Serial expansion board—offering an increase from the standard 16 ports to a total of 48 RJ45 EIA-232/422/485 ports. 
  • Digital I/O expansion board—24 inputs with software-configurable voltage ranges, and 8 outputs.
  • Redundant hot-swappable power supplies. 
Learn more about the SEL-3350 computing platform.
Back to Newsroom 
Featured Stories

Technical

SEL Achieves IEC 62443-2-4 Certification, Strengthening Cybersecurity Assurance for Critical-Infrastructure Customers

Press Release

SEL Continues to Expand Manufacturing Capacity With New Post Falls, Idaho Facility

Press Release

SEL Expands Manufacturing Operations in Idaho with New Facility in Nampa

  • Idaho: Closing the Innovation Gap
  • SEL Increases Manufacturing Wages to Support Growing Global Demand

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow