Schweitzer Engineering Laboratories

Newsroom

Jan 26, 2023

Webinar: Innovation in IEC 61850 Digital Secondary Systems

Process bus communications systems must maintain high availability for analog-to-digital data streams and control signals from protective relays. A webinar on February 22, 2023, will discuss recent innovations in IEC 61850-compliant digital secondary system devices that allow increased availability and reliability in process bus applications.In this webinar, learn about recent enhancements to SEL-400 series relays that make them even more flexible and valuable additions to an IEC 61850-9-2 Sampled Values (SV)-based system. Enhanced communications capabilities improve access to diagnostic information, allow the use of the Parallel Redundancy Protocol (PRP) on process bus applications and provide an additional port for engineering access.For more information and to register, visit the webinar webpage.  
Back to Newsroom 
Featured Stories

Press Release

SEL Advances Development of Investigational Autism Screening Device, Launches Clinical Trial

Press Release

SEL Names New VP of Marketing and SEL University

Press Release

SEL Completes Purchase of New Post Falls Manufacturing Site

  • SEL Invests More Than $500 Million to Expand U.S. Manufacturing Capacity
  • SEL Releases Two New Solutions for High-Density Serial-to-Ethernet Communications

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow