Schweitzer Engineering Laboratories
Newsroom
Feb 12, 2015
SEL Expands High-Performance Transformer Differential Protection for 2-, 3- and 4-Terminal Applications
PULLMAN, Wash. — Schweitzer Engineering Laboratories, Inc. (SEL) today announced three new additions to the popular SEL-787 family of differential protection relays, providing low-cost, versatile transformer differential protection for an expanded range of applications.The new relays (SEL-787-3E, -3S, -4X) offer the following benefits for transformer protection:
- Protection for transformers in 2-, 3-, or 4-terminal applications using one relay family, keeping schematics simple and minimizing the learning curve
- Expanded capability to apply current differential, voltage, frequency, and/or thermal-based protection functions
- Sensitive detection of internal faults near the grounded neutral with as many as three restrictive earth fault (REF) elements
Featured StoriesSEL Achieves IEC 62443-2-4 Certification, Strengthening Cybersecurity Assurance for Critical-Infrastructure CustomersSEL Continues to Expand Manufacturing Capacity With New Post Falls, Idaho FacilitySEL Expands Manufacturing Operations in Idaho with New Facility in Nampa
Technical
Press Release
Press Release