Device Management and Automation (DMA)
Download the Latest Versions
Blueframe Device Management and Automation (DMA)
DMA is a software solution designed to support automated data collection, management, normalization, and availability from critical infrastructure devices within the Blueframe platform. DMA automates and accelerates the collection of oscillography, Sequence of Events (SOE), device settings, and property information. DMA applications also provide automated password rotation and streamline device audits through custom summary reports to identify device changes.
Configuration Monitoring
Configuration Monitoring is an optional DMA package that enables settings and device property data collection and viewing from supported devices. Within this package, you will find the Configuration Monitoring application, which is used for configuring the data collection plans, and Configuration Monitoring Archive, which is used for viewing assessments of collected data.
Version: 1.19.0Size: 243.09 MBDate Code: 20260802
Credential Management
Credential Management is an optional DMA package that enables automated credential rotation with the use of an SEL security gateway and collection of the proxy reports. Within this package, you will find the Credential Management application, which is used for configuring the rotation and proxy report collection plans, and the Credential Management Archive, which is used for report creation and viewing related to resource credentials and their rotation schedule.
Version: 1.20.0Size: 286.15 MBDate Code: 20260802
Custom Monitoring
Custom Monitoring is an optional DMA package that enables automated file or command result collection. Within this package, you will find the Custom Monitoring application, which is used for configuring the file or command result collection plans, and the Custom Monitoring Archive, which is used for viewing the collected files or command results.
Version: 1.13.0Size: 243.45 MBDate Code: 20260802
Disturbance Monitoring
Disturbance Monitoring is an optional DMA package that enables event and SOE data collection and viewing from supported devices. Within this package, you will find the Disturbance Monitoring application, which is used for configuring the data collection plans, and Disturbance Monitoring Archive, which is used for viewing assessments of collected data.
Version: 1.21.0Size: 265.57 MBDate Code: 20260802
DMA Tools
The DMA Tools package is included with any DMA package purchase and provides the DMA Diagnostics and DMA REST API applications. DMA Diagnostics provides troubleshooting, diagnostics, and system status information crucial for managing the sophisticated communications infrastructure that the automation system must traverse to gather device data. The DMA REST API provides read-only access to DMA-collected data and logs. When installed through this package, this application provides documentation on the specific queries available for programmatic access to the data stored in the DMA private database.
Version: 1.19.1Size: 222.14 MBDate Code: 20260802
Meter Monitoring
Meter Monitoring is an optional DMA package that enables load data profile (LDP) and voltage sag, swell, and interruption (VSSI) data collection and viewing from supported devices. Within this package, you will find the Meter Monitoring application, which is used for configuring the data collection plans, and Meter Monitoring Archive, which is used for viewing assessments of collected data.
Version: 1.10.0Size: 243.07 MBDate Code: 20260802
Resource Communication Services
Resource Communication Services contains the communications services and automation execution logic to enable the proper fulfillment of DMA application plan configuration. Resource Communication Services also provides the communications layer for the Direct Resource Access application.
Full Install
Version: 1.23.1Size: 511.43 MBDate Code: 20260810
Connection Services
The Connection Services package is required for use with any DMA package purchase. This package includes Resource Management, which is the application in which system resources are defined with their associated attributes and connection parameters. Other applications in the Blueframe ecosystem can use the Connection Services package to support resource interaction.
Full Install
Version: 1.21.1Size: 255.73 MBDate Code: 20260810
Blueframe OS
The Blueframe platform rests on the Blueframe OS and serves as its main user interface. The Linux-based Blueframe OS offers basic hardware settings, such as display configuration.
Full Install
Version: 1.16.1Size: 1.52 GBDate Code: 20261103