Schweitzer Engineering Laboratories

Newsroom

Oct 5, 2021

SEL Releases Enhanced SEL-2725 Five-Port Ethernet Switch

Schweitzer Engineering Laboratories has released numerous enhancements for the SEL-2725 Five-Port Ethernet Switch that provide additional flexibility when it is used in utility and industrial applications. The unmanaged five-port switch and copper-to-fiber-optic media converter now includes the following:

  • An all-copper option to provide five 10/100BASE-T ports.
  • A field interface option that combines 100BASE-LX single-mode and 100BASE-FX multimode ports for media converter applications.
  • A universal power supply (12–250 Vdc, 110–240 Vac) to simplify the hardware.
  • Improved surge immunity for better performance, allowing the SEL-2725 to continue meeting or exceeding IEEE 1613 Class 2 standards.
  • The CE Mark, indicating that it meets the regulatory requirements for use within the European Economic Area.

To learn more, visit the product webpage.

Back to Newsroom 
Featured Stories

Press Release

SEL Announces 2025-2026 Scholarship Recipients

Corporate

SEL Receives Purdue Senior Design Partner of the Year Award

Corporate

SEL Technical Experts Recognized for Contributions to Industry

  • SEL Raises Starting Hourly Wage to $20
  • SEL develops a land mobile radio solution that protects first responders

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow