Schweitzer Engineering Laboratories

Newsroom

Sep 23, 2021

Two New Field Interfaces Available for the SEL-734W Capacitor Bank Control

Schweitzer Engineering Laboratories has released two new field interface options for the SEL-734W Capacitor Bank Control—a 7-pin connector and a terminal block—to offer increased installation versatility for the SEL-734W and SEL-8340 Wireless Current Sensor solution. This solution delivers a quicker, simpler and safer way to provide accurate current-based control for capacitor bank installations. With all of the SEL-734W control’s field interface options, installing new capacitor banks with advanced control or updating existing time- and temperature-based capacitor bank controls for more accurate switching is simpler than ever.Using either the 4-jaw socket-based interface or the new terminal block interface, replace existing socket-based controls with a current-enabled solution without replacing any of the primary equipment. The terminal block option allows for end-user access and self-wiring through a weather-tight opening at the bottom of the enclosure, providing additional SEL-734W implementation versatility. For new installations, the SEL-734W control’s new 7-pin connector-based interface makes it easier to install in the field using a single cable for both measurement and control. Both the 7-pin connector-based and self-wired versions of the control have provisions for a wired neutral current input to detect imbalance or failed capacitors. They also have a contact input that can be used for switch status. To learn more about the SEL-734W and SEL-8340 solution, visit the product webpage. 
Back to Newsroom 
Featured Stories

Technical

SEL Website Improves Navigation With New Sections for Products, Industries, and Services

SEL In The News

Inventing the future: An interview with Dr. Ed Schweitzer

SEL In The News

Tariffs are harming manufacturing. Congress must act now

  • SEL enhances the performance and digital input capacity of the SEL-2240 Axion
  • How two SEL employees turned a simple fix into a patented solution

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow