Schweitzer Engineering Laboratories

Newsroom

Oct 23, 2020

SEL Releases Redundant Power Module

Schweitzer Engineering Laboratories has released the SEL-RPM Redundant Power Module, a reliable and simple multisource module to power protection, monitoring and control equipment.The SEL-RPM combines as many as three ac sources and one dc source to provide uninterrupted ride-through during voltage sags, momentary interruptions or a complete loss of control power. The module’s unregulated 125 Vdc output helps reduce device restarts, and its large energy storage capacitors allow it to support switch or breaker trip/close applications.With no jumpers, user settings, batteries, firmware or other components that wear out or need attention, the SEL-RPM is easy to use and maintenance-free. Learn more about the SEL-RPM on the product webpage.
Back to Newsroom 
Featured Stories

Technical

SEL Achieves IEC 62443-2-4 Certification, Strengthening Cybersecurity Assurance for Critical-Infrastructure Customers

Press Release

SEL Continues to Expand Manufacturing Capacity With New Post Falls, Idaho Facility

Press Release

SEL Expands Manufacturing Operations in Idaho with New Facility in Nampa

  • Idaho: Closing the Innovation Gap
  • SEL Increases Manufacturing Wages to Support Growing Global Demand

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow