Schweitzer Engineering Laboratories

Newsroom

Oct 14, 2016

Compact, Expandable Industrial Computer Includes 10-Year Warranty and Delivers Performance and Durability

Made in the USA, the new SEL-3360E Compact Industrial Computer from SEL features the Intel® Core™ i7 processor, a –40° to +60°C operating range, no vents and no moving parts.PULLMAN, Wash. — Schweitzer Engineering Laboratories, Inc. (SEL) announced the newest addition to their compact industrial computer family, the SEL 3360E. The SEL-3360E and the SEL-3360S are industrial computers designed for extreme environments and small spaces. SEL-3360 Computers feature powerful processing power provided by Intel Core i7 processors. To ensure the highest reliability, SEL-3360 Computers support RAID configurations and use single-level cell (SLC) NAND flash memory. Up to 16 GB of error-correcting code (ECC) RAM provides ample memory for demanding applications. In addition, the SEL-3360E incorporates two PCI expansion slots to enable I/O customization.The SEL-3360E operates reliably in environments ranging from –40° to +60°C (–40° to +140°F) with no fans or forced airflow. Built and tested to utility substation standards, SEL-3360 Computers withstand up to 15 kV of electrostatic discharge, high electromagnetic interference and shock up to 15 g.“We are excited to add the SEL-3360E to the SEL-3360 family of computers, all of which offer a 10-year warranty,” said Dave Whitehead, SEL vice president of research and development. “SEL provides this no-questions-asked warranty to reflect the high level of reliability that we build into all of the products we manufacture.”Out-of-band remote management features, such as Intel Active Management Technology (AMT), reduce the time required to service SEL-3360 Computers. Users can perform diagnostics, install software or operating systems and even reboot remotely via a cryptographically secure interface. The SEL Backup and Recovery Tool (BaRT), a unique system monitor (SysMon) and an independent embedded controller (watchdog) help maximize system uptime by alerting users to potential issues and minimizing operational outages when a system failure occurs.SEL designs, manufactures, and tests all of its computers at its headquarters in Pullman, Washington. SEL-3360 Computers are cUL-certified, CE-marked and RoHS-compliant. The SEL-3360E is available now for only $3,350. For more information on its features, benefits and applications, visit www.selinc.com/p244.SEL serves the power industry worldwide through the design, manufacture, supply and support of products and services for power system protection, monitoring, control, automation, communications and metering. For more than 30 years, SEL has provided industry-leading performance in products and services, local technical support, a 10-year worldwide warranty and a commitment to making electric power safer, more reliable and more economical.
Back to Newsroom 
Featured Stories

Corporate

SEL Expands Manufacturing Operations in West Lafayette

Technical

SEL Achieves IEC 62443-2-4 Certification, Strengthening Cybersecurity Assurance for Critical-Infrastructure Customers

Press Release

SEL Continues to Expand Manufacturing Capacity With New Post Falls, Idaho Facility

  • SEL Expands Manufacturing Operations in Idaho with New Facility in Nampa
  • Idaho: Closing the Innovation Gap

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow