html{display:none} Software Downloads | Schweitzer Engineering Laboratories

Software Downloads


Filter
Model
Operating System
Categories
61 Results Found Current Page: 1 of 1

SEL-3355 Device Drivers and System Software

The SEL-3355 requires device drivers and software to be installed on the operating system in order for the devices, such as Ethernet, video, and audio devices, and the system Watchdog to function. Products shipped from the factory with an operating system installed already include all necessary drivers and software. Use the downloads below when installing your own operating system or to update existing software and drivers on your SEL-3355. Please read the installation instructions and release notes that are included in each download prior to installation.

SEL-3355-2 Drivers and Software, All

This package contains all device drivers and software for SEL-3355-2 computing platforms with Intel Xeon CPUs. Most 64-bit Windows operating systems are fully supported, while some Linux and 32-bit Windows operating systems are only partially supported (no SEL SysMon or Watchdog support). Contact SEL if you have questions about support for a specific operating system.

Version 20240116
Size 812.02 MB
Date Code 20240117

Verifying SEL Software Downloads

SEL-3355 Drivers and Software, All

This package contains all device drivers and software for SEL-3355 computing platforms with Intel i7 CPUs. Most 64-bit Windows operating systems are fully supported, while some Linux and 32-bit Windows operating systems are only partially supported (no SEL SysMon or Watchdog support). Contact SEL if you have questions about support for a specific operating system.

Size 568.95 MB
Date Code 20220713

Notes

Updated the following driver packages to the versions listed:

  • Intel Ethernet version 27.3 for Windows [8, 8.1, 10, 2012R2, 2016, 2019, 2022] x86-x64

Verifying SEL Software Downloads

SEL-3355 SATA Link Power Management Patch

This patch disables link power management, a power conservation function that is known to cause reliability issues with some solid-state drives (SSDs). Link power management provides little power-saving benefit in SEL-3355 computing platforms, and disabling the function has no negative impact on SEL-3355 operation. This patch is only applicable to SEL-3355 computing platforms with Windows operating systems in which the Intel serial ATA (SATA) driver is installed.

Size 161.23 kB
Date Code 20150409

Verifying SEL Software Downloads

SEL USB Driver

This driver enables USB communication between Windows computers and SEL USB ports for the following devices:

  • SEL-2440
  • SEL-3031
  • SEL-C662
  • SEL-C667
  • SEL-3021
  • SEL-9192
  • SEL-T4287

Installation Instructions

  1. Download the driver that corresponds to your version of Windows.
  2. Run the installer, if present, or follow the driver instructions.
  3. To see new COM port assignment, open Device Manager and expand Ports.
For Windows 11 operating systems.

Version R11.1.0.53
Size 1.88 MB
Date Code 20221007

Verifying SEL Software Downloads

For 32-bit and 64-bit Windows 10 operating systems. (Multi-language support)

Version R6.7.5
Size 3.58 MB
Date Code 20180515

Verifying SEL Software Downloads

For 32-bit and 64-bit Windows 8, Windows 7, Vista, and XP operating systems. (Multi-language Support)

Version R6.6.0.0
Size 3.56 MB
Date Code 20130215

Verifying SEL Software Downloads

SEL-3355 Firmware and BIOS Updates

These updates provide enhancements, bug fixes, and security updates to the firmware and BIOS embedded in the SEL-3355 system. Please read the installation instructions and release notes that are included in each download prior to installation.

SEL-3355-2 BIOS Update

This package contains the files necessary to update the BIOS in SEL-3355-2 computing platforms with Intel Xeon CPUs. This update contains a number of security updates, see the included ReleaseNotes.txt file for details.

Version 2.6
Size 56.42 MB
Date Code 20230913

Verifying SEL Software Downloads

SEL-3355-2 Intel Management Engine (ME) Firmware Update

This package includes the Intel Management Engine firmware and update tools as provided by Intel to update SEL-3355-2 computing platforms with Intel Xeon CPUs. It contains the latest security updates and bug fixes at the time of this release (see the README.txt file included in the download for more information). This update is not included in the BIOS update package and must be installed to ensure your computing platform's firmware is fully up to date. 

Version 11.8.93.4323
Size 277.97 MB
Date Code 20221115

Verifying SEL Software Downloads

SEL-3355 BIOS Update

This package contains the files necessary to update the BIOS in SEL-3355 Computers with Intel i7 CPUs. This update contains a number of enhancements, see the included ReleaseNotes.txt file for details.

Version 1.9
Size 5.57 MB
Date Code 20200206

Notes

  • Processor microcode updates to address Fallout, ZombieLoad/RIDL, and other security issues. See INTEL-SA-00233, CVE-2018-12126, CVE-2018-12127, CVE-2018-12130, CVE-2019-11091, and CVE-2019-0161 for more details.

Verifying SEL Software Downloads

SEL-3355 Intel Management Engine (ME) Firmware Update

This package includes the Intel Management Engine firmware and update tools as provided by Intel to update SEL-3355 computing platforms with Intel i7 CPUs. It contains the latest security updates and bug fixes at the time of this release (see the README.txt file included in the download for more information). This update is not included in the BIOS update package and must be installed to ensure your computing platform's firmware is fully up to date. 

Version 8.1.72.3002
Size 100.53 MB
Date Code 20180508

Notes

  • Intel released firmware update for the PCH in the SEL-3355 and SEL-3360 that addresses the AMT security vulnerabilities documented in CVE-2017-5711, CVE-2017-5712, CVE-2017-13077, CVE-2017-13078, and CVE-2017-13080.

Verifying SEL Software Downloads

128 GB and 256 GB SLC Solid State Drive (SSD) Firmware Update

This update is to address possible data corruption under certain high workloads when using certain 128 GB and 256 GB Industrial Grade SLC SSDs included in SEL-3355 and SEL-3360 computing platforms sold from 2015 to 2018. Please see the documentation included in this package to learn how to identify any of your SSDs that require this update.

Version 1.3
Size 66.86 MB
Date Code 20181003

Notes

  • Made changes to help prevent update application from getting interrupted and leaving SSD in a non-functioning state.
  • Added the revision 2b upgrade tool from Virtium, which attempts to recover an SSD left in a non-functioning state if a new update attempt on that SSD is started immediately after the failed attempt. The recovery uses data, stored in the log, about the last attempted update.
  • Same firmware update version 0502-001.

Verifying SEL Software Downloads

SEL-3332 Operating System Updates

Contains updates and modifications to the operating system environment. Please install any missing updates in the order in which they were released and carefully follow instructions if included with the update you download.

Microsoft Windows Security Update KB4500331

Updates SEL-3332 R3.X.X systems with Microsoft's Remote Desktop Security Update KB4500331 (CVE-2019-0708)

Version SEL-3332 All Versions
Size 736.23 kB
Date Code 20190523

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2017)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2017). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from July 2016 through June 2017, and includes the MS17-010 (KB4012598) Security Update previously released for the SEL-3332.

Microsoft Windows Security Updates (Spring 2016)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2016). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2016 through June 2016.

Microsoft Windows Security Updates (Fall 2015)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2015). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from July 2015 through December 2015.

Size 109.56 MB
Date Code 20160225

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2015)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2015). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2015 through June 2015.

Version SEL-3332 R304 versions
Size 19.74 MB
Date Code 20150805

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Fall 2014)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2014). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from June 2014 through December 2014.

Version SEL-3332 R304 versions
Size 10.42 MB
Date Code 20150226

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2014)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2014). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from October 2013 through May 2014.

Version SEL-3332 R304 versions
Size 9.66 MB
Date Code 20141002

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Fall 2013)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2013). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from May 2013 through October 2013.

Version SEL-3332 R304 versions
Size 54.30 MB
Date Code 20131227

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2013)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable DUA covering primarily July 2012 through May 2013. This update also updates the Foxit Reader.

Version SEL-3332 R304 versions
Size 64.74 MB
Date Code 20130731

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2012)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable DUA covering primarily November 2011 through June 2012. This update also installs the latest version of Foxit Reader.

Version SEL-3332 R304 versions
Size 32.50 MB
Date Code 20120827

Verifying SEL Software Downloads

MS12-020 Security Update (KB2621440)

Updates SEL-3332 R3.0.4 systems with Microsoft's Remote Desktop Security Update KB2621440.

Version SEL-3332 R3.0.4 VERSIONS ONLY
Size 776.73 kB
Date Code 20120402

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Fall 2011)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable DUA covering primarily April 2011 through November 2011 as well as some older, lower priority Microsoft Security Updates. This update also installs the Foxit Reader instead of Adobe Reader.

Version SEL-3332 R304 VERSIONS
Size 45.63 MB
Date Code 20120125

Verifying SEL Software Downloads

Microsoft Windows Security Updates (April 2011)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable DUA covering primarily August 2010 through April 2011 as well as some older, lower priority Microsoft Security Updates. We have also included two relevant Security Updates from Adobe Systems Incorporated.

Version SEL-3332 ALL VERSIONS
Size 72.20 MB
Date Code 20110525

Verifying SEL Software Downloads

Microsoft Windows Security Updates (August 2010)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable DUA covering January 2010 through August 2010. This update addresses the vulnerability discussed in NERC R-2010-09-13-01 (MS10-046).

Version SEL-3332 ALL VERSIONS
Size 35.61 MB
Date Code 20101022

Verifying SEL Software Downloads

Microsoft Windows Security Updates (January 2010)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable DUA covering August 2009 through January 2010.

Version SEL-3332 ALL VERSIONS
Size 16.41 MB
Date Code 20100301

Verifying SEL Software Downloads

MS08-067 Security Update (KB958644)

Updates all OS revisions with Microsoft's Patch Security Update KB958644.

Version SEL-3332 ALL VERSIONS
Size 776.73 kB
Date Code 20081027

Verifying SEL Software Downloads

Protected Storage sub-system Update (R3.0.3)

Updates OS revision 3.0.2 with an updated protected storage sub-system.

Version SEL-3332 OS R3.0.3
Size 7.63 MB
Date Code 20151102

Verifying SEL Software Downloads

Daylight-Saving Time Update (R3.0.2)

Updates OS revision 3.0.1 to handle the change to daylight-saving time that phases in March 11, 2007.

Version SEL-3332 OS R3.0.2
Size 645.73 kB
Date Code 20070207

Verifying SEL Software Downloads

SEL-3354 Security Updates

Contains updates and modifications to the operating system environment. Please install any missing updates in the order in which they were released and carefully follow instructions if included with the update you download.

Microsoft Windows Security Update KB4500331

Updates all Windows Embedded Standard SEL-3354 with Microsoft's Remote Desktop Security Update KB4500331 (CVE-2019-0708)

Version SEL-3354 With Windows Embedded Standard
Size 736.23 kB
Date Code 20190523

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Security Update 2018)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Security Update 2018). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2018 through January 2019. 

Microsoft announced on January 8, 2019, that it discontinued support for the Windows Embedded Standard operating system. This is the final Microsoft Windows Security Update for the SEL-3354. To receive future security updates, customers must upgrade to a newer operating system.

Version SEL-3354 With Windows Embedded Standard
Size 123.84 MB

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Fall 2017)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2017). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from June 2017 through December 2017. 

Version SEL-3354 With Windows Embedded Standard
Size 12.63 MB

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2017)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2017). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2016 through June 2017 and includes the MS17-010 (KB4012598) Security Update previously released for the SEL-3354.

Version SEL-3354 With Windows Embedded Standard
Size 61.44 MB

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Fall 2016)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2016). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from June 2016 through December 2016.

Version SEL-3354 With WindowsEmbedded Standard
Size 78.69 MB

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2016)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2016). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2016 through June 2016.

Version SEL-3354 With WindowsEmbedded Standard
Size 50.42 MB

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Fall 2015)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2015). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from July 2015 through December 2015.

Version SEL-3354 With Windows Embedded Standard
Size 59.38 MB
Date Code 20160225

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2015)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2015). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2015 through June 2015. This update also includes a security update from Adobe.

Version SEL-3354 With Windows Embedded Standard
Size 99.30 MB
Date Code 20150805

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Fall 2014)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2014). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from May 2014 through December 2014. This update also includes security updates for Adobe Reader and Silverlight.

Version SEL-3354 With Windows Embedded Standard
Size 214.41 MB
Date Code 20150226

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2014)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2014). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from October 2013 through May 2014. This update also includes security updates for Adobe Reader and Silverlight.

Version SEL-3354 With Windows Embedded Standard
Size 127.98 MB
Date Code 20141002

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Fall 2013)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2013). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from May 2013 through October 2013. We have also included relevant Security Updates from Adobe® Systems Incorporated.

Version SEL-3354 With Windows Embedded Standard
Size 79.23 MB
Date Code 20131227

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2013)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable executable covering primarily July 2012 through May 2013. This update also includes security updates for Adobe Reader and Silverlight.

Version SEL-3354 With Windows Embedded Standard
Size 108.32 MB
Date Code 20130731

Verifying SEL Software Downloads

Microsoft Windows Security Updates (Spring 2012)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable executable covering primarily November 2011 through June 2012. This update includes security updates for a few non-Operating System supporting software such as Adobe Reader and Silverlight.

Version SEL-3354 With Windows Embedded Standard
Size 288.33 MB
Date Code 20120827

Verifying SEL Software Downloads

MS12-020 Security Update (KB2621440)

Updates all Windows Embedded Standard SEL-3354 with KB2621440.

Version SEL-3354 With Windows Embedded Standard
Size 631.20 kB
Date Code 20120402

Verifying SEL Software Downloads

Microsoft Windows Security Updates (November 2011)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable executable covering primarily May 2011 through October 2011 as well as some older, lower priority Microsoft Security Updates. We have also included relevant Security Updates from Adobe Systems and the new .NET 4 Framework for Windows Embedded Standard.

Version SEL-3354 With Windows Embedded Standard
Size 467.91 MB
Date Code 20111123

Verifying SEL Software Downloads

Microsoft Windows Security Updates (April 2011)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable DUA covering primarily August 2010 through April 2011 as well as some older, lower priority Microsoft Security Updates. We have also included two relevant Security Updates from Adobe Systems Incorporated.

Version SEL-3354 With Windows Embedded Standard
Size 109.82 MB
Date Code 20110531

Verifying SEL Software Downloads

Microsoft Windows Security Updates (August 2010)

SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable installer covering January 2010 through August 2010. This update addresses the vulnerability discussed in NERC R-2010-09-13-01 (MS10-046).

Version SEL-3354 With Windows Embedded Standard
Size 46.42 MB
Date Code 20101022

Verifying SEL Software Downloads

SEL-3354 Silverlight

4.0.60531.0

This version of Silverlight for Windows Embedded Standard will update your current Silverlight 4.X version to 4.0.60531.0.

Version 4.0.60531.0
Size 5.99 MB
Date Code 20110830

Verifying SEL Software Downloads

SEL-3354 Ethernet Port

Microsoft Windows Ethernet Port Intel Teaming Upgrade

This package configures the rear ethernet ports to enable Intel Advanced Network Services (ANS) functionality, such as Teaming. This is only applicable to systems manufactured after May 2011 (serial number 1111350000 and higher). See the included readme.txt file for more information.

Version 1.1.49152.1
Size 40.90 MB
Date Code 20141216

Verifying SEL Software Downloads

Ubuntu Linux (64-bit) Ethernet Port Configuration

This package configures the rear ethernet ports to force 100 Mbps full-duplex operation. This should be applied to systems that have fiber-optic rear Ethernet ports or when connected to network devices that do not support autonegotiation of speed and duplex.

Version Ubuntu Linux (64-bit)
Size 166.73 kB

Verifying SEL Software Downloads

Ubuntu Linux (32-bit) Ethernet Port Configuration

This package configures the rear ethernet ports to force 100 Mbps full-duplex operation. This should be applied to systems that have fiber-optic rear Ethernet ports or when connected to network devices that do not support autonegotiation of speed and duplex.

Version Ubuntu Linux (32-bit)
Size 166.73 kB

Verifying SEL Software Downloads

SEL-3351 Operating System Updates

Contain updates and modifications to the operating system environment. Please install any missing updates in the order in which they were released and carefully follow instructions if included with the update you download.

MS08-067 Security Update (KB958644)

Updates all OS revisions with Microsoft's Patch with Security Update KB958644.

Daylight-Saving Time Update (R1.0.2)

Updates OS revisions 1.0.0—1.0.1 to handle the change to daylight-saving time that phases in March 11, 2007.

Version SEL-3351 OS R1.0.2
Size 520.00 kB
Date Code 20070207

Verifying SEL Software Downloads

System Control Monitor Updates

Contain updates to the watchdog, alarming, and time-acquisition processes.

Version R1.0.0.13
  SystemMonitor 1.1.1.2
  SystemControlMonitor 1.1.1.0
Size 611.23 kB
Date Code 20060110

Verifying SEL Software Downloads

SEL-3360 Device Drivers and System Software

The SEL-3360 requires device drivers and software to be installed on the operating system in order for the devices such as Ethernet, video, audio, and the system Watchdog to function. Products shipped from the factory with an operating system installed already include all necessary drivers and software. Use the downloads below when installing your own operating system or to update existing software and drivers on your SEL-3360. Please read the installation instructions and release notes that are included in each download prior to installation.

SEL-3360-2 Drivers and Software, All

This package contains all device drivers and software for SEL-3360-2 computing platforms with Intel Xeon CPUs. Most 64-bit Windows operating systems are fully supported, while some Linux and 32-bit Windows operating systems are only partially supported (no SEL SysMon or Watchdog support). Contact SEL if you have questions about support for a specific operating system.

Version 20240116
Size 812.02 MB
Date Code 20240117

Verifying SEL Software Downloads

SEL-3360 Drivers and Software, All

This package contains all device drivers and software for SEL-3360 computing platforms with Intel i7 CPUs. Most 64-bit Windows operating systems are fully supported, while some Linux and 32-bit Windows operating systems are only partially supported (no SEL SysMon or Watchdog support). Contact SEL if you have questions about support for a specific operating system.

Size 568.95 MB
Date Code 20220713

Notes

Updated the following driver packages to the versions listed:

  • Intel Ethernet version 27.3 for Windows [8, 8.1, 10, 2012R2, 2016, 2019, 2022] x86-x64

Verifying SEL Software Downloads

SEL-3360 SATA Link Power Management Patch

This patch disables link power management, a power conservation function that is known to cause reliability issues with some Solid State Drives (SSDs). Link power management provides little power saving benefit in SEL-3360 computing platforms, and disabling the function has no negative impact on SEL-3360 operation. This patch is only applicable to SEL-3360 computing platforms with Windows operating systems in which the Intel serial ATA (SATA) driver is installed.

Size 969.00 B
Date Code 20150409

Verifying SEL Software Downloads

SEL-3390E4 Drivers

The SEL-3390E4 requires device drivers to be installed on the operating system in order for the device to function. Select the download below that matches your operating system. Installation Instructions and Release Notes are included in each package. Operating systems not listed below are currently not supported.

SEL-3300 Driver Bundle for Microsoft Windows 10, Server 2016, Server 2019, and Server 2022

This bundle includes device drivers used in SEL computing platforms and PCIe expansion cards. This bundle also includes supporting software and utilities, such as SEL SysMon software.

Version 2.16.0.2
Size 43.29 MB
Date Code 20240401

Verifying SEL Software Downloads

SEL-3390E4 Driver for Microsoft Windows 7/8/8.1 and Server 2008R2/2012

This is an older version of the SEL-3390E4 driver for use with older versions of Microsoft Windows. For Windows 10 or Server 2016 or newer, use the SEL-3300 Driver Bundle.

Version 1.4
Size 67.01 MB
Date Code 20161128

Verifying SEL Software Downloads

SEL-3300 Driver Bundle for Linux CentOS 6/7, Red Hat 6/7/8/9, SUSE 15, and Ubuntu 16.04/18.04/20.04/22.04

This bundle includes device drivers for SEL Ethernet, serial, and time devices used in SEL computing platforms and PCIe expansion cards.

SEL provides repositories that can be used to install a selection of the packages in the download link below, including RHEL pre-compiled packages.  For more information, see the README at the following URL: https://cdn.selinc.com/repos/README.txt

Version 4.0.1.401
Size 149.14 MB
Date Code 20240207

Verifying SEL Software Downloads

SEL-3390E4 Driver for Linux CentOS 6

This is an older version of the SEL-3390E4 driver for use with CentOS 6.9 or earlier. For later versions of CentOS or any other Linux distribution, use the SEL-3300 Driver Bundle.

Version 1.4
Size 4.47 MB
Date Code 20190920

Verifying SEL Software Downloads

SEL-3390E4 Driver for VMware ESXi 8.0

This is the VMware certified and signed SEL-3390E4 Ethernet driver for use with VMware ESXi 8.0.

Version 1.0.0.247
Size 10.16 MB
Date Code 20240301

Verifying SEL Software Downloads

SEL-3390E4 Driver for VMware ESXi 7.0

This is the VMware certified and signed SEL-3390E4 Ethernet driver for use with VMware ESXi 7.0.

Version 1.0.0.247
Size 10.16 MB
Date Code 20240403

Verifying SEL Software Downloads

SEL-3390E4 Driver for VMware ESXi v6.7 Update 3

This driver is for use with VMWare ESXi Version 6.7 Update 3. Newer versions of VMWare ESXi are not currently supported.

Version 2.0
Size 10.12 MB
Date Code 20220919

Verifying SEL Software Downloads

SEL-3390E4 Driver for VMware ESXi v5.x

This driver is for use with VMWare ESXi Version 5.

Version 1.2
Size 2.00 MB
Date Code 20150701

Verifying SEL Software Downloads

SEL-5025 Secure Port Service

Secures serial communications using the SEL-3045 and SEL-3055

Notes

Version information: - [Cybersecurity] Updated the installer to protect against maliciously placed files.
- [Cybersecurity Enhancement] Enabled additional compiler features to help prevent the execution of malicious code.
- Updated a third-party driver for better Windows 10 and 11 compatibility.

Full Install

Version 1.0.3.4
Size 6.72 MB
Date Code 20231214

Verifying SEL Software Downloads

SEL-3351 Device Driver and System Software

The SEL-3351 requires device drivers and software to be installed on the operating system in order for the devices, such as Ethernet, video, and audio devices, and the system Watchdog to function. Products shipped from the factory with an operating system installed already include all necessary drivers and software. Use the downloads below when installing your own operating system or to update existing software and drivers on your SEL-3351.

SEL-3351 Drivers and Software, All

This package contains all SEL-3351 device drivers and software. Windows XP is fully supported, and some versions of Linux are also supported. Contact SEL if you have questions about support for a specific operating system.

Size 13.65 MB
Date Code 20140307

Verifying SEL Software Downloads

SEL-1102 Device Driver and System Software

The SEL-1102 requires device drivers and software to be installed on the operating system in order for the devices, such as Ethernet, video, and audio devices, and the system Watchdog to function. Products shipped from the factory with an operating system installed already include all necessary drivers and software. Use the downloads below when installing your own operating system or to update existing software and drivers on your SEL-1102.

SEL-1102 Drivers and Software, All

This package contains all SEL-1102 device drivers and software. Windows XP is fully supported, and some versions of Linux are also supported. Contact SEL if you have questions about support for a specific operating system.

Size 13.52 MB
Date Code 20140307

Verifying SEL Software Downloads

SEL-3354 Device Driver and System Software

The SEL-3354 requires device drivers and software to be installed on the operating system in order for the devices, such as Ethernet, video, and audio devices, and the system Watchdog to function. Products shipped from the factory with an operating system installed already include all necessary drivers and software. Use the downloads below when installing your own operating system or to update existing software and drivers on your SEL-3354.

SEL-3354 Drivers and Software, All

This package contains all SEL-3354 device drivers and software. Windows XP, 7, and Server 2008R2 are fully supported, and some versions of Linux are also supported. Contact SEL if you have questions about support for a specific operating system.

Size 204.88 MB
Date Code 20160721

Verifying SEL Software Downloads

SEL-3354 IRIG Driver

This package contains the installation files for the SEL-3354 IRIG Driver.

Version 1.1.4.0
Size 58.93 MB
Date Code 20160715

Notes

  • Addressed issue which in previous version caused the date to incorrectly be set to March 1st instead of February 29th of a leap year.
  • Modified IRIG device properties page in Windows 7 Device Manager to properly change settings without causing a system restart.
  • IRIG driver now prevents the year from being set incorrectly to 2000 when an IRIG-B002 source is connected.
  • Enhanced IRIG driver to include 64-bit Windows device properties page Settings tab.

Verifying SEL Software Downloads

SEL-3354 Firmware Updates

These updates provide enhancements, bug fixes, and security updates to the firmware embedded in the SEL-3354 system. Please see the instruction manual Appendix A for release notes.

SEL-3354 Firmware, Windows

This file updates the SEL-3354 firmware to the latest release for use with Microsoft Windows operating systems.

Version 1.1.3.0
Size 5.94 MB
Date Code 20140528

Verifying SEL Software Downloads

SEL-3354 Firmware, Linux

This file updates the SEL-3354 firmware to the latest release for use with Linux operating systems.

Version 2.0.3.0
Size 677.73 kB
Date Code 20110411

Verifying SEL Software Downloads

SEL-5056 Flow Controller—Windows

The SEL-5056 Software-Defined Network Flow Controller is software designed to optimize software-defined networking (SDN) configuration and management for critical infrastructure. The SEL-5056 Flow Controller is designed to work collectively with the SEL SDN switches to provide a complete traffic-engineering solution for Ethernet-based LANs. Traffic engineering with the SEL-5056 Flow Controller enables flexible configuration of each communications flow path and the ability to proactively engineer fault-tolerant networks, resulting in greater performance, improved reliability, and more deterministic packet delivery.

Full Install

Version 2.14.0
Size 89.18 MB
Date Code 20240228

Verifying SEL Software Downloads

USB Port Driver and Installation Instructions

This driver enables USB communication between Windows computers and SEL USB ports for the following devices:

  • SEL-311C
  • SEL-351
  • SEL-351A
  • SEL-351RS Kestrel
  • SEL-351S
  • SEL-651R
  • SEL-651RA
  • SEL-T400L
  • SEL-T401L
  • Installation Instructions

    1. Download zip directory and extract files.
    2. Open and follow installation instructions.
For Microsoft Windows operating systems.

Size 583.10 kB
Date Code 20220930

Verifying SEL Software Downloads

SEL-3600 USB Driver

Use the built-in front USB Port to connect locally with the Ethernet Security Gateway.

Installation Instructions

  1. Unzip the archive to a location on your computer.
  2. Connect the USB A-to-B cable to your computer and an SEL-36XX.
  3. Go to the Device Manager and find the device. Right click and select "Update Driver Software."
  4. Choose "Browse my computer for driver software in the pop-up window.
  5. Browse to the folder that you saved the archive contents to and select that folder. Click "Next."
  6. Click "Install" when prompted.
  7. Once the installer finishes you will see "SEL USB Ethernet/RNDIS Gadget" under Network Adapters in the Device Manager.
For Windows 7, and Windows 10 operating systems.

Version 1.0
Size 8.00 kB
Date Code 20170228

Verifying SEL Software Downloads

SEL-5051/5052 Client/Server Network Management System (NMS) Software

The SEL-5052 Server NMS software is used to manage SEL ICON networks in combination with the SEL-5051 Client Software.

SEL-5052 Server Network Management System (NMS) Software for ICON

This package contains the software installation package for the SEL-5052 Server NMS software.

Version 4.4.0.1
Size 457.53 MB

Verifying SEL Software Downloads

SEL-3390T Drivers

The SEL-3390T requires device drivers to be installed on the OS in order for the device to function. Select the download below that matches your OS. Installation Instructions and Release Notes are included in each package. OSs not listed below are currently not supported.

SEL-3300 Driver Bundle for Microsoft Windows 10, Server 2016, Server 2019, and Server 2022

This bundle includes device drivers used in SEL computing platforms and PCIe expansion cards. This bundle also includes supporting software and utilities, such as SEL SysMon software.

Version 2.16.0.2
Size 43.29 MB
Date Code 20240401

Verifying SEL Software Downloads

SEL-3300 Driver Bundle for Linux CentOS 6/7, Red Hat 6/7/8/9, SUSE 15, and Ubuntu 16.04/18.04/20.04/22.04

This bundle includes device drivers for SEL Ethernet, serial, and time devices used in SEL computing platforms and PCIe expansion cards.

SEL provides repositories that can be used to install a selection of the packages in the download link below, including RHEL pre-compiled packages.  For more information, see the README at the following URL: https://cdn.selinc.com/repos/README.txt

Version 4.0.1.401
Size 149.14 MB
Date Code 20240207

Verifying SEL Software Downloads

SEL-3390T Driver for VMware ESXi 8.0

This is the VMware signed SEL-3390T Ethernet driver for use with VMware ESXi 8.0.

Version 1.0.0.247
Size 10.16 MB
Date Code 20240301

Notes

This driver provides VMware ESXi 8.0 support for the Ethernet ports only, not IRIG-B or PTP hardware timestamping functionality.

Verifying SEL Software Downloads

SEL-3390T Driver for VMware ESXi 7.0

This is the VMware signed SEL-3390T Ethernet driver for use with VMware ESXi 7.0.

Version 1.0.0.247
Size 10.16 MB
Date Code 20240403

Notes

This driver provides VMware ESXi 7.0 support for the Ethernet ports only, not IRIG-B or PTP hardware timestamping functionality.

Verifying SEL Software Downloads

SEL-3350-1 Firmware and BIOS Updates

These updates provide enhancements, bug fixes, and security updates to the firmware and BIOS embedded in the SEL-3350 systems. Please read the installation instructions and release notes that are included in each download prior to installation.

SEL-3350-1 BIOS Update

This package contains the files necessary to update the BIOS in SEL-3350-1 computing platform with Intel Atom CPU. This update contains a number of security updates, see the included ReleaseNotes.txt file for details.

Version 1.3
Size 4.89 MB
Date Code 20230913

Verifying SEL Software Downloads

Blueframe OS

The Blueframe application platform rests on the Blueframe operating system and serves as its main user interface. The Linux-based Blueframe operating system offers basic hardware settings, such as display configuration.

Full Install

Version 1.8.0
Size 1.33 GB
Date Code 20231127

Verifying SEL Software Downloads

Connection Services

The Connection Services package is required for use with any DMA purchased package. This package includes Resource Management, which is the Blueframe application in which system resources are defined with their associated attributes and connection parameters. Other applications in the Blueframe ecosystem can use the Connection Services package to support resource interaction.

Full Install

Version 1.13.1
Size 197.20 MB
Date Code 20240112

Verifying SEL Software Downloads

Resource Communication Services

Resource Communication Services contains the communication services and automation execution logic to enable the proper fulfillment of DMA application plan configuration. Resource Communication Services also provides the communication layer for the Blueframe Direct Resource Access application.

Full Install

Version 1.16.3
Size 445.35 MB
Date Code 20240315

Verifying SEL Software Downloads

acSELerator QuickSet SEL-5030 Software

acSELerator QuickSet SEL-5030 Software is a tool for engineers and technicians to quickly and easily configure, commission, and manage devices for power system protection, control, metering, and monitoring. QuickSet Device Manager, included as a free, optional expansion pack, provides additional device management, control, and versioning capabilities.

Full Install

Version 7.3.1.0
Size 1.27 GB
Date Code 20240328

Verifying SEL Software Downloads

SEL Compass

SEL Compass goes beyond basic software updates to provide, among other offerings, a rich selection of meaningful literature, application guides, and general software products. Use the enhanced sorting capabilities to facilitate product planning, organize and distribute information, and learn about the many products SEL provides.

Full Install

Version 4.0.3.0
Size 23.96 MB
Date Code 20230828

Verifying SEL Software Downloads

acSELerator Architect Software

Architect configures and documents IEC 61850 systems that include GOOSE, Sampled Values, or Manufacturing Message Specification (MMS) for process bus or SCADA applications.

To configure SEL devices, download and install both Architect and the ICD Package.

Architect Install

Version 2.3.16.143
Size 42.19 MB
Date Code 20240304

Verifying SEL Software Downloads

ICD Package

Version 3.0.28.94
Size 10.74 MB
Date Code 20240409

Verifying SEL Software Downloads

acSELerator RTAC SEL-5033 Software

acSELerator RTAC is a graphical, easy-to-use tool that helps users quickly and easily configure the SEL-3530 Real-Time Automation Controller (RTAC).

Full Install

Version 1.36.152.9500
Size 1.51 GB
Date Code 20240328

Verifying SEL Software Downloads

Library Extensions

Version 4.24.3.0
Size 27.89 MB
Date Code 20240325

Verifying SEL Software Downloads

acSELerator Diagram Builder Software

The SEL Real-Time Automation Controller (RTAC) family of devices supports an optional web-based human-machine interface (HMI) system that is well-suited for use in substations and small processes. acSELerator Diagram Builder SEL-5035 Software is a Microsoft Windows application that enables the creation and management of HMI visualization projects for all of the RTACs in your system.

Diagram Builder

Version 3.8.0.58
Size 32.17 MB
Date Code 20240307

Verifying SEL Software Downloads

RTAC HMI Runtime Files

Version 3.8.0.58
Size 139.62 MB
Date Code 20240227

Verifying SEL Software Downloads

SEL-5806 Curve Designer Software

SEL-387E Relay Volts/Hertz User Curve Design Software.

Full Install

Version 1.3.0.0
Size 584.00 kB
Date Code 20160526

Verifying SEL Software Downloads

SEL-5020 Settings Assistant Software

Enter settings to and communicate with your SEL communications processors. Use to create a template for a new device.

Full Install

Version 3.60.4.0
Size 8.00 MB
Date Code 20190917

Verifying SEL Software Downloads

SEL-5010 Relay Assistant Software

Communicate with and manage SEL Relays across your system.

Full Install

Version 4.36.1.0
Size 70.91 MB
Date Code 20100202

Verifying SEL Software Downloads

SEL-5231 SEL Configuration API

Service that provides a programmatic interface to the acSELerator Database

Install

Version 3.1.15.0
Size 94.20 MB
Date Code 20231219

Verifying SEL Software Downloads

SEL-5037 Grid Configurator

SEL Grid Configurator is a freely distributed software tool for engineers and technicians to quickly and confidently create, manage, and deploy settings for SEL power system devices. It features a modern interface designed for ease of use, with powerful protection visualization and comprehensive reporting to reduce device deployment complexity. 

Notes

Please refer to Section 1 of the SEL Grid Configurator instruction manual to determine the appropriate installation type to use. 

SEL-5037 Grid Configurator Admin Install

Version 5.3.0.7
Size 989.06 MB
Date Code 20240402

Notes

This install requires administrator privileges to install.  SEL Grid Configurator will be available to all users on the computer.

Verifying SEL Software Downloads

SEL-5037 Grid Configurator User Install

Version 5.3.0.7
Size 836.94 MB
Date Code 20240402

Notes

This install does not require administrator privileges to install.  SEL Grid Configurator will only be available to the user that installed it.

Verifying SEL Software Downloads

Protocol Services

Protocol Services provides the functionality for configuring communications protocols data ingress (client) and egress (server) in the Blueframe application platform. This application provides communications data concentration among IEDs (resources) and protocol conversion for upstream SCADA, HMI, or other polling devices.

Full Install

Version 1.1.8
Size 366.29 MB
Date Code 20230912

Verifying SEL Software Downloads

SEL-5056 Flow Controller—Blueframe

The SEL-5056 Software-Defined Network Flow Controller is software designed to optimize software-defined networking (SDN) configuration and management for critical infrastructure. The SEL-5056 Flow Controller is designed to work collectively with the SEL SDN switches to provide a complete traffic-engineering solution for Ethernet-based LANs. Traffic engineering with the SEL-5056 Flow Controller enables flexible configuration of each communications flow path and the ability to proactively engineer fault-tolerant networks, resulting in greater performance, improved reliability, and more deterministic packet delivery.

Full Install

Version 2.13.0
Size 214.27 MB
Date Code 20230525

Verifying SEL Software Downloads

PDC Assistant Software

The SEL PDC Assistant software provides quick and easy commissioning for the SEL-5073 software PDC as well as SEL-3573 and SEL-3373 hardware PDCs.  Make settings in online or offline mode, monitor system status, export diagnostic logs and archives, and manage user accounts.

Full Install

Version 2.5.1.0
Size 76.83 MB
Date Code 20210225

Verifying SEL Software Downloads

acSELerator Team SEL-5045 Software

acSELerator Team automates the collection of power system data from multiple devices and stores these data in a central location for easy access. 

Trial downloads: Please read the TEAM_IS_TeamTrial.pdf document found in the extracted contents of the download for additional information.

Installs

Version DDC, EDT, TMS: 1.46.6.3; Sync: 2.3.10.0
Size 409.66 MB
Date Code 20231011

Verifying SEL Software Downloads

Data Management and Automation (DMA) Suite

Data Management and Automation (DMA) is a suite of applications designed to support automated data collection, management, normalization, and availability from critical infrastructure devices within the Blueframe application platform. DMA automates and accelerates the collection of oscillography, Sequence of Events (SOE), device settings, and property information. DMA applications also provide automated password rotation and streamline device audits through custom summary reports to identify device changes.

Configuration Monitoring

Configuration Monitoring is an optional DMA package that enables settings and device property data collection and viewing from supported devices. Within this package, you will find the Configuration Monitoring application, which is used for configuring the data collection plans, and Configuration Monitoring Archive, which is used for viewing assessments of collected data.

Version 1.11.0
Size 245.03 MB
Date Code 20231127

Verifying SEL Software Downloads

Credential Management

Credential Management is an optional DMA package that enables automated credential rotation with the use of an SEL Security Gateway and collection of the proxy reports. Within this package, you will find the Credential Management application, which is used for configuring the rotation and proxy report collection plans, and the Credential Management Archive, which is used for report creation and viewing related to resource credentials and their rotation schedule.

Version 1.11.0
Size 194.98 MB
Date Code 20240315

Verifying SEL Software Downloads

Custom Monitoring

Custom Monitoring is an optional DMA package that enables automated file or command result collection. Within this package, you will find the Custom Monitoring application, which is used for configuring the file or command result collection plans, and the Custom Monitoring Archive, which is used for viewing of the collected files or command results.

Version 1.5.0
Size 244.02 MB
Date Code 20231127

Verifying SEL Software Downloads

Disturbance Monitoring

Disturbance Monitoring is an optional DMA package that enables event and Sequence of Events (SOE) data collection and viewing from supported devices. Within this package, you will find the Disturbance Monitoring application, which is used for configuring the data collection plans, and Disturbance Monitoring Archive, which is used for viewing assessments of collected data.

Version 1.13.0
Size 255.41 MB
Date Code 20231127

Verifying SEL Software Downloads

DMA Tools

The DMA Tools package is included with any DMA package purchase and provides the DMA Diagnostics and DMA REST API applications. DMA Diagnostics provides troubleshooting, diagnostics, and system status information crucial for managing the sophisticated communications infrastructure that the automation system must transverse to gather device data. The DMA REST API provides read-only access to DMA collected data and logs. This application installed through this package provides documentation on the specific queries available for programmatic access to the data stored in the DMA private database.

Version 1.13.0
Size 190.76 MB
Date Code 20231127

Verifying SEL Software Downloads

Distribution Management System (DMS) Suite

The SEL Distribution Management System (DMS) suite is a collection of Blueframe applications that provide wide-area system control and management functionality while emphasizing simplicity, scalability, and security. The DMS suite will expand in capability over time. Its current functionality includes fault location, isolation, and service restoration (FLISR) and Power System Model (PSM). DMS FLISR uses near-real-time field data and automatically isolates faults and restores load from adjacent sources, maximizing system margin and minimizing switching. PSM creates the SEL DMS model from customer GIS data or manually created feeders and substations. 

FLISR

The FLISR application contains the run-time algorithms and simulation capabilities that are compatible with the SEL DMS suite. Feeder and Substation canvases deployed from within PSM (Power System Model) are visible when FLISR is launched from the Blueframe portal. When you view a canvas through the FLISR application, the canvas is populated with DNP3 data incoming from field device connections as well as status information from the FLISR algorithms. The feeder canvas can convey to the user what data FLISR is receiving and what events it is processing in real time, all within a web browser. FLISR supports voltage and fault event reconfiguration to include loss of source and open phase. Compatible with PSM v1.2.0+.

Version 2.1.0
Size 355.10 MB
Date Code 20240112

Verifying SEL Software Downloads

FLISR

The FLISR application contains the run-time algorithms and simulation capabilities that are compatible with the DMS suite. Feeder canvases deployed from within PSM (Power System Model) are visible when FLISR is launched from the Blueframe portal. When you view a feeder canvas through the FLISR application, the canvas is populated with DNP3 data incoming from field device connections as well as status information from the FLISR algorithms. The feeder canvas can convey to the user what data FLISR is receiving and what events it is processing in real time, all within a web browser. Compatible with PSM v1.0.0.

Version 2.0.0
Size 350.64 MB
Date Code 20230913

Verifying SEL Software Downloads

PSM (Power System Model)

PSM (Power System Model) provides a graphical configuration environment for SEL's DMS application suite, like FLISR. MDI (Model Data Import) is an additional application supplied with PSM that supports GIS model integration. These are designed to simplify and accelerate the creation of distribution models in SEL's DMS application suite by creating Substation and Feeder models. Compatible with FLISR v2.1.0.

Version 1.2.0
Size 172.79 MB
Date Code 20240112

Verifying SEL Software Downloads

PSM (Power System Model)

PSM (Power System Model) provides a graphical configuration environment for SEL's DMS application suite, like FLISR. MDI (Model Data Import) is an additional application supplied with PSM that supports GIS model integration. These are designed to simplify and accelerate the creation of distribution models in SEL's DMS application suite. Compatible with FLISR v2.0.0.

Version 1.0.0
Size 171.89 MB
Date Code 20230913

Verifying SEL Software Downloads

Data Viewer

The Data Viewer application displays the near real-time status of any data shared across the Blueframe platform. This rich environment gives end users, who are working in any number of applications within the Blueframe ecosystem, an easy way to see what values are being updated across the system. For example, any client or server added to Blueframe by the Protocol Services applications would be visible to the user, allowing for validation and additional troubleshooting to take place in this powerful tool.

Full Install

Version 1.0.8
Size 372.92 MB
Date Code 20231222

Verifying SEL Software Downloads

Resource Viewer

The Resource Viewer application displays the status information from device in Resource Manager. This application gives users a quick way to see summary data of many devices in a tabular format to get a quick system view of device states. Select a device and easily view more detailed information to help compliance and troubleshooting activities. The Resource Viewer currently support RTAC devices. Expanded device support coming soon!

Full Install

Version 1.3.0
Size 500.81 MB
Date Code 20231222

Verifying SEL Software Downloads

synchroWAVe Event Relay Event Visualization and Analysis Software

SEL-5601-2 synchroWAVe Event Software helps engineers diagnose a protective relay’s behavior during a power system fault. It is a powerful yet easy-to-use solution for displaying and analyzing SEL relay event reports and COMTRADE files.

Full Install

Version 1.9.1.80
Size 106.76 MB
Date Code 20240314

Verifying SEL Software Downloads

SubstationSERVER.NET

V1.51 SEL-3332 - Update from v1.38

DUA update package for use with the SEL-3332 Intelligent Server. Upgrades from v1.38 to v1.51.

Version 1.51
Size 38.47 MB
Date Code 20101001

Verifying SEL Software Downloads

V1.51 SEL-3332 - Update from v1.32

DUA update package for use with the SEL-3332 Intelligent Server. Upgrades from v1.32 to v1.51.

Version 1.51
Size 36.63 MB
Date Code 20101001

Verifying SEL Software Downloads

SEL-5705 Synchrowave Reports

SEL-5705 Synchrowave Reports automates power quality data analysis and report generation. It can be set to deliver daily or weekly reports via email to quickly identify harmonic disturbances and other power quality concerns.

Synchrowave Platform Installer

Version 2.6.0
Size 225.41 MB
Date Code 20230915

Verifying SEL Software Downloads

Synchrowave Reports Applications Package

Version 2.6.0
Size 467.99 MB
Date Code 20230915

Verifying SEL Software Downloads

SEL Software and Drivers

The SEL-3350-1 requires device drivers to be installed on the OS in order for the device to function. Select the download below that matches your OS. Installation Instructions and Release Notes are included in each package. OSs not listed below are currently not supported.

SEL-3300 Driver Bundle for Microsoft Windows 10, Server 2016, Server 2019, and Server 2022

This bundle includes device drivers used in SEL computing platforms and PCIe expansion cards. This bundle also includes supporting software and utilities, such as SEL SysMon software.

Version 2.16.0.2
Size 43.29 MB
Date Code 20240401

Verifying SEL Software Downloads

SEL-3300 Driver Bundle for Linux CentOS 6/7, Red Hat 6/7/8/9, SUSE 15, and Ubuntu 16.04/18.04/20.04/22.04

This bundle includes device drivers for SEL Ethernet, serial, and time devices used in SEL computing platforms and PCIe expansion cards.

SEL provides repositories that can be used to install a selection of the packages in the download link below, including RHEL pre-compiled packages.  For more information, see the README at the following URL: https://cdn.selinc.com/repos/README.txt

Version 4.0.1.401
Size 149.14 MB
Date Code 20240207

Verifying SEL Software Downloads

Intel HD Graphics 5xx Driver Installer for Microsoft Windows 10, Server 2019, and Server 2022

This driver provides extended graphics settings and features for the graphics processor on the SEL-3350. Installation instructions and release notes are included in each package.

Version 30.0.101.1960
Size 590.95 MB
Date Code 20220713

Verifying SEL Software Downloads

SEL-3350-1 Chipset Drivers for Microsoft Windows 10, Server 2019, and Server 2022

This package includes device drivers for the Intel Atom E3940 chipset devices in the SEL-3350-1. 

Version 1.0
Size 446.50 kB
Date Code 20220713

Notes

  • Initial Release
  • Intel Chipset driver version 10.1.17.1
  • Intel GPIO driver version 30.100.1750.1
  • Intel I2C driver version 30.100.1750.1
  • Intel TXEI driver version 3.0.0.1115

Verifying SEL Software Downloads

SEL-3060 Discovery Tool

This Windows-based tool is designed to easily find SEL-3060 Ethernet Radios and set their IP addresses. From the SEL-3060 Discovery Tool, users can connect to each device webpage for configuration of wireless settings.

Notes

The SEL-3060 Discovery Tool is designed for use with SEL-3060 Ethernet Radios only.

For 32-bit and 64-bit Windows Vista, Windows 7, Windows 8, and 64-bit Windows XP operating systems.

SEL-3060 Discovery Tool

Version 1.0.0.0
Size 484.00 kB
Date Code 20131210

Verifying SEL Software Downloads

SEL-5801 Cable Selector

Quickly and easily select proper SEL cables for your various applications. The SEL-5801 Cable Selector helps you select the right cable, with a user interface and database of standard SEL cables. The Cable Selector is available as a free download.

Full Install

Version 3.0.9.2
Size 5.56 MB
Date Code 20191210

Verifying SEL Software Downloads

SEL Virtual Port Software

Transform unsecured serial or legacy Ethernet communications on Windows computers to cryptographically secure channels by using SEL-5827 Virtual Connect Client or SEL-5828 Virtual Port Service Software. These applications are provided free by SEL to make remote SEL-3620 Ethernet Security Gateway ports available for existing software and terminal applications on your PC, including those using Modbus TCP/RTU.

Notes

The SEL Virtual Port Software family includes the following applications:

  • SEL-5827 Virtual Connect Client—Create a temporary serial COM port or Ethernet TCP port for engineering access applications with the SEL-3620 and SEL-3622 Security Gateways.
  • SEL-5828 Virtual Port Service—Create multiple persistent serial COM ports or Ethernet TCP ports for automation applications.
SEL-5828 Virtual Port Service

  • Create up to 128 persistent virtual COM ports and/or virtual TCP ports on a Windows PC, and send serial data over Raw TCP, Telnet, and Secure Shell Protocol (SSH) Ethernet protocols.
  • Use DSA or RSA 1024-bit encryption with SSH to ensure confidentiality and authenticity for serial or Ethernet data.
  • Quickly create virtual serial or Ethernet ports with a simple user interface.
Version 1.3.1.0
Size 3.12 MB
Date Code 20190226

Verifying SEL Software Downloads

SEL-5827 Virtual Connect Client

  • Enhance the communications security of existing engineering access software solutions, such as SEL-5010 Relay Assistant Software, SEL-5020 Settings Assistant Software, and GE EnerVista™ software by converting serial and unencrypted TCP data to SSH.
  • Run on isolated SEL computers—SEL virtual port software does not connect to the Internet or require a license to run.
  • Back up virtual port configurations for quick commissioning of new computers and redundancy.
  • Use the built-in terminal window to interact with remote devices’ command-line interface.
Version 1.3.0.0
Size 3.49 MB
Date Code 20160913

Verifying SEL Software Downloads

SEL-5891 Data Courier Configurator

Configure the SEL-4391 Data Courier.

Notes

The SEL-4391 is no longer available for purchase.

English Version

Version 1.0.5.0
Size 668.00 kB
Date Code 20100303

Verifying SEL Software Downloads

Español Version

Version 1.0.5.0
Size 804.00 kB
Date Code 20100303

Verifying SEL Software Downloads

SEL Backup and Recovery Tool (BaRT)

Use SEL BaRT to quickly and easily create a complete drive backup to capture your computing platform’s operating system and applications. Backups can be used for disaster recovery or to deploy a configured image across many similar systems. SEL BaRT was designed specifically for SEL’s computing platform line to ensure ease of use and compatibility with each platform’s features, including the system watchdog which is responsible for monitoring system availability.

SEL BaRT is custom-developed by SEL using open-source technology to be fast, portable, and free of charge. Back up a system drive in as little as 15 minutes, then, when needed, you can restore the backup image in even less time. Easily install SEL BaRT onto a USB drive using the included make_bart Windows and Linux installation tools. See the included README.TXT file for installation instructions. The included application guide AG2012-05 (also available for download) provides detailed installation and usage instructions.

SEL BaRT

Version 5.0.1.1
Size 139.64 MB
Date Code 20240328

Notes

The download will be in the form of a self-extracting executable with an .exe extension.  From a Windows OS, click on the file once downloaded and the files will extract similar to a .zip file.

Verifying SEL Software Downloads

SEL-3354 System Software

SEL System Monitor (SysMon)

The Windows SysMon is a front-end graphical user interface (GUI) and back-end Windows service (SEL Service).

Copy the setup.exe file to your SEL-3354 and as an administrator user run the setup program with the following arguments, depending on your Microsoft® operating system version.

Operating SystemInstallation Arguments
Windows XP Prosetup.exe /product=3354
Windows Embedded Standardsetup.exe /product=3354WES
Windows 2008 Server setup.exe /Product=3354 /D=C:\Windows\SysWOW64\SELShell
Version 2.1.8.0
  SEL Service 2.1.4.0
  SEL SysMon GUI 2.1.2.0
Size 589.91 kB
Date Code 20130204

Verifying SEL Software Downloads

SEL-5401 Test Software for SEL-4000

Full Install

Version 1.0.0.7
Size 2.51 MB
Date Code 20110223

Verifying SEL Software Downloads

The SEL-3390S8 requires device drivers to be installed on the operating system in order for the device to function. Select the download below that matches your operating system. Installation Instructions and Release Notes are included in each package. Operating systems not listed below are currently not supported.

SEL-3300 Driver Bundle for Microsoft Windows 10, Server 2016, Server 2019, and Server 2022

This bundle includes device drivers used in SEL computing platforms and PCIe expansion cards. This bundle also includes supporting software and utilities, such as SEL SysMon software.

Version 2.16.0.2
Size 43.29 MB
Date Code 20240401

Verifying SEL Software Downloads

SEL-3390S8 Driver for Microsoft Windows 7/8/8.1 and Server 2008R2/2012

This is an older version of the SEL-3390S8 driver for use with older versions of Microsoft Windows. For Windows 10 or Server 2016 or newer, use the SEL-3300 Driver Bundle.

Version 1.3
Size 18.66 MB
Date Code 20141104

Verifying SEL Software Downloads

SEL-3300 Driver Bundle for Linux CentOS 6/7, Red Hat 6/7/8/9, SUSE 15, and Ubuntu 16.04/18.04/20.04/22.04

This bundle includes device drivers for SEL Ethernet, serial, and time devices used in SEL computing platforms and PCIe expansion cards.

SEL provides repositories that can be used to install a selection of the packages in the download link below, including RHEL pre-compiled packages.  For more information, see the README at the following URL: https://cdn.selinc.com/repos/README.txt

Version 4.0.1.401
Size 149.14 MB
Date Code 20240207

Verifying SEL Software Downloads

SEL-3390S8 Driver for Linux RHEL\CentOS 6

This is an older version of the SEL-3390S8 driver for use with RHEL\CentOS 6.9 or earlier. For later versions of RHEL\CentOS or any other Linux distribution, use the SEL-3300 Driver Bundle.

Version 1.2
Size 211.73 kB
Date Code 20151110

Verifying SEL Software Downloads

SEL-3360 Firmware and BIOS Updates

These updates provide enhancements, bug fixes, and security updates to the firmware and BIOS embedded in the SEL-3360 system. Please read the installation instructions and release notes that are included in each download prior to installation.

SEL-3360-2 BIOS Update

This package contains the files necessary to update the BIOS in SEL-3360-2 computing platforms with Intel Xeon CPUs. This update contains a number of enhancements, see the included ReleaseNotes.txt file for details.

Version 2.6
Size 56.42 MB
Date Code 20230913

Verifying SEL Software Downloads

SEL-3360-2 Intel Management Engine (ME) Firmware Update

This package includes the Intel Management Engine firmware and update tools as provided by Intel to update SEL-3360-2 computing platforms with Intel Xeon CPUs. It contains the latest security updates and bug fixes at the time of this release (see the README.txt file included in the download for more information). This update is not included in the BIOS update package and must be installed to ensure your computing platform's firmware is fully up to date. 

Version 11.8.93.4323
Size 277.97 MB
Date Code 20221115

Verifying SEL Software Downloads

SEL-3360 BIOS Update

This package contains the files necessary to update the BIOS in SEL-3360 computing platforms with Intel i7 CPUs. This update contains a number of enhancements, see the included ReleaseNotes.txt file for details.

Version 1.9
Size 5.42 MB
Date Code 20200206

Notes

  • Processor microcode updates to address Fallout, ZombieLoad/RIDL, and other security issues. See INTEL-SA-00233, CVE-2018-12126, CVE-2018-12127, CVE-2018-12130, CVE-2019-11091, and CVE-2019-0161 for more details.

Verifying SEL Software Downloads

SEL-3360 Intel Management Engine (ME) Firmware Update

This package includes the Intel Management Engine firmware and update tools as provided by Intel to update SEL-3360 computing platforms with Intel i7 CPUs. It contains the latest security updates and bug fixes at the time of this release (see the README.txt file included in the download for more information). This update is not included in the BIOS update package and must be installed to ensure your computing platform's firmware is fully up to date.  

Version 8.1.72.3002
Size 104.98 MB
Date Code 20180508

Notes

  • Intel released firmware update for the PCH in the SEL-3355 and SEL-3360 that addresses the AMT security vulnerabilities documented in CVE-2017-5711, CVE-2017-5712, CVE-2017-13077, CVE-2017-13078, and CVE-2017-13080.

Verifying SEL Software Downloads

128 GB and 256 GB SLC Solid State Drive (SSD) Firmware Update

This update is to address possible data corruption under certain high workloads when using certain 128 GB and 256 GB Industrial Grade SLC SSDs included in SEL-3355 and SEL-3360 computing platforms sold from 2015 to 2018. Please see the documentation included in this package to learn how to identify any of your SSDs that require this update.

Version 1.3
Size 66.89 MB
Date Code 20181003

Verifying SEL Software Downloads

SEL-5057 Flow Auditor

STREAMLINE DATA COLLECTION FOR NERC CIP REPORTING

Use the SEL Flow Auditor application to streamline data collection for NERC CIP-007-6 R1 audit reporting. It collects network configurations from the SEL-5056 v2.7 or higher without the need for network scanning. With Flow Auditor, data collection takes minutes instead of days or weeks.

SEL-5057 Flow Auditor

The SEL-5057 requires an activation license.  Please contact SEL to obtain a 30-day demonstration license or to purchase an activation license.

Version 2.0.1.1
Size 147.95 MB
Date Code 20230725

Verifying SEL Software Downloads

SEL-2740S MIBs

This zip file contains the MIBs for the SEL-2740S.

SEL-2740S MIBs

Version R113
Size 39.96 kB

Verifying SEL Software Downloads

SEL-2742S MIBs

SEL-2742S MIBs

Version R112-V3
Size 40.21 kB

Verifying SEL Software Downloads

SEL-5051 Network Management System (NMS) Software

The SEL-5051 NMS software is used to manage SEL ICON networks in standalone mode or client mode when used with SEL-5052 Server software.

SEL-5051 Network Management System (NMS) Software for ICON

This package contains the software installation package for the SEL-5051 NMS software.

Version 4.4.0.1
Size 215.33 MB

Verifying SEL Software Downloads

McAfee Embedded Control Update

This update is to address security vulnerabilities in McAfee Embedded Control versions 8.3.2.133 or earlier, which is an optional software package that may be purchased on SEL Computing Platforms.

McAfee Embedded Control Update for Microsoft Windows 10, Server 2012R2, Server 2016, and Server 2019

Version 8.3.4.225
Size 86.15 MB

Notes

  • [Cybersecurity] Addresses CVE-2021-31833, Potential product security bypass vulnerability.

Verifying SEL Software Downloads

McAfee Embedded Control Update for Microsoft Windows 7 and Server 2008R2

Version 8.3.4.225
Size 75.02 MB

Notes

  • [Cybersecurity] Addresses CVE-2021-31833, Potential product security bypass vulnerability.

Verifying SEL Software Downloads

SEL-2731 MIBs

This zip file contains the MIBs for the SEL-2731.


Version R100-V1
Size 108.13 kB

Verifying SEL Software Downloads