The SEL-3355 requires device drivers and software to be installed on the operating system in order for the devices, such as Ethernet, video, and audio devices, and the system Watchdog to function. Products shipped from the factory with an operating system installed already include all necessary drivers and software. Use the downloads below when installing your own operating system or to update existing software and drivers on your SEL-3355. Please read the installation instructions and release notes that are included in each download prior to installation.
This package contains all device drivers and software for SEL-3355-2 computing platforms with Intel Xeon CPUs. Most 64-bit Windows operating systems are fully supported, while some Linux and 32-bit Windows operating systems are only partially supported (no SEL SysMon or Watchdog support). Contact SEL if you have questions about support for a specific operating system.
Version | 20240507 | |
---|---|---|
Size | 776.30 MB | |
Date Code | 20240507 |
This package contains all device drivers and software for SEL-3355 computing platforms with Intel i7 CPUs. Most 64-bit Windows operating systems are fully supported, while some Linux and 32-bit Windows operating systems are only partially supported (no SEL SysMon or Watchdog support). Contact SEL if you have questions about support for a specific operating system.
Size | 568.95 MB | |
---|---|---|
Date Code | 20220713 |
Updated the following driver packages to the versions listed:
This patch disables link power management, a power conservation function that is known to cause reliability issues with some solid-state drives (SSDs). Link power management provides little power-saving benefit in SEL-3355 computing platforms, and disabling the function has no negative impact on SEL-3355 operation. This patch is only applicable to SEL-3355 computing platforms with Windows operating systems in which the Intel serial ATA (SATA) driver is installed.
This driver enables USB communication between Windows computers and SEL USB ports for the following devices:
Installation Instructions
These updates provide enhancements, bug fixes, and security updates to the firmware and BIOS embedded in the SEL-3355 system. Please read the installation instructions and release notes that are included in each download prior to installation.
This package contains the files necessary to update the BIOS in SEL-3355-2 computing platforms with Intel Xeon CPUs. This update contains a number of security updates, see the included ReleaseNotes.txt file for details.
Version | 2.7 | |
---|---|---|
Size | 56.32 MB | |
Date Code | 20240507 |
This package includes the Intel Management Engine firmware and update tools as provided by Intel to update SEL-3355-2 computing platforms with Intel Xeon CPUs. It contains the latest security updates and bug fixes at the time of this release (see the README.txt file included in the download for more information). This update is not included in the BIOS update package and must be installed to ensure your computing platform's firmware is fully up to date.
Version | 11.8.95.4551 | |
---|---|---|
Size | 243.41 MB | |
Date Code | 20240507 |
This package contains the files necessary to update the BIOS in SEL-3355 Computers with Intel i7 CPUs. This update contains a number of enhancements, see the included ReleaseNotes.txt file for details.
Version | 1.9 | |
---|---|---|
Size | 5.57 MB | |
Date Code | 20200206 |
This package includes the Intel Management Engine firmware and update tools as provided by Intel to update SEL-3355 computing platforms with Intel i7 CPUs. It contains the latest security updates and bug fixes at the time of this release (see the README.txt file included in the download for more information). This update is not included in the BIOS update package and must be installed to ensure your computing platform's firmware is fully up to date.
Version | 8.1.72.3002 | |
---|---|---|
Size | 100.53 MB | |
Date Code | 20180508 |
This update is to address possible data corruption under certain high workloads when using certain 128 GB and 256 GB Industrial Grade SLC SSDs included in SEL-3355 and SEL-3360 computing platforms sold from 2015 to 2018. Please see the documentation included in this package to learn how to identify any of your SSDs that require this update.
Version | 1.3 | |
---|---|---|
Size | 66.86 MB | |
Date Code | 20181003 |
Contains updates and modifications to the operating system environment. Please install any missing updates in the order in which they were released and carefully follow instructions if included with the update you download.
Updates all Windows Embedded Standard SEL-3354 with Microsoft's Remote Desktop Security Update KB4500331 (CVE-2019-0708)
Version | SEL-3354 With Windows Embedded Standard | |
---|---|---|
Size | 736.23 kB | |
Date Code | 20190523 |
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Security Update 2018). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2018 through January 2019.
Microsoft announced on January 8, 2019, that it discontinued support for the Windows Embedded Standard operating system. This is the final Microsoft Windows Security Update for the SEL-3354. To receive future security updates, customers must upgrade to a newer operating system.
Version | SEL-3354 With Windows Embedded Standard | |
---|---|---|
Size | 123.84 MB |
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2017). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from June 2017 through December 2017.
Version | SEL-3354 With Windows Embedded Standard | |
---|---|---|
Size | 12.63 MB |
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2017). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2016 through June 2017 and includes the MS17-010 (KB4012598) Security Update previously released for the SEL-3354.
Version | SEL-3354 With Windows Embedded Standard | |
---|---|---|
Size | 61.44 MB |
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2016). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from June 2016 through December 2016.
Version | SEL-3354 With WindowsEmbedded Standard | |
---|---|---|
Size | 78.69 MB |
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2016). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2016 through June 2016.
Version | SEL-3354 With WindowsEmbedded Standard | |
---|---|---|
Size | 50.42 MB |
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2015). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from July 2015 through December 2015.
Version | SEL-3354 With Windows Embedded Standard | |
---|---|---|
Size | 59.38 MB | |
Date Code | 20160225 |
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2015). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from January 2015 through June 2015. This update also includes a security update from Adobe.
Version | SEL-3354 With Windows Embedded Standard | |
---|---|---|
Size | 99.30 MB | |
Date Code | 20150805 |
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2014). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from May 2014 through December 2014. This update also includes security updates for Adobe Reader and Silverlight.
Version | SEL-3354 With Windows Embedded Standard | |
---|---|---|
Size | 214.41 MB | |
Date Code | 20150226 |
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Spring 2014). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from October 2013 through May 2014. This update also includes security updates for Adobe Reader and Silverlight.
Version | SEL-3354 With Windows Embedded Standard | |
---|---|---|
Size | 127.98 MB | |
Date Code | 20141002 |
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable update, Microsoft Windows Security Updates (Fall 2013). This SEL update includes the relevant Security Updates for bulletins that Microsoft released from May 2013 through October 2013. We have also included relevant Security Updates from Adobe® Systems Incorporated.
Version | SEL-3354 With Windows Embedded Standard | |
---|---|---|
Size | 79.23 MB | |
Date Code | 20131227 |
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable executable covering primarily July 2012 through May 2013. This update also includes security updates for Adobe Reader and Silverlight.
Version | SEL-3354 With Windows Embedded Standard | |
---|---|---|
Size | 108.32 MB | |
Date Code | 20130731 |
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable executable covering primarily November 2011 through June 2012. This update includes security updates for a few non-Operating System supporting software such as Adobe Reader and Silverlight.
Version | SEL-3354 With Windows Embedded Standard | |
---|---|---|
Size | 288.33 MB | |
Date Code | 20120827 |
Updates all Windows Embedded Standard SEL-3354 with KB2621440.
Version | SEL-3354 With Windows Embedded Standard | |
---|---|---|
Size | 631.20 kB | |
Date Code | 20120402 |
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable executable covering primarily May 2011 through October 2011 as well as some older, lower priority Microsoft Security Updates. We have also included relevant Security Updates from Adobe Systems and the new .NET 4 Framework for Windows Embedded Standard.
Version | SEL-3354 With Windows Embedded Standard | |
---|---|---|
Size | 467.91 MB | |
Date Code | 20111123 |
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable DUA covering primarily August 2010 through April 2011 as well as some older, lower priority Microsoft Security Updates. We have also included two relevant Security Updates from Adobe Systems Incorporated.
Version | SEL-3354 With Windows Embedded Standard | |
---|---|---|
Size | 109.82 MB | |
Date Code | 20110531 |
SEL has combined the relevant Microsoft Security Update software for bulletins that Microsoft rated critical or important into a single downloadable installer covering January 2010 through August 2010. This update addresses the vulnerability discussed in NERC R-2010-09-13-01 (MS10-046).
Version | SEL-3354 With Windows Embedded Standard | |
---|---|---|
Size | 46.42 MB | |
Date Code | 20101022 |
This version of Silverlight for Windows Embedded Standard will update your current Silverlight 4.X version to 4.0.60531.0.
This package configures the rear ethernet ports to enable Intel Advanced Network Services (ANS) functionality, such as Teaming. This is only applicable to systems manufactured after May 2011 (serial number 1111350000 and higher). See the included readme.txt file for more information.
This package configures the rear ethernet ports to force 100 Mbps full-duplex operation. This should be applied to systems that have fiber-optic rear Ethernet ports or when connected to network devices that do not support autonegotiation of speed and duplex.
This package configures the rear ethernet ports to force 100 Mbps full-duplex operation. This should be applied to systems that have fiber-optic rear Ethernet ports or when connected to network devices that do not support autonegotiation of speed and duplex.
Contain updates and modifications to the operating system environment. Please install any missing updates in the order in which they were released and carefully follow instructions if included with the update you download.
Updates all OS revisions with Microsoft's Patch with Security Update KB958644.
Updates OS revisions 1.0.0—1.0.1 to handle the change to daylight-saving time that phases in March 11, 2007.
Version | SEL-3351 OS R1.0.2 | |
---|---|---|
Size | 520.00 kB | |
Date Code | 20070207 |
Contain updates to the watchdog, alarming, and time-acquisition processes.
Version | R1.0.0.13 | |
---|---|---|
SystemMonitor | 1.1.1.2 | |
SystemControlMonitor | 1.1.1.0 | |
Size | 611.23 kB | |
Date Code | 20060110 |
The SEL-3360 requires device drivers and software to be installed on the operating system in order for the devices such as Ethernet, video, audio, and the system Watchdog to function. Products shipped from the factory with an operating system installed already include all necessary drivers and software. Use the downloads below when installing your own operating system or to update existing software and drivers on your SEL-3360. Please read the installation instructions and release notes that are included in each download prior to installation.
This package contains all device drivers and software for SEL-3360-2 computing platforms with Intel Xeon CPUs. Most 64-bit Windows operating systems are fully supported, while some Linux and 32-bit Windows operating systems are only partially supported (no SEL SysMon or Watchdog support). Contact SEL if you have questions about support for a specific operating system.
Version | 20240507 | |
---|---|---|
Size | 776.30 MB | |
Date Code | 20240507 |
This package contains all device drivers and software for SEL-3360 computing platforms with Intel i7 CPUs. Most 64-bit Windows operating systems are fully supported, while some Linux and 32-bit Windows operating systems are only partially supported (no SEL SysMon or Watchdog support). Contact SEL if you have questions about support for a specific operating system.
Size | 568.95 MB | |
---|---|---|
Date Code | 20220713 |
Updated the following driver packages to the versions listed:
This patch disables link power management, a power conservation function that is known to cause reliability issues with some Solid State Drives (SSDs). Link power management provides little power saving benefit in SEL-3360 computing platforms, and disabling the function has no negative impact on SEL-3360 operation. This patch is only applicable to SEL-3360 computing platforms with Windows operating systems in which the Intel serial ATA (SATA) driver is installed.
The SEL-3390E4 requires device drivers to be installed on the operating system in order for the device to function. Select the download below that matches your operating system. Installation Instructions and Release Notes are included in each package. Operating systems not listed below are currently not supported.
This bundle includes device drivers used in SEL computing platforms and PCIe expansion cards. This bundle also includes supporting software and utilities, such as SEL SysMon software.
Version | 2.16.0.2 | |
---|---|---|
Size | 43.29 MB | |
Date Code | 20240401 |
This is an older version of the SEL-3390E4 driver for use with older versions of Microsoft Windows. For Windows 10 or Server 2016 or newer, use the SEL-3300 Driver Bundle.
This bundle includes device drivers for SEL Ethernet, serial, and time devices used in SEL computing platforms and PCIe expansion cards.
SEL provides repositories that can be used to install a selection of the packages in the download link below, including RHEL pre-compiled packages. For more information, see the README at the following URL: https://cdn.selinc.com/repos/README.txt
Version | 4.0.1.401 | |
---|---|---|
Size | 149.14 MB | |
Date Code | 20240207 |
This is an older version of the SEL-3390E4 driver for use with CentOS 6.9 or earlier. For later versions of CentOS or any other Linux distribution, use the SEL-3300 Driver Bundle.
This is the VMware certified and signed SEL-3390E4 Ethernet driver for use with VMware ESXi 8.0.
Version | 1.0.0.247 | |
---|---|---|
Size | 10.16 MB | |
Date Code | 20240301 |
This is the VMware certified and signed SEL-3390E4 Ethernet driver for use with VMware ESXi 7.0.
Version | 1.0.0.247 | |
---|---|---|
Size | 10.16 MB | |
Date Code | 20240403 |
This driver is for use with VMWare ESXi Version 6.7 Update 3. Newer versions of VMWare ESXi are not currently supported.
Secures serial communications using the SEL-3045 and SEL-3055
Version information: - [Cybersecurity] Updated the installer to protect against maliciously placed files.
- [Cybersecurity Enhancement] Enabled additional compiler features to help prevent the execution of malicious code.
- Updated a third-party driver for better Windows 10 and 11 compatibility.
The SEL-3351 requires device drivers and software to be installed on the operating system in order for the devices, such as Ethernet, video, and audio devices, and the system Watchdog to function. Products shipped from the factory with an operating system installed already include all necessary drivers and software. Use the downloads below when installing your own operating system or to update existing software and drivers on your SEL-3351.
This package contains all SEL-3351 device drivers and software. Windows XP is fully supported, and some versions of Linux are also supported. Contact SEL if you have questions about support for a specific operating system.
The SEL-1102 requires device drivers and software to be installed on the operating system in order for the devices, such as Ethernet, video, and audio devices, and the system Watchdog to function. Products shipped from the factory with an operating system installed already include all necessary drivers and software. Use the downloads below when installing your own operating system or to update existing software and drivers on your SEL-1102.
This package contains all SEL-1102 device drivers and software. Windows XP is fully supported, and some versions of Linux are also supported. Contact SEL if you have questions about support for a specific operating system.
The SEL-3354 requires device drivers and software to be installed on the operating system in order for the devices, such as Ethernet, video, and audio devices, and the system Watchdog to function. Products shipped from the factory with an operating system installed already include all necessary drivers and software. Use the downloads below when installing your own operating system or to update existing software and drivers on your SEL-3354.
This package contains all SEL-3354 device drivers and software. Windows XP, 7, and Server 2008R2 are fully supported, and some versions of Linux are also supported. Contact SEL if you have questions about support for a specific operating system.
This package contains the installation files for the SEL-3354 IRIG Driver.
Version | 1.1.4.0 | |
---|---|---|
Size | 58.93 MB | |
Date Code | 20160715 |
These updates provide enhancements, bug fixes, and security updates to the firmware embedded in the SEL-3354 system. Please see the instruction manual Appendix A for release notes.
This file updates the SEL-3354 firmware to the latest release for use with Microsoft Windows operating systems.
This file updates the SEL-3354 firmware to the latest release for use with Linux operating systems.
The SEL-5056 Software-Defined Network Flow Controller is software designed to optimize software-defined networking (SDN) configuration and management for critical infrastructure. The SEL-5056 Flow Controller is designed to work collectively with the SEL SDN switches to provide a complete traffic-engineering solution for Ethernet-based LANs. Traffic engineering with the SEL-5056 Flow Controller enables flexible configuration of each communications flow path and the ability to proactively engineer fault-tolerant networks, resulting in greater performance, improved reliability, and more deterministic packet delivery.
This driver enables USB communication between Windows computers and SEL USB ports for the following devices:
Installation Instructions
Use the built-in front USB Port to connect locally with the Ethernet Security Gateway.
Installation Instructions
The SEL-5052 Server NMS software is used to manage SEL ICON networks in combination with the SEL-5051 Client Software.
This package contains the software installation package for the SEL-5052 Server NMS software.
The SEL-3390T requires device drivers to be installed on the OS in order for the device to function. Select the download below that matches your OS. Installation Instructions and Release Notes are included in each package. OSs not listed below are currently not supported.
This bundle includes device drivers used in SEL computing platforms and PCIe expansion cards. This bundle also includes supporting software and utilities, such as SEL SysMon software.
Version | 2.16.0.2 | |
---|---|---|
Size | 43.29 MB | |
Date Code | 20240401 |
This bundle includes device drivers for SEL Ethernet, serial, and time devices used in SEL computing platforms and PCIe expansion cards.
SEL provides repositories that can be used to install a selection of the packages in the download link below, including RHEL pre-compiled packages. For more information, see the README at the following URL: https://cdn.selinc.com/repos/README.txt
Version | 4.0.1.401 | |
---|---|---|
Size | 149.14 MB | |
Date Code | 20240207 |
This is the VMware signed SEL-3390T Ethernet driver for use with VMware ESXi 8.0.
Version | 1.0.0.247 | |
---|---|---|
Size | 10.16 MB | |
Date Code | 20240301 |
This driver provides VMware ESXi 8.0 support for the Ethernet ports only, not IRIG-B or PTP hardware timestamping functionality.
This is the VMware signed SEL-3390T Ethernet driver for use with VMware ESXi 7.0.
Version | 1.0.0.247 | |
---|---|---|
Size | 10.16 MB | |
Date Code | 20240403 |
This driver provides VMware ESXi 7.0 support for the Ethernet ports only, not IRIG-B or PTP hardware timestamping functionality.
These updates provide enhancements, bug fixes, and security updates to the firmware and BIOS embedded in the SEL-3350 systems. Please read the installation instructions and release notes that are included in each download prior to installation.
This package contains the files necessary to update the BIOS in SEL-3350-1 computing platform with Intel Atom CPU. This update contains a number of security updates, see the included ReleaseNotes.txt file for details.
The Blueframe application platform rests on the Blueframe operating system and serves as its main user interface. The Linux-based Blueframe operating system offers basic hardware settings, such as display configuration.
The Connection Services package is required for use with any DMA purchased package. This package includes Resource Management, which is the Blueframe application in which system resources are defined with their associated attributes and connection parameters. Other applications in the Blueframe ecosystem can use the Connection Services package to support resource interaction.
Resource Communication Services contains the communication services and automation execution logic to enable the proper fulfillment of DMA application plan configuration. Resource Communication Services also provides the communication layer for the Blueframe Direct Resource Access application.
acSELerator QuickSet SEL-5030 Software is a tool for engineers and technicians to quickly and easily configure, commission, and manage devices for power system protection, control, metering, and monitoring. QuickSet Device Manager, included as a free, optional expansion pack, provides additional device management, control, and versioning capabilities.
SEL Compass goes beyond basic software updates to provide, among other offerings, a rich selection of meaningful literature, application guides, and general software products. Use the enhanced sorting capabilities to facilitate product planning, organize and distribute information, and learn about the many products SEL provides.
Architect configures and documents IEC 61850 systems that include GOOSE, Sampled Values, or Manufacturing Message Specification (MMS) for process bus or SCADA applications.
To configure SEL devices, download and install both Architect and the ICD Package.
acSELerator RTAC is a graphical, easy-to-use tool that helps users quickly and easily configure the SEL-3530 Real-Time Automation Controller (RTAC).
The SEL Real-Time Automation Controller (RTAC) family of devices supports an optional web-based human-machine interface (HMI) system that is well-suited for use in substations and small processes. acSELerator Diagram Builder SEL-5035 Software is a Microsoft Windows application that enables the creation and management of HMI visualization projects for all of the RTACs in your system.
SEL-387E Relay Volts/Hertz User Curve Design Software.
Enter settings to and communicate with your SEL communications processors. Use to create a template for a new device.
Service that provides a programmatic interface to the acSELerator Database
SEL Grid Configurator is a freely distributed software tool for engineers and technicians to quickly and confidently create, manage, and deploy settings for SEL power system devices. It features a modern interface designed for ease of use, with powerful protection visualization and comprehensive reporting to reduce device deployment complexity.
Please refer to Section 1 of the SEL Grid Configurator instruction manual to determine the appropriate installation type to use.
Version | 6.2.0.11 | |
---|---|---|
Size | 1,004.65 MB | |
Date Code | 20240702 |
This install requires administrator privileges to install. SEL Grid Configurator will be available to all users on the computer.
Version | 6.2.0.11 | |
---|---|---|
Size | 851.02 MB | |
Date Code | 20240702 |
This install does not require administrator privileges to install. SEL Grid Configurator will only be available to the user that installed it.
Protocol Services provides the functionality for configuring communications protocols data ingress (client) and egress (server) in the Blueframe application platform. This application provides communications data concentration among IEDs (resources) and protocol conversion for upstream SCADA, HMI, or other polling devices.
The SEL-5056 Software-Defined Network Flow Controller is software designed to optimize software-defined networking (SDN) configuration and management for critical infrastructure. The SEL-5056 Flow Controller is designed to work collectively with the SEL SDN switches to provide a complete traffic-engineering solution for Ethernet-based LANs. Traffic engineering with the SEL-5056 Flow Controller enables flexible configuration of each communications flow path and the ability to proactively engineer fault-tolerant networks, resulting in greater performance, improved reliability, and more deterministic packet delivery.
The SEL PDC Assistant software provides quick and easy commissioning for the SEL-5073 software PDC as well as SEL-3573 and SEL-3373 hardware PDCs. Make settings in online or offline mode, monitor system status, export diagnostic logs and archives, and manage user accounts.
acSELerator Team automates the collection of power system data from multiple devices and stores these data in a central location for easy access.
Trial downloads: Please read the TEAM_IS_TeamTrial.pdf document found in the extracted contents of the download for additional information.
Version | DDC, EDT, TMS: 1.46.6.3; Sync: 2.3.10.0 | |
---|---|---|
Size | 409.66 MB | |
Date Code | 20231011 |
Data Management and Automation (DMA) is a suite of applications designed to support automated data collection, management, normalization, and availability from critical infrastructure devices within the Blueframe application platform. DMA automates and accelerates the collection of oscillography, Sequence of Events (SOE), device settings, and property information. DMA applications also provide automated password rotation and streamline device audits through custom summary reports to identify device changes.
Configuration Monitoring is an optional DMA package that enables settings and device property data collection and viewing from supported devices. Within this package, you will find the Configuration Monitoring application, which is used for configuring the data collection plans, and Configuration Monitoring Archive, which is used for viewing assessments of collected data.
Credential Management is an optional DMA package that enables automated credential rotation with the use of an SEL Security Gateway and collection of the proxy reports. Within this package, you will find the Credential Management application, which is used for configuring the rotation and proxy report collection plans, and the Credential Management Archive, which is used for report creation and viewing related to resource credentials and their rotation schedule.
Custom Monitoring is an optional DMA package that enables automated file or command result collection. Within this package, you will find the Custom Monitoring application, which is used for configuring the file or command result collection plans, and the Custom Monitoring Archive, which is used for viewing of the collected files or command results.
Disturbance Monitoring is an optional DMA package that enables event and Sequence of Events (SOE) data collection and viewing from supported devices. Within this package, you will find the Disturbance Monitoring application, which is used for configuring the data collection plans, and Disturbance Monitoring Archive, which is used for viewing assessments of collected data.
The DMA Tools package is included with any DMA package purchase and provides the DMA Diagnostics and DMA REST API applications. DMA Diagnostics provides troubleshooting, diagnostics, and system status information crucial for managing the sophisticated communications infrastructure that the automation system must transverse to gather device data. The DMA REST API provides read-only access to DMA collected data and logs. This application installed through this package provides documentation on the specific queries available for programmatic access to the data stored in the DMA private database.
The SEL Distribution Management System (DMS) suite is a collection of Blueframe applications that provide wide-area system control and management functionality while emphasizing simplicity, scalability, and security. The DMS suite will expand in capability over time. Its current functionality includes fault location, isolation, and service restoration (FLISR) and Power System Model (PSM). DMS FLISR uses near-real-time field data and automatically isolates faults and restores load from adjacent sources, maximizing system margin and minimizing switching. PSM creates the SEL DMS model from customer GIS data or manually created feeders and substations.
The FLISR application contains the run-time algorithms and simulation capabilities that are compatible with the SEL DMS suite. Feeder and Substation canvases deployed from within PSM (Power System Model) are visible when FLISR is launched from the Blueframe portal. When you view a canvas through the FLISR application, the canvas is populated with DNP3 data incoming from field device connections as well as status information from the FLISR algorithms. The feeder canvas can convey to the user what data FLISR is receiving and what events it is processing in real time, all within a web browser. FLISR supports voltage and fault event reconfiguration to include loss of source and open phase. Compatible with PSM v1.2.0+.
The FLISR application contains the run-time algorithms and simulation capabilities that are compatible with the DMS suite. Feeder canvases deployed from within PSM (Power System Model) are visible when FLISR is launched from the Blueframe portal. When you view a feeder canvas through the FLISR application, the canvas is populated with DNP3 data incoming from field device connections as well as status information from the FLISR algorithms. The feeder canvas can convey to the user what data FLISR is receiving and what events it is processing in real time, all within a web browser. Compatible with PSM v1.0.0.
PSM (Power System Model) provides a graphical configuration environment for SEL's DMS application suite, like FLISR. MDI (Model Data Import) is an additional application supplied with PSM that supports GIS model integration. These are designed to simplify and accelerate the creation of distribution models in SEL's DMS application suite by creating Substation and Feeder models. Compatible with FLISR v2.1.0.
PSM (Power System Model) provides a graphical configuration environment for SEL's DMS application suite, like FLISR. MDI (Model Data Import) is an additional application supplied with PSM that supports GIS model integration. These are designed to simplify and accelerate the creation of distribution models in SEL's DMS application suite. Compatible with FLISR v2.0.0.
The Data Viewer application displays the near real-time status of any data shared across the Blueframe platform. This rich environment gives end users, who are working in any number of applications within the Blueframe ecosystem, an easy way to see what values are being updated across the system. For example, any client or server added to Blueframe by the Protocol Services applications would be visible to the user, allowing for validation and additional troubleshooting to take place in this powerful tool.
The Resource Viewer application displays the status information from device in Resource Manager. This application gives users a quick way to see summary data of many devices in a tabular format to get a quick system view of device states. Select a device and easily view more detailed information to help compliance and troubleshooting activities. The Resource Viewer currently support RTAC devices. Expanded device support coming soon!
SEL-5601-2 synchroWAVe Event Software helps engineers diagnose a protective relay’s behavior during a power system fault. It is a powerful yet easy-to-use solution for displaying and analyzing SEL relay event reports and COMTRADE files.
Use SEL BaRT to quickly and easily create a complete drive backup to capture your computing platform’s operating system and applications. Backups can be used for disaster recovery or to deploy a configured image across many similar systems. SEL BaRT was designed specifically for SEL’s computing platform line to ensure ease of use and compatibility with each platform’s features, including the system watchdog which is responsible for monitoring system availability.
SEL BaRT is custom-developed by SEL using open-source technology to be fast, portable, and free of charge. Back up a system drive in as little as 15 minutes, then, when needed, you can restore the backup image in even less time. Easily install SEL BaRT onto a USB drive using the included make_bart Windows and Linux installation tools. See the included README.TXT file for installation instructions. The included application guide AG2012-05 (also available for download) provides detailed installation and usage instructions.
Version | 5.0.1.1 | |
---|---|---|
Size | 139.64 MB | |
Date Code | 20240328 |
The download will be in the form of a self-extracting executable with an .exe extension. From a Windows OS, click on the file once downloaded and the files will extract similar to a .zip file.
These updates provide enhancements, bug fixes, and security updates to the firmware and BIOS embedded in the SEL-3360 system. Please read the installation instructions and release notes that are included in each download prior to installation.
This package contains the files necessary to update the BIOS in SEL-3360-2 computing platforms with Intel Xeon CPUs. This update contains a number of enhancements, see the included ReleaseNotes.txt file for details.
Version | 2.7 | |
---|---|---|
Size | 56.32 MB | |
Date Code | 20240507 |
This package includes the Intel Management Engine firmware and update tools as provided by Intel to update SEL-3360-2 computing platforms with Intel Xeon CPUs. It contains the latest security updates and bug fixes at the time of this release (see the README.txt file included in the download for more information). This update is not included in the BIOS update package and must be installed to ensure your computing platform's firmware is fully up to date.
Version | 11.8.95.4551 | |
---|---|---|
Size | 243.41 MB | |
Date Code | 20240507 |
This package contains the files necessary to update the BIOS in SEL-3360 computing platforms with Intel i7 CPUs. This update contains a number of enhancements, see the included ReleaseNotes.txt file for details.
Version | 1.9 | |
---|---|---|
Size | 5.42 MB | |
Date Code | 20200206 |
This package includes the Intel Management Engine firmware and update tools as provided by Intel to update SEL-3360 computing platforms with Intel i7 CPUs. It contains the latest security updates and bug fixes at the time of this release (see the README.txt file included in the download for more information). This update is not included in the BIOS update package and must be installed to ensure your computing platform's firmware is fully up to date.
Version | 8.1.72.3002 | |
---|---|---|
Size | 104.98 MB | |
Date Code | 20180508 |
This update is to address possible data corruption under certain high workloads when using certain 128 GB and 256 GB Industrial Grade SLC SSDs included in SEL-3355 and SEL-3360 computing platforms sold from 2015 to 2018. Please see the documentation included in this package to learn how to identify any of your SSDs that require this update.
The SEL-3350-1 requires device drivers to be installed on the OS in order for the device to function. Select the download below that matches your OS. Installation Instructions and Release Notes are included in each package. OSs not listed below are currently not supported.
This bundle includes device drivers used in SEL computing platforms and PCIe expansion cards. This bundle also includes supporting software and utilities, such as SEL SysMon software.
Version | 2.16.0.2 | |
---|---|---|
Size | 43.29 MB | |
Date Code | 20240401 |
This bundle includes device drivers for SEL Ethernet, serial, and time devices used in SEL computing platforms and PCIe expansion cards.
SEL provides repositories that can be used to install a selection of the packages in the download link below, including RHEL pre-compiled packages. For more information, see the README at the following URL: https://cdn.selinc.com/repos/README.txt
Version | 4.0.1.401 | |
---|---|---|
Size | 149.14 MB | |
Date Code | 20240207 |
This driver provides extended graphics settings and features for the graphics processor on the SEL-3350. Installation instructions and release notes are included in each package.
This package includes device drivers for the Intel Atom E3940 chipset devices in the SEL-3350-1.
Version | 1.0 | |
---|---|---|
Size | 446.50 kB | |
Date Code | 20220713 |
DUA update package for use with the SEL-3332 Intelligent Server. Upgrades from v1.38 to v1.51.
DUA update package for use with the SEL-3332 Intelligent Server. Upgrades from v1.32 to v1.51.
SEL-5705 Synchrowave Reports automates power quality data analysis and report generation. It can be set to deliver daily or weekly reports via email to quickly identify harmonic disturbances and other power quality concerns.
Quickly and easily select proper SEL cables for your various applications. The SEL-5801 Cable Selector helps you select the right cable, with a user interface and database of standard SEL cables. The Cable Selector is available as a free download.
Transform unsecured serial or legacy Ethernet communications on Windows computers to cryptographically secure channels by using SEL-5827 Virtual Connect Client or SEL-5828 Virtual Port Service Software. These applications are provided free by SEL to make remote SEL-3620 Ethernet Security Gateway ports available for existing software and terminal applications on your PC, including those using Modbus TCP/RTU.
The SEL Virtual Port Software family includes the following applications:
This zip file contains the MIBs for the SEL-2740S.
The SEL-5051 NMS software is used to manage SEL ICON networks in standalone mode or client mode when used with SEL-5052 Server software.
This package contains the software installation package for the SEL-5051 NMS software.
This zip file contains the MIBs for the SEL-2731.