Schweitzer Engineering Laboratories

Newsroom

Jan 29, 2026

SEL Releases New Transformer Controller With LTC Control

PULLMAN, Washington—Schweitzer Engineering Laboratories (SEL), a global leader in power system protection, automation and control solutions, has released a new controller for transformers that delivers thermal and voltage regulation in a single device. The SEL-2414 Transformer Automation Controller (TAC) is built on the same proven hardware as the original thermal-monitoring device and now includes functionality for load tap changer (LTC) control. It is an efficient and economical solution that extends the lifespan of transformers and optimizes power system performance.  The SEL-2414 allows users to:
  • Reduce energy losses and maintain bus voltages within acceptable limits.
  • Optimize performance for changing load conditions, power flow directions, seasonal variations and network demands.
  • Prevent transformer overloading by controlling transformers operating in parallel.
  • Extend the lifespan of a transformer by using IEEE or IEC thermal modeling and cooling stage control.
Customers have the option to specify the SEL-2414 with a new transformer installation or to purchase an LTC license to add functionality to an existing SEL-2414. Optional adapter plates are available to replace controllers from other manufacturers.Designed, manufactured and tested in the United States, every SEL-2414 is engineered to withstand the harshest environments. The SEL-2414 is backed by a ten-year, worldwide warranty and comes with no-cost SEL technical support.Visit the SEL-2414 webpage to learn more.
Back to Newsroom 
Featured Stories

Press Release

Two SEL Leaders Honored by the Manufacturing Institute

Technical

SEL and Puget Sound Energy Collaborate With Customers for Community Microgrid

Press Release

SEL Begins Work on New Electronic Device Manufacturing Facility in Moscow, Idaho

  • SEL Executive Vice President Elected Chair of the Board of Directors of ESCA
  • SEL President Appointed to the Federal Reserve Bank of San Francisco Economic Advisory Council

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow