Schweitzer Engineering Laboratories

Newsroom

Feb 16, 2024

New to FLISR—Automatic Configuration Using GIS Data

SEL recently introduced several enhancements to the Fault Location, Isolation, and Service Restoration (FLISR) application package on the SEL Blueframe platform.Users can now automatically configure FLISR systems using geographic information system (GIS) data.This update represents the next evolution in simplicity for FLISR. One major benefit is that GIS integration makes it easier to scale to and regularly update large systems with hundreds to thousands of feeders.As part of this release, SEL is introducing two new apps to Blueframe: Model Data Import (MDI) and Power System Model (PSM). Users will import GIS data with the MDI app and configure their model with the PSM app.SEL has incorporated feedback from FLISR users to provide an enhanced graphical configuration interface with PSM. This app keeps configuration simple and minimizes the potential for introducing errors while configuring the model for a FLISR system.In addition to supporting FLISR, the MDI and PSM apps will enable other Distribution Management System (DMS) applications and advanced solutions in the future.FLISR on SEL Blueframe is a software solution that enables power systems to rapidly detect permanent faults and restore service to unaffected portions of feeders—which helps reduce customer outages and improve reliability metrics. With features such as GIS integration, FLISR on SEL Blueframe is redefining simplicity in distribution automation.Watch an on-demand webinar to learn more.Read more about FLISR on SEL Blueframe.
Back to Newsroom 
Featured Stories

Press Release

SEL Names New Vice President of Sales and Customer Service

Press Release

SEL Names New Vice President of Engineering Services

Corporate

SEL Founder Urges Civic Engagement and Civility at Pullman Chamber Luncheon

  • SEL supports ambitious grid modernization project in Central America
  • Employee Owners Do More Than Show Up — We Build Things Better

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow