Schweitzer Engineering Laboratories

Newsroom

Apr 24, 2024

Introducing the SEL-TWFL Dual Traveling-Wave Fault Locator and 12-Channel MHz Recorder

Schweitzer Engineering Laboratories (SEL), a global leader in power system protection, automation, and control solutions, introduced the SEL-TWFL Dual Traveling-Wave Fault Locator and 12-Channel MHz Recorder, a standalone device that provides accurate fault locating, line monitoring and high-resolution event recording.     The device uses traveling-wave- and impedance-based methods to accurately locate faults within one tower span. The combination of these methods provides unmatched fault-locating accuracy and dependability for a variety of operating conditions and fault types. Like the SEL-T401L Ultra-High-Speed Line Relay, the SEL-TWFL includes line-monitoring functionality that localizes early traveling-wave activity to address potential line problems. In addition, the SEL-TWFL can monitor two lines from a single substation and is suitable for radial, two- and three-terminal applications. The device works with series-compensated lines, overhead lines, cable lines and hybrid transmission lines. For multi-ended fault-locating methods, SEL-TWFL devices exchange data over a communications channel or via communications protocols over a SCADA network. The SEL-TWFL reports fault locations locally or at a central location using a client computer.With its ultra-high sampling rate capability, the SEL-TWFL collects data from as many as six currents and six voltages for as long as 1.2 seconds at a 1 MHz sampling rate with 18 bits of resolution. This data offers an enhanced understanding of power system high-frequency transients from faults, switching events, breaker restrikes and self-extinguishing faults.The SEL-TWFL draws from 40 years of SEL innovation and field experience locating faults in power systems around the world. This device joins a long line of fault-locating technology, from the earliest SEL products, like the SEL-21, SEL-LFL and SEL-321, to available products, like the SEL-421, SEL-411L, SEL-T400L and SEL-T401L. As a nod to the original devices in this product family, the SEL-TWFL sports a silver faceplate like those used in the SEL-21 and SEL-LFL.“We’re excited to be launching the SEL-TWFL,” said CEO Dave Whitehead. “With this technology, customers can reduce the time and effort spent locating faults, while increasing their understanding of events occurring on a variety of line types and benefitting from line monitoring.” The SEL-TWFL is now available to order. Visit the SEL website to learn more: selinc.com/products/twfl
Back to Newsroom 
Featured Stories

Press Release

SEL Announces 2026–2027 Scholarship Program Recipients

Technical

SEL Fault Indicators and Sensors Now Feature the LINAM Name

Press Release

SEL Raises Starting Hourly Wage to $21.50

  • Two SEL Leaders Honored by the Manufacturing Institute
  • SEL and Puget Sound Energy Collaborate With Customers for Community Microgrid

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow