Schweitzer Engineering Laboratories

Newsroom

Feb 8, 2023

New OT SDN Switch Increases Speed, Port Count

SEL recently expanded its operational technology (OT) software-defined networking (SDN) switch portfolio with the introduction of the SEL-2741, a premium OT SDN Ethernet switch. This new 19-inch, 1U rack-mount switch builds on the success of the SEL-2740S Software-Defined Network Switch and incorporates feedback we’ve received from users. It offers more and faster Ethernet ports and supports SEL or third-party small form-factor pluggable (SFP) transceivers.  Features include: 
  • 24 ports that can run Fast Ethernet or Gigabit speeds. 
  • Integration of the digital inputs found on the SEL-2742S Software-Defined Network Switch. 
  • SFP support, which provides the microflexibility of fiber options. The switch supports SEL and third-party SFPs with simple hot-swappable plug-and-play capability. 
  • A convenient place on the front panel for a configurable name label.  
The SEL-2741 provides the same reliability and capabilities as the SEL-2740S, without an increase in price. These features include large flow table sizes, broad OpenFlow capabilities, detailed alarm and activity indicators, redundant power supplies, Precision Time Protocol (PTP) transparent clock support, a Form C alarm contact and full compliance with standards such as IEEE 1613 and IEC 61850-3. The SEL-2741 is integrated into the SEL-5056 Software-Defined Network Flow Controller (version 2.12 or higher), offering the same seamless network engineering as the SEL-2740S. Learn more about the SEL-2741 Ethernet Switch.
Back to Newsroom 
Featured Stories

Press Release

SEL Announces New Vice President of Sales and Customer Service

SEL In The News

Pullman School District Sale of Aquatic Center to SEL Finalized

Press Release

SEL Names New Vice President of Sales and Customer Service

  • SEL Names New Vice President of Engineering Services
  • SEL Founder Urges Civic Engagement and Civility at Pullman Chamber Luncheon

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow