Schweitzer Engineering Laboratories

Newsroom

Aug 12, 2021

New SEL-3390T Time and Ethernet Adapter Card for SEL Automation Controllers

Now available, the SEL-3390T Time and Ethernet Adapter Card is a PCI Express (PCIe) expansion card that adds precise time synchronization and distribution functionality to SEL automation and computing devices such as the SEL-3355 and SEL-3360 Automation Controllers. It provides two Ethernet ports, one BNC input and one BNC output, allowing customers to source and distribute time from IRIG-B and Ethernet devices without the need for cable adapters. Benefits of the SEL-3390T include:
  • Direct BNC input and output connections for IRIG-B.
  • RJ45 and small form-factor pluggable (SFP) Ethernet port configuration options.
  • Time synchronization of different IEDs and end devices within the substation.
  • Precise time synchronization over Ethernet.
  • Accurate synchronization of data communications.
It is easy to install the SEL-3390T card into existing SEL-3355 and SEL-3360E Automation Controllers or order these automation controllers with the card preconfigured. To learn more about the SEL-3390T, visit the product webpage.
Back to Newsroom 
Featured Stories

Technical

SEL Releases New Transformer Controller With LTC Control

Press Release

SEL President Appointed to the Federal Reserve Bank of San Francisco Economic Advisory Council

Press Release

SEL Announces New Vice President of Sales and Customer Service

  • Pullman School District Sale of Aquatic Center to SEL Finalized
  • SEL Names New Vice President of Sales and Customer Service

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow