Schweitzer Engineering Laboratories

Newsroom

Jul 29, 2021

SEL Refreshes SEL-2414 Transformer Monitor and Expands Its Capabilities

Schweitzer Engineering Laboratories has released numerous enhancements for the SEL-2414 Transformer Monitor, further expanding its abilities to manage and protect critical substation assets.The SEL-2414 now supports the IEC 60076-7 thermal model, providing an alternative to its existing IEEE C57.91 thermal model. The IEC thermal model accounts for overshoot in hot spots and is more accurate with varying loads.The monitor’s new 14-digital-input card supports load tap position and control monitoring. Using predefined I/O with the function block, users can ensure transformer output voltage is stable and that load tap changers (LTCs) are healthy.To make using the transformer monitor easier, several new features were also developed. These include an acSELerator QuickSet SEL-5030 Software template for transformer nameplate and test data settings, SELogic templates for improved load tap change control and a list of preferred configurations for fan control. In addition, users can now upgrade firmware over Ethernet.Two new communications protocols are now available with the SEL-2414 as well: IEC 61850 Edition 2 and the IEC 62439 Parallel Redundancy Protocol. These protocols increase flexibility for SCADA and distributed control system integration and enhance reliability for communications links.To learn more, visit the product webpage.
Back to Newsroom 
Featured Stories

Press Release

SEL Advances Development of Investigational Autism Screening Device, Launches Clinical Trial

Press Release

SEL Names New VP of Marketing and SEL University

Press Release

SEL Completes Purchase of New Post Falls Manufacturing Site

  • SEL Invests More Than $500 Million to Expand U.S. Manufacturing Capacity
  • SEL Releases Two New Solutions for High-Density Serial-to-Ethernet Communications

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow