Schweitzer Engineering Laboratories

Newsroom

Jan 8, 2021

New, Versatile SEL-3350 Automation Controller Now Available for Order

SEL has released the SEL-3350 Automation Controller. This new addition to the automation controller family, designed to complement the SEL-3355 and SEL-3360 Automation Controllers, provides a lower price point and a smaller 1U form factor. The SEL-3350 is ideal for applications that require midlevel I/O and computation.The SEL-3350 is orderable with a variety of computer operating systems, such as Microsoft Windows 10 IoT Enterprise, Windows Server and Linux drivers for CentOS, Red Hat and Ubuntu. SEL Blueframe and RTAC operating system options will be available in the first quarter of 2021. To learn about how the SEL-3350 fits into the automation controller family, please refer to the Automation Controller Family Comparison Table.For more information about the SEL-3350 features, visit the product webpage.
Back to Newsroom 
Featured Stories

Corporate

SEL Expands Manufacturing Operations in West Lafayette

Technical

SEL Achieves IEC 62443-2-4 Certification, Strengthening Cybersecurity Assurance for Critical-Infrastructure Customers

Press Release

SEL Continues to Expand Manufacturing Capacity With New Post Falls, Idaho Facility

  • SEL Expands Manufacturing Operations in Idaho with New Facility in Nampa
  • Idaho: Closing the Innovation Gap

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow