Schweitzer Engineering Laboratories

Newsroom

Oct 30, 2020

SEL Releases Motor Bus Transfer Relay

Schweitzer Engineering Laboratories has released the SEL-700BT Motor Bus Transfer Relay, a purpose-built relay which offers comprehensive bus transfer and protection for critical process environments that require a continuous and reliable supply of electric power. Using its automatic and manual methods, the SEL-700BT transfers critical loads from a primary source to an auxiliary feeder during faults in the primary feeder line. This keeps processes running without requiring a cold start, helps avoid costly shutdowns, provides personnel safety and helps avoid environmental damage.The relay’s numerous current, voltage, frequency and directional elements provide comprehensive protection for motor bus transfer applications. Users can easily integrate the SEL-700BT into new or existing control systems with its advanced communications protocols, such as EtherNet/IP and the IEC 62439 Parallel Redundancy Protocol. In addition, its 5-inch color touchscreen display allows users to quickly configure, monitor and control their system.Learn more about the SEL-700BT on the product webpage.
Back to Newsroom 
Featured Stories

SEL In The News

Pullman School District Sale of Aquatic Center to SEL Finalized

Press Release

SEL Names New Vice President of Sales and Customer Service

Press Release

SEL Names New Vice President of Engineering Services

  • SEL Founder Urges Civic Engagement and Civility at Pullman Chamber Luncheon
  • SEL supports ambitious grid modernization project in Central America

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow