Schweitzer Engineering Laboratories

Newsroom

Oct 21, 2020

SEL Broadens SDN Portfolio With the SEL-2742S

SEL has released the SEL-2742S Software-Defined Network Switch. With this release, utility and industrial network engineers have a choice of 19" rack mounting (with the SEL-2740S Software-Defined Network Switch) or DIN-rail or surface mounting (with the SEL-2742S) for their software-defined networking (SDN) switch hardware.  Like the SEL-2740S, the SEL-2742S integrates with the SEL-5056 Software-Defined Network Flow Controller to improve LAN cybersecurity with a deny-by-default approach to network traffic forwarding. SDN also provides faster network failover, streamlines network management and change control and automates data collection for cybersecurity audits.The SEL-2742S is a 12-port switch designed and built for operation in harsh environments, meeting IEEE 1613 requirements. The SEL-2742S operates from –40° to +85°C (–40° to +185°F), and dual power supply connections provide connectivity to primary and backup power sources.Pricing for the SEL-2742S starts at $2,200.For more information about the SEL-2742S, visit the product webpage. 
Back to Newsroom 
Featured Stories

Press Release

SEL Releases 2026 Index of Freedom

Press Release

SEL to Purchase Former Pullman Building Supply Property

Press Release

SEL Names New Vice President of Property

  • SEL Announces 2026–2027 Scholarship Program Recipients
  • SEL Fault Indicators and Sensors Now Feature the LINAM Name

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow