Schweitzer Engineering Laboratories

Newsroom

Oct 20, 2020

New Protocols for SEL-849 Motor Management Relay

Three new protocols are now available for the SEL-849 Motor Management Relay: EtherNet/IP, the IEC 62439 Parallel Redundancy Protocol (PRP) and DNP3. With these additions, the multipurpose protection and control relay can more easily be applied in industrial and utility applications.EtherNet/IP, which is commonly used in industrial automation networks, allows the SEL-849 to better integrate with process controls. Its availability also eliminates the need for protocol converters, thereby reducing costs and system complexity. When dual Ethernet ports are selected, the SEL-849 supports PRP and fast failover switching. PRP helps increase communications system reliability, reduces wiring and labor and provides confidence in non-hardwired motor controls.DNP3 delivers accurate time-stamped data over Ethernet for event reporting and allows the SEL-849 to act as a low-cost telemetry device, both fitting uses for utilities. With DNP3, the relay can be used for end-of-line monitoring; fault location, isolation and system restoration; power metering; and more.For more information about these enhancements and the capabilities of the relay, visit the SEL-849 product webpage.
Back to Newsroom 
Featured Stories

Press Release

Two SEL Leaders Honored by the Manufacturing Institute

Technical

SEL and Puget Sound Energy Collaborate With Customers for Community Microgrid

Press Release

SEL Begins Work on New Electronic Device Manufacturing Facility in Moscow, Idaho

  • SEL Executive Vice President Elected Chair of the Board of Directors of ESCA
  • SEL Releases New Transformer Controller With LTC Control

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow