Schweitzer Engineering Laboratories

Newsroom

Apr 28, 2020

Webinar: How Source Diversity Improves Control Power Supply Reliability


DC control power can fail for a number of reasons—battery failures, dc control system faults, battery charger failures, testing or maintenance errors—leaving critical equipment without power. If a fault occurs when protection equipment are not energized, even a minor event can lead to damaged equipment, costly repairs and harm to personnel. Redundancy can help prevent a single point of failure in control power systems and help you avoid these outcomes.

During the May 13, 2020, 11:00 a.m. (Pacific) webinar, Senior Application Engineer Austin Wade will discuss the importance of control power reliability for protection, monitoring and control equipment. He will also explain how the new SEL-RPM Redundant Power Module, which combines multiple ac and dc power sources, stores energy to enable breaker tripping and how its ride-through time allows event reports to be saved when needed most. 

Register now to learn how source diversity improves control power supply reliability.

Back to Newsroom 
Featured Stories

Press Release

SEL Announces 2025-2026 Scholarship Recipients

Corporate

SEL Receives Purdue Senior Design Partner of the Year Award

Corporate

SEL Technical Experts Recognized for Contributions to Industry

  • SEL Raises Starting Hourly Wage to $20
  • SEL develops a land mobile radio solution that protects first responders

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow