Schweitzer Engineering Laboratories

Newsroom

Aug 14, 2019

Montclair State University Chooses SEL for Microgrid Control System


SEL Engineering Services recently installed a microgrid control system at Montclair State University that is estimated to save the New Jersey college over $4 million per year. The system, which runs in tandem with the university’s 5.4 MW heating, cooling, and power production plant, is designed to reduce emissions and ensure energy-efficient delivery of steam for heating, chilled water for air conditioning, and natural gas for electricity.
In the event of a power disturbance, the SEL microgrid control system can respond within milliseconds, islanding the university from the utility, maintaining voltage and frequency, and shedding the lowest priority loads while keeping most of the campus up and running. Commands are sent to generation units to spin up, and once campus generation is online, the remainder of the campus is energized. When the utility is back up and running, the system can then seamlessly reconnect to the utility grid. Montclair State University now has a system that ensures uninterrupted energy delivery to all key university assets. Redundancy, reliability, seamless transition, and the ability to blend multiple sources of power generation have all contributed to making this SEL microgrid system the best solution for the university.Read more about the Montclair State University project and more about SEL microgrid solutions on the SEL website.
Back to Newsroom 
Featured Stories

Technical

SEL Website Improves Navigation With New Sections for Products, Industries, and Services

SEL In The News

Inventing the future: An interview with Dr. Ed Schweitzer

SEL In The News

Tariffs are harming manufacturing. Congress must act now

  • SEL enhances the performance and digital input capacity of the SEL-2240 Axion
  • How two SEL employees turned a simple fix into a patented solution

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow