Schweitzer Engineering Laboratories

Newsroom

Jul 5, 2019

SDN Provides New Solution for Interconnecting IEC 61850 Ethernet Networks

A newly published white paper from SEL, SDN Advantages for Ethernet-Based Control, describes the use of software-defined networking (SDN) technology at Itaipu Dam, one of the world’s largest hydroelectric facilities.

Itaipu needed to interconnect a new IEC 61850 Ethernet network with the large, in-service dam without making any configuration changes to the existing network. Traditional networking solutions, such as VLANs, could not meet this challenge. But SDN provided the answer. SDN provides complete network control by allowing engineers to predefine every communications flow on the network, including backup paths. This allowed network engineers to connect the two networks physically while keeping them logically separate.

SDN not only allowed Itaipu to interconnect their networks with no modifications to the existing network logic, it also provided low network failure recovery times, enhanced cybersecurity, and increased control and visibility of network traffic. Because of these benefits and the simplicity of SDN, Itaipu is now applying SDN elsewhere on their system, even where traditional networking solutions would be an option. 

Get more technical details in SEL’s newest white paper.

Back to Newsroom 
Featured Stories

Press Release

SEL enhances the performance and digital input capacity of the SEL-2240 Axion

SEL In The News

How two SEL employees turned a simple fix into a patented solution

SEL In The News

Pursuing patents a regular routine for SEL

  • SEL Index of Freedom Highlights Top States for Business and Trade
  • Rep. Dan Newhouse and Dr. Ed Schweitzer: It’s Vital to WA That Congress Reassert Control Over Trade

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow