Schweitzer Engineering Laboratories

Newsroom

Dec 17, 2015

SEL Axion Becomes First IEEE-Certified PMU

PULLMAN, Wash. — Schweitzer Engineering Laboratories, Inc. (SEL) today announced that the IEEE Standards Association (IEEE-SA) certified the SEL-2240 Axion as complying with all applicable requirements in the IEEE Synchrophasor Measurement Test Suite Specification—Version 2.

To attain this certification, the Axion met or exceeded the rigorous requirements established by the IEEE Synchrophasor Conformity Assessment Steering Committee (SCASC), which consists of industry subject matter experts. Consumers Energy Laboratory Services, an IEEE-authorized independent laboratory, conducted the tests to verify compliance.

“Certification of the SEL-2240 Axion from a notable industry leader in power and energy, such as SEL, marks an important milestone for the IEEE Synchrophasor Certification program,” said Konstantinos Karachalios, managing director, IEEE-SA. “This program addresses a gap in the power industry by offering buyers of PMU technology a method to determine compliance of a product to the IEEE C37.118.1a standard before purchase and large-scale deployments.”

In 2002, SEL was the first to introduce PMU capability in a relay—a feature that has become standard in many SEL relays. In 2005, IEEE published the first version of the IEEE C37.118™ standard for synchrophasors in response to a market technology need. SEL participated in the IEEE Synchrophasor Certification program pilot in 2015.

“As an industry leader in synchrophasor technology and PMU devices, SEL has continually innovated these types of technologies to produce the first PMU that is compliant with the IEEE C37.118.1a™-2014 standard,” said SEL R&D Manager Max Ryan. “This accomplishment demonstrates SEL’s continued leadership and commitment to synchrophasor technology on a global scale.”

The SEL Axion is a fully modular, scalable, and distributed I/O measurement and control solution suitable for numerous utility and industrial applications. Due to its modular design, the Axion scales easily to the amount of phasor measurements required in a system. Capable of serving up to 64 phasor quantities at 60 measurements per second, it provides an economical solution for small to large PMUs. The expandable and distributable design also allows multiple Axion nodes to collect IEEE C37.118.1a-2014 compliant synchrophasor data at the point of measurement, providing a reduction in copper wiring. In addition, the flexible configuration of the synchrophasor server in the Axion also provides an option to send time-stamped and accurate P or M Class synchrophasor measurements to as many as six master stations for wide-area monitoring.

The SEL Axion is available now for order. For more information on the features, benefits, and applications, visit www.selinc.com/p236.

To find out more about the IEEE standards, visit their website here.

SEL serves the power industry worldwide through the design, manufacture, supply and support of products and services for power system protection, monitoring, control, automation, communications and metering. For more than 30 years, SEL has provided industry-leading performance in products and services, local technical support, a 10-year worldwide warranty and a commitment to making electric power safer, more reliable and more economical.

Back to Newsroom 
Featured Stories

Corporate

SEL Index of Freedom Highlights Top States for Business and Trade

SEL In The News

Rep. Dan Newhouse and Dr. Ed Schweitzer: It’s Vital to WA That Congress Reassert Control Over Trade

Press Release

SEL Announces 2025-2026 Scholarship Recipients

  • SEL Receives Purdue Senior Design Partner of the Year Award
  • SEL Technical Experts Recognized for Contributions to Industry

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow