Flow Auditor is a new application in the SEL-5057 SDN Application Suite. It is designed to operate with the SEL-5056 to provide safe, nondisruptive audits and documentation on the hosts that can connect to the software-defined network and on the conversations allowed between each host on your critical infrastructure network. Flow Auditor reads OpenFlow configurations from the SEL-5056 and reports all the devices, ports, and services allowed on the network.
This application provides situational awareness by showing exactly what traffic is allowed on the network. It also provides the data needed to support compliance to NERC CIP-007-6 R1.
For more about Flow Auditor, visit selinc.com/products/5057.