Automation News
56 results
Learn how adding load tap changer (LTC) control to the SEL-2414 Transformer Automation Controller brings thermal and voltage regulation into a single device.
Learn About Improvements to Resource Management and DMA Workflow and Updates to DMA Licensing Locked
Learn about features in SEL Blueframe that streamline data collection and management.
Learn how the RTAC R155-R201 firmware enhances Axion substation monitoring capabilities.
A new set of Real-Time Automation Controller (RTAC) human machine interface (HMI) tagged templates is now available to enhance workflow.
SEL is releasing two new modules for the SEL-2240 Axion: the upgraded SEL-2241-2 Real-Time Automation Controller (RTAC) Module and SEL-2244-4 Digital Input Module. The new SEL-2241-2 RTAC now contains the same CPU as the popular SEL-3350 RTAC. The SEL-2244-4 is a new 32 digital input module that increases the total digital I/O and offers new combinations to support product retrofits.
We’ve recently released enhancements to applications in SEL Blueframe, including Resource Management, Direct Resource Access, and the Device Management and Automation (DMA) application suite.
We are updating the Real-Time Automation Controller (RTAC) product line with new features and adding a 64-bit version of the RTAC OS. These updates add power quality measurement capabilities to the SEL-2240 Axion, enhance interoperability with devices from other vendors, and upgrade cybersecurity features by supporting SNMPv3.
Larger SSD makes SEL computers and select RTACs more effective in storage-heavy applications.
We’ve added 32 new DI/DO status LEDs to SEL-3350 3U RTACs ordered with a DI/DO expansion board.
Easily monitor and manage alarms on-site.
SEL Axion modules now stream synchrophasor data at 120 messages per second.
We’ve added a new use for session IDs created in the Resource Management application on Blueframe that makes it easier to securely connect to a device.
The latest RTAC firmware update includes new alarm functionality for Axion Bay Controller touchscreens, a tag selector tool for acSELerator RTAC SEL-5033 Software, automated network event capture, and more.
Collect system-wide metering data using the Device Management and Automation (DMA) application suite on the SEL Blueframe application platform.
With a last-time buy date set for acSELerator Team, read our recommendation for smoothly transitioning to its successor, the DMA application suite on SEL Blueframe.
Upgrading to an SEL-3300 series automation and computing platform becomes easier with the newly released SEL-2902 RJ45 to DB-9 Adapter Panel.
The SEL-2414 Transformer Monitor now offers a five-inch color touchscreen option, an enhanced processor, and IEC 61850 enhancements.
The SEL-3355-2 computing platform is now VMware-certified. We’ve also released a VMware-certified driver for the SEL-3390E4 Ethernet card.
Built-in redundancy for SEL Blueframe minimizes downtime during unexpected failures or system upgrades. The feature is currently available for Blueframe virtual machine deployments and will soon become available for deployments on SEL computing platforms.