Products
Industries
Services
Education
Support
Company
Login
SEL-351R
Overview
Documentation
Support
SEL-351R
Toggle Dropdown
Overview
Documentation
Support
Documentation
Featured
Instruction Manual
SEL-351R-4 Recloser Control
Literature
Documents sorted by newest first.
Include English Literature
Literature
Instruction Manuals
SEL-351R-4 Quick-Start Installation and User's Guide
SEL-351R-4 Recloser Control
Instruction Sheets
SEL Recloser Control Heater Accessory
SEL-351R-4 Terminal Block for I/O Wiring
SEL-351R-4 Terminal Block for Field Wiring
SEL-351R AC Throw-Over Accessory
SEL-9250001 Accessory Mounting Kit for SEL-351R Recloser Controls
Settings Sheets
SEL-351R-4 EZ Settings Sheets
SEL-351R-4 DNP Settings Sheets
SEL-351R-4 Settings Sheets
Configurable Labels
SEL-351R User-Configurable Labels for SEL-351R Recloser Control Front Panel
SEL-351R Configurable Label Template (A4)
SEL-351R Configurable Label Template (Vertical Merged)
Certificates
IEEE C37.60-2003 Compliance - Cooper NOVA 27 - November 2010 (SEL-351R)
IEEE C37.60-2003 Compliance - Cooper NOVA 27 - November 2005
IEEE C37.60-2003 Compliance - Cooper VWVE - August 2004
ANSI/IEEE C37.60-1981 Compliance - Cooper NOVA 15
ANSI/IEEE C37.60-1981 Compliance - Whipp & Bourne GVR
Publications
Application Guides
Creating Sectionalizer Logic on the SEL-351R and SEL-651R Recloser Controls
Using the Wireless Protection System to Selectively Block Fuse-Saving and Accelerated Tripping in the SEL-351R Recloser Control
Introduction to SEL Relays for New Users
Defining DCE and DTE: Null Modem Cable and Straight-Through Cable Applications
Setting and Testing Frequency Elements With Time Delay in Cycles
Using the SEL-FT50/SEL-FR12 System to Selectively Permit Accelerated Tripping in the SEL-351R Recloser Control
Securing Critical Assets in Control Cabinets With the SEL-3622
Converting SEL-351R-2 Recloser Control Settings Files for Use in an SEL-351R-4 Recloser Control
Enabling Instantaneous Tripping During a Hot Line Tag Condition With the SEL-351S, SEL-351R, and SEL-651R Relays
Vacuum Bottle Contact Flashover and Failure to Interrupt Load Current Detection Logic in the SEL-351R Recloser Control
Using SEL-351s and SEL-351Rs to Provide Automated Load Restoration for Distribution Feeders
Lockout Alarm for the SEL-351R Recloser Control
DNP Auto Dial-Out With the SEL-351R Recloser Control
Compensate for Constant Phase Angle Difference in Synchronism Check With the SEL-351 Relay Family
Using the SEL-351 Relay Synch-Check Element With Dissimilar Voltage Magnitudes on the Polarizing and Synchronizing Inputs
Multiple Trip Outputs for SEL-351 and SEL-551 Relays
Making SEL-351R Recloser Controls Talk
Related Material
351R-1 - AMS Test (.mdb)
351R-1 (.mdb)
351R-2 - AMS Test (.mdb)
351R-2 (.mdb)
Programming Front-Panel Operator Controls in the SEL-351R Recloser Control (Underfrequency Load Shedding Control Example)
Change Logic in SEL-351R Recloser Control for Motor-Operated Reclosers
SEL-351R Sensitive Ground Directional Elements
Application Notes
Using a Soldering Gun to Perform Current Injection Testing for SEL Recloser Controls
Case Studies
Rural Idaho Electric Cooperative Saves Restoration Time With SEL Recloser Controls and Remote Communications
Drawings