html{display:none} Lighting up the Desert Nation | Schweitzer Engineering Laboratories
Hero Option 3

Lighting up the Desert Nation

It’s microburst season in the Sonoran Desert, the land of the Tohono O’odham Nation. These powerful bursts of wind come on suddenly and cause as much damage as a tornado.

For the Tohono O'odham Utility Authority, that usually means outages for their customers, long nights, and overtime for the 16 technicians that cover over 4,400 square miles of territory.

But all of that is about to change.

This year marks a historic feat for both their region and the electric power industry worldwide. As one of the first utilities to install the SEL-T400L—a relay operating with time-domain technology—they were the first to experience the relay’s unprecedented tripping speed during a live event. The faster a relay trips, the less time dangerous fault currents remain on the system to cause damage. This speed, combined with advanced technologies like traveling-wave fault locating, make the SEL-T400L a relay that saves a utility precious time and money. The live event marked the entrance into a new era of electric power system protection for TOUA, where they will secure the reliability of their service for years to come.

In the remote Native American region of Arizona is the second-oldest tribally owned and operated electric utility in the United States: the Tohono O’odham Utility Authority (TOUA).

The Tohono O’odham, which means “Desert People” in their language, created TOUA in the late 1960s to boost their sovereignty and economic future. After purchasing an on-reservation distribution system from an outside electric cooperative, the utility’s first big undertaking was to connect more homes to the electric grid. In a hot, desolate area of dirt roads, no signage, and far-flung homes, it was a big accomplishment for a tiny utility. A half-century later, the utility has evolved to provide telephone, water, cellular, and internet services.

TOUA Logo

TOUA provides power, telephone, water, cellular, and internet services to 3,000 customers over 4,400 miles—with only 16 employees. Their logo features an arrowhead splitting the desert landscape while power lines tower above, a perfect blend of cultural tradition and modern technology.

Ancient World, High-Tech

The Tohono O’odham Nation spans 4,460 square miles west of Tucson and south across the border into northern Mexico. 

Cactus in the desert
Mission San Xavier del Bac

Saguaro cacti (top left) can reach heights of 40 ft and dot the desert landscape alongside innumerable other species (bottom right). The cacti are carefully cultivated around the historic Mission San Xavier del Bac (top right), “the white dove of the desert,” for their unique appearance and beautiful summertime blossoms.

View Gallery
Closeup of cactus spikes

In the heart of their ancient homeland and off a winding dirt road is a TOUA metering station protected by a chainlink fence. Inside is a metal cabinet that houses the SEL-T400L. The site represents a cultural juxtaposition: hidden amid an environment steeped in history is a leading-edge technology to help ensure the Tohono O’odham future.

Monsoons peak in summer, when dramatic thunderstorms called microbursts erupt over the desert landscape—most often at night—bringing rain to the parched landscape but also strong winds.

“We get some bad storms here, including a lot of lightning, which can make it challenging to provide reliable electricity to our customers,” said Darrold Hobbs, operations manager of TOUA’s electric department. “To prevent outages and blackouts, we knew we had to modernize aging equipment. I heard about Schweitzer Engineering’s new relay—that it was both fast and simple—and we decided to upgrade with it.”

That decision made TOUA the second utility in the world to use SEL’s time-domain technology for tripping line breakers. TOUA serves 3,000 customers, buys power from several outside companies, and has just 16 employees on its electric crew.

two men in a control house looking at equipment

Installation of the SEL-T400L allows TOUA’s employees to spend their time and effort where it’s needed most.

“They work hard and they’re skilled, but we’re a small utility with limited resources trying to cover a lot of territory,” said Hobbs.

A disturbance on a line can mean crew members have to drive an hour and a half to isolate a fault, sometimes on washed-out roads during a monsoon storm, he added.

Part of the SEL-T400L design includes traveling-wave fault locating, a technology that can save utilities hours when searching for faults. The technology pinpoints a fault’s location to within one tower span.

The First Real-World Test

Not long after the SEL-T400L went online, an intense windstorm rolled across Tohono O’odham territory, giving the relay its first real-world test. In just over half an hour, there were seven faults, and each time the SEL-T400L tripped in under 2 ms. These events made TOUA the first sub-transmission utility to experience this relay’s unprecedented tripping speed.

“If not for this new technology, the power would have gone out and our crews would have been driving around and trying to restore it in bad weather,” said Hobbs. “Instead, it did the job so well that we didn’t even know about the disturbance until later.”

With this event, TOUA made electric transmission protection history.

—The End—


“Brain surgery” performed on live substation

View The Project
“Brain surgery” performed on live substation

Request a Follow-Up

(0/250)