This webinar introduces the SEL-T35 Time-Domain Power Monitor, a continuous data streaming device that delivers high-precision ac and dc voltage and current measurements for observation and analysis—increasing efficiency and reliability.
This webinar covers different technologies—like downed-conductor detection and high-speed tripping—that can be used as part of a scalable solution for wildfire mitigation.
This webinar describes high-impedance bus differential protection solutions and demonstrates features of the new SEL-787Z High-Impedance Differential Relay and SEL-HZM High-Impedance Module.
Learn how enhancements to the SEL-487E Transformer Protection Relay expand its capabilities in centralized protection and control (CPC) applications.
Direct-replacement assemblies (DRAs) are complete, preassembled retrofit kits. This webinar provides an overview of DRAs and the benefits they offer for protection retrofit projects at any scale, including how they save time, save money, and simplify installation.
Learn how enhancements to the SEL-734W and SEL-734B simplify the deployment and configuration of advanced capacitor bank controls.
This webinar discusses how streaming and recording high-resolution continuous waveform data improves power system awareness. Learn about solutions that can stream and record data at rates of 3,000 to 14,400 samples per second. We also share real-world use cases and insights.
Operational technology (OT) software-defined networking (SDN) delivers cybersecurity and performance advantages that make it the ideal networking solution for IEC 61850 substation applications.
Learn how the SEL ICON provides high-availability service to TDM and packet-based WANs, allowing it to serve as a single scalable multiplexer platform for seamless migration to Ethernet-based networks at the pace you choose.
This webinar introduces a complete solution that improves reliability metrics by enhancing protection and restoration in distribution systems that have a high recloser density.
This webinar discusses our next-generation solution for automated data collection: the DMA application suite on the SEL Blueframe application platform.
In this webinar, we share metering data collection and visualization software, including Synchrowave Reports and the new Meter Monitoring application package on DMA.
This webinar discusses the advanced digital fault recorders (DFRs) and substation monitoring solutions that SEL offers.
This webinar provides information on flexible transformer protection, distance elements in the SEL-487E Transformer Protection Relay, a centralized protection and control solution with the SEL-487E, and traditional and Time-Domain Link (TiDL) relay solutions.
This webinar discusses a recent innovation for FLISR on SEL Blueframe—geographic information system (GIS) integration. This functionality allows users to import GIS data and use it to automatically configure and update their FLISR system while retaining the simplicity FLISR is known for.
This webinar discusses our next-generation solution for automated data collection: the DMA application suite on SEL Blueframe.
This webinar provides an introduction to powerMAX for utilities and information on power system challenges, wide-area monitoring and control, control and mitigation strategies, system validation and testing, and case studies.
This webinar discusses advanced DFR and substation monitoring solutions, including several recent innovations: continuous oscillography streaming and recording, simplified configuration, advanced digital asset monitoring and digital signal processing capabilities, and more.
This webinar shows how enhancements to the SEL-2431 Voltage Regulator Control improve voltage regulation in systems with multiple power sources and distributed generation.
This webinar will provides information about the thermal element in the SEL-710, including the first-order thermal model, different methods to set the thermal element, developing settings using the rating method, and checking coordination.
This webinar describes high-impedance bus differential protection solutions and demonstrates features of the new SEL-787Z High-Impedance Differential Relay and SEL-HZM High-Impedance Module.
This recorded webinar provides information on bridging the gap between second, millisecond, and microsecond accuracies, maintaining time accuracy by implementing best practices, and adding precise-time redundancy and mitigating GPS vulnerabilities.
Direct Replacement Assemblies (DRAs) are complete, preassembled retrofit kits. This webinar provides an overview of DRAs and the benefits they offer for protection retrofit projects at any scale, including how they save time, save money, and simplify installation.
This recorded webinar provides an introduction to the SEL wide-area situational awareness (WASA) software Synchrowave Operations. It includes a demonstration of methods for detection and location of generation loss events and of failing voltage transformers (VTs).
Learn how the SEL RTAC platform and its Grid Connect library provide visualization, local control, and protocol conversion functionality for utility-scale inverter generation, commercial-scale inverter generation, and behind-the-meter applications.
This recorded webinar focuses on the SEL Wireless Protection System and its new SEL-RP50 Fault Repeater. The system, which also includes the SEL-FT50 Fault Transmitter and SEL-FR12 Fault Receiver, is a simple and cost-effective solution for utilities to enhance distribution protection. It can be easily implemented on feeders to help recloser controls and protective relays make the best decisions.
In this webinar, Engineering Manager Darrin Kite presents on SEL’s solutions for substation gateway applications and RTU replacements, including the new SEL-3350 3U RTAC model.
This webinar highlights two solutions for monitoring harmonics distortion and confirming IEEE 519 compliance: SEL-5705 Synchrowave Reports, a new browser-based meter reporting tool, and the SEL Real-Time Automation Controller (RTAC).
Learn about SEL’s digital secondary system (DSS) process bus solutions that use IEC 61850 Sampled Values, GOOSE, and PTP protocols. This recorded webinar discusses communications features of SEL-400 series relays that support Parallel Redundancy Protocol (PRP) on process bus networks and an additional, dedicated communications port for Engineering Access.
In this webinar, Lead Application Engineer Lance Dice presents on the File Import application recently added to the SEL-5056 Software-Defined Network Flow Controller as well as the new SEL-2741 Ethernet Switch.
This recorded webinar provides information about automated password rotation available in the DMA Credential Management applications on the SEL Blueframe platform. This new feature supports and simplifies asset management and compliance efforts.
Join us for a recorded webinar to learn about the future of meter data analysis and reporting software with SEL. Webinar host Michael Holland discusses a phased approach to transitioning from SEL-5630 acSELerator Meter Reports to SEL-5705 Synchrowave Reports—Meter Data. SEL Synchrowave Reports software offers many enhancements in meter data reporting.
This recorded webinar provides information about SEL solutions related to managing data, automating processes, and performing other software-based tasks in an operational technology (OT) environment with SEL Blueframe—a user-friendly, modular OT application platform that allows users to automate OT processes and manage substation and recloser data more efficiently. Topics include secure engineering access and resource management tools, security, ease of use, the Data Management and Automation (DMA) application suite, and the Credential Management application package.
This webinar provides information on transformer protection applications with the SEL-487E Transformer Protection Relay for centralized protection and control (CPC) schemes. We also discuss transformer event analysis using SEL-5601-2 Synchrowave Event Software.
This recorded webinar provides information on protection relay elements that can help utilities mitigate the risk of wildfires caused by distribution and transmission lines, including discussions of phase discontinuity detection, broken conductor detection, incipient fault detection, travelling-wave-based fault locating, and line monitoring.
In this recorded webinar, presenters from SEL and San Diego Gas & Electric (SDG&E) demonstrate the functionality of a falling conductor mitigation solution on distribution circuits and include examples of field applications.
This recorded webinar describes the broken conductor detection algorithm available in the SEL-411L Advanced Line Differential Protection, Automation, and Control System. During the webinar, we describe how this new algorithm is validated using field events and simulations.
This recorded webinar provides information about the alpha plane operating characteristic, including discussions about CT saturation for internal and external faults, long transmission lines and cables with charging current, series-compensated lines, and channel impairments and data alignment errors.
This webinar introduces new benefits that SEL-5702 Synchrowave Operations Software offers to users, including preventing incipient PT failures and quickly locating generation loss events.
This webinar introduces and demonstrates SEL’s next-generation solution for automating fault location, isolation, and service restoration (FLISR)—available in the new Distribution Management System (DMS) application suite on the SEL Blueframe software platform.
This recorded webinar provides information on situational awareness software for power system operators, broken-conductor detection, and traveling-wave fault locating. We also discuss a line-monitoring solution that detects incipient faults, recurring faults, and incipient cable faults and how autoreclosing is allowed or inhibited using TWFL results with ARC logic.
This recorded webinar focuses on a new, resilient approach to time synchronization using the SEL ICON for time distribution over WAN. This solution will provide submicrosecond timing accuracy for critical applications, maintaining synchronization consistency with multiple discrete timing sources even in the event of localized GPS outages due to antenna failures, jamming, or GPS spoofing attacks.
It's possible to get more out of a basic feeder protection relay without adding complexity. We've combined protection, monitoring, and control in a simple, compact package in the new SEL-851 Feeder Protection Relay. This webinar discusses the features and benefits of the SEL-851, from preventing equipment damage and increasing safety to easy integration.
This recorded webinar highlights two solutions for monitoring harmonic distortion and confirming IEEE 519 compliance: SEL-5705 Synchrowave Reports, a new browser-based meter reporting tool, and the SEL Real-Time Automation Controller (RTAC).
This recorded webinar introduces and demonstrates the Direct Resource Access tool on the SEL Blueframe application platform as well as enhancements to the Resource Management tool. Direct Resource Access provides a secure engineering access interface, simplifying fleet management.
This recorded webinar provides information about advances for the phasor-based distance protection element and an overview of the time-domain distance protection element.
This recorded webinar will teach you what to keep track of when it comes to properly loading transformers without exceeding their loss-of-life limits—from monitoring thermal conditions and through-fault events to controlling transformers and fan banks.
This recorded webinar provides information on how and why trust factors into the field of cybersecurity, the core tenets of zero trust, tools and techniques to modify and apply zero-trust principles to operational technology (OT) industrial control networks, and existing policies and controls that make applying zero trust more attainable.
In this webinar, presenter Scott Wenke introduces the latest additions to the SEL-487E and the new applications it offers.
This webinar provides information on SEL’s falling conductor mitigation solution. This solution identifies and de-energizes overhead power lines within milliseconds of a break, preventing high-impedance faults and hazardous conditions.
This webinar provides information on how Converged Industrial Edge (CIE)—the joint SEL, Juniper Networks, and Dragos solution—unifies inventory management, simplifies NERC CIP auditing, eliminates repetitive data entry and network configuration errors, and automates end-to-end circuit provisioning. CIE also provides deny-by-default, zero-trust cybersecurity and total situational awareness and reduces operational expenses and simplifies processes.
This webinar introduces an ICS attack framework that may be used by any power system entity to evaluate emerging technology security risks. Participants will learn how this framework helps entities effectively and uniformly assess risks and weigh risks against potential benefits.
This webinar provides information on the first-order thermal model, explains the different methods to set the thermal element, and develops settings using the rating method and check coordination.
This webinar provides information on simplifying device setup using transformer nameplate and test data settings templates, monitoring transformer loss of life using IEEE and IEC thermal models, developing a more responsive cooling system with fan control, and optimizing settings for top-oil temperature calculations.
Learn how MACsec in the SEL-651R and SEL-651RA Recloser Controls enhances the cybersecurity of both new and already installed recloser cabinets. See how to set up MACsec in new and upgraded recloser controls.
This webinar introduces the features that make the SEL-3780 Test Point Voltage Sensor dependable, economical, and easy to retrofit in source-transfer switchgear applications.
This webinar provides information on the SEL Real-Time Automation Controller (RTAC) platform, libraries, and extensions for power system monitoring, automation tools, and control solutions.
This webinar provides an overview and demonstration of SEL’s new Blueframe application platform, which allows users to automate operational technology (OT) processes and manage substation and recloser data more efficiently.
This webinar focuses on the techniques, technologies, and engineering approaches that give SEL powerMAX microgrid control systems the scalability and versatility to meet a diverse range of use cases, including commercial, military, and mobile applications.
This webinar explores powerful tools available in the SEL-5601-2 synchroWAVe Event Software and how they aid in analysis of transformer relay event reports.
This webinar highlights the Converged Industrial Edge—a purpose-engineered, zero.trust network architecture. Learn how the solution simplifies the information exchange between IT and operational technology (OT) devices, minimizes the cyber-attack surface, and reduces operations and maintenance costs.
SEL’s new substation bay controller provides reliable control and monitoring of breakers, switches, instrument transformers, and other equipment. The Axion Bay Controller is a flexible and expandable solution to address the challenges of variety and complexity in bay configurations. This solution combines the scalable architecture of the SEL-2240 Axion with a fully integrated, 7-inch touchscreen display and the logic engine of the SEL Real-Time Automation Controller (RTAC) for complete and customizable bay control.
Tune in for a technical presentation exploring the benefits and advantages of Time-Domain Link (TiDL) technology, a digital secondary system solution from SEL.
This webinar focused on recent additions to the Blueframe application platform and its Data Management and Automation (DMA) application suite.
This webinar explores the new Synchrowave Monitoring and Synchrowave Operations software and how they help transform a variety of power system data into actionable information. The webinar includes a demonstration of Synchrowave Operations, which was designed to complement existing SCADA and EMS solutions.
This technical presentation describes the new SEL-851 Feeder Protection Relay, which offers comprehensive protection and advanced communications in a simple, compact package.
This webinar describes scalable fault location, isolation, and service restoration (FLISR) solutions that use SEL recloser controls, communications devices, automation controllers, and software to locate and isolate permanent faults and restore power to healthy portions of affected distribution lines or feeders. It details how FLISR can be applied in local, peer-to-peer, or regional system configurations to minimize downtime for customers, limit potential equipment damage, and improve reliability indices.
In this technical presentation, we teach you what you need to know to avoid costly outages due to incorrect transformer compensation settings. We present four simple rules to ensure that you always get your transformer compensation settings correct, and we show how to use an existing Application Guide tool to identify incorrect compensation settings during commissioning or after a fault. We also show an event where using Matrix 12 for compensation led to an undesired operation, and how following the four rules would have kept the relay secure.
This webinar describes SEL’s position on the concept of zero trust, how zero trust differs between operational technology (OT) applications and IT applications, and how to incorporate the tenets of zero trust in OT environments while taking into account the unique requirements of critical infrastructure networks.
This technical presentation describes event playback testing, a built-in feature available in the SEL-T400L Time-Domain Line Protection and the SEL-T401 Ultra-High-Speed Line Relay.
A system-focused approach to energy metering can improve efficiency, increase uptime, and decrease operating costs. This is especially important for industrial plants, commercial buildings, transportation hubs, and multibuilding campuses, like manufacturing facilities and universities. During this webinar, we will discuss SEL’s scalable campus metering systems—which use the SEL-735 Power Quality and Revenue Meter as a foundation—and share real-world examples of their data visualization and analysis capabilities.
This technical presentation talks about ongoing partnerships with utilities around the world and how SEL continues to develop sophisticated remedial action schemes (RASs) that solve complex power system issues.
It's possible to get more out of a basic feeder protection relay without adding complexity. We've combined protection, monitoring, and control in a simple, compact package in the new SEL-851 Feeder Protection Relay.
This technical presentation provides information about bridging the gap between second, millisecond, and microsecond accuracies; maintaining time accuracy by implementing best practices; and adding precise-time redundancy and mitigating GPS vulnerabilities.
This webinar describes the SEL-FLT and SEL-FLR Fault and Load Transmitter and Receiver System, which quickly identifies faults and accurately monitors loads. This system includes built-in security features and easily integrates into existing systems for enhanced decision-making and planning. This webinar also discusses the new SEL-FLR enclosure, which makes deploying the solution in pole-mount applications even easier and allows you to package the receiver with the SEL-3061 Cellular Router.
This technical presentation provides information on SEL cybersecurity solutions for substation operational technology (OT) and software-defined networking (SDN).
This technical presentation will provide information about information technology (IT) and operational technology (OT) security, OT cybersecurity design criteria, and SEL OT cybersecurity technologies.
This webinar introduces the SEL Blueframe and Data Management and Automation applications. During the webinar, you will learn how these new solutions support your efforts in increasing system security, efficiency (ease of use), and data utilization.
This technical presentation provides information on SEL solutions for reducing wildfire risks. Learn about high-impedance fault (HIF) detection and how it is used in SEL relays to detect a downed conductor in distribution systems. Also learn how traveling-wave fault locating, line monitoring, automatic reclose cancel, and Synchrowave Operations are used as wildfire mitigation solutions in transmission systems.
This webinar focuses on the SEL Wireless Protection System and its new SEL-RP50 Fault Repeater. The system, which also includes the SEL-FT50 Fault Transmitter and SEL-FR12 Fault Receiver, is a simple and cost-effective solution for utilities to enhance distribution protection. It can be easily implemented on feeders to help recloser controls and protective relays make the best decisions.
This webinar describes the new SEL-851 Feeder Protection Relay, which offers comprehensive protection and advanced communications in a simple, compact package.
This technical presentation will provide information on Sampled Values and Time-Domain Link (TiDL) technology solutions for digital secondary systems.
This webinar discusses how an SEL powerMAX remedial action scheme (RAS) solution helps the bulk power system function closer to stability limits and prevents blackouts. We also cover how to operate transmission corridors more efficiently at a higher capacity. Additionally, we share techniques to help you organize your specific RAS objectives, meet NERC requirements, and test and validate the solution using a hardware-in-the-loop (HIL) environment prior to field deployment.
This technical presentation provides information about the SEL-3350 Real-Time Automation Controller (RTAC) enhancements, improving substation monitoring, and the control and operational efficiency with modern SEL automation technologies.
This technical presentation provides information about operational technology (OT) cybersecurity systems with SEL’s technology and expertise. Topics include current cyber threats, regulations, standards, frameworks, system design, defense in depth, and a holistic look at competing risk. The webinar also includes overviews on SEL OT software-defined networking (SDN), SEL Blueframe, and SEL ambassador and covers balancing cybersecurity against cost, time, complexity, and usability.
This webinar describes event playback testing, a built-in feature available in the SEL-T400L Time-Domain Line Protection and the SEL-T401 Ultra-High-Speed Line Relay.
This webinar explains CT saturation in an intuitive way using simple animations and avoiding complex math and physics. We examine symmetrical and asymmetrical saturation, remanence, the equivalent circuit of a CT, and CT excitation graphs. We also show how CT saturation can affect relay operation and how to detect saturation in relay event reports.
This recorded webinar provides information on the SEL-735 for utility and industrial applications, including an overview of power quality and revenue metering capabilities, how to use the SEL-735 and data for various applications, and details about new advanced features like the touchscreen HMI.
This recorded webinar will provide information on the SEL-T401L Ultra-High-Speed Line Relay, field event analysis, and line monitoring.
This webinar focuses on how SEL powerMAX commercial microgrids provide greater resiliency, seamless islanding from and reconnection to the bulk electric system, and simultaneous energy storage management—maximizing renewable generation, reducing peak charges, and keeping the lights on.
This recorded webinar introduces you to the SEL-T401L, which is built on successes and learning from field applications of the SEL-T400L Time-Domain Line Protection. The presentation demonstrates the ultra-high-speed time-domain protection in the SEL-T401L, which now includes phasor-based distance, overcurrent, power swing blocking, and out-of-step tripping functions. We cover how simplified settings parameters reduce complexity and how the line monitor function and high-resolution oscillography help locate problems before they become unplanned outages.
This webinar focuses on a new, resilient approach to time synchronization using the SEL ICON for time distribution over WAN with an IEEE 1588 Precision Time Protocol telecom input as a time source in addition to GPS. You’ll learn about new options for WAN and substation timing, new capabilities of the Enhanced Protection Line Module, plus new enhancements to SEL-5051 Client and SEL-5052 Server Network Management System Software.
This recorded webinar will help you understand traveling waves, retrieve event report data from the SEL-T400L Time-Domain Line Protection relay, learn about SEL-5601-2 synchroWAVe Event Software, and use Bewley lattice diagrams in the software.
This technical presentation provides a step-by-step tutorial on analyzing event reports, identifying root causes, and resolving problems using real transmission line event examples. The practical methods taught in this webinar help you analyze your system events quickly and accurately.
Learn how SEL powerMAX Power Management and Control Systems prevent blackouts and keep critical processes online using advanced protection and control technologies.
This recorded webinar helps you understand the need and applications where motor bus transfer can be beneficial, provides information about system conditions used to undertake a motor bus transfer, and offers a product overview where we discuss additional features.
This recorded webinar provides information about the incipient cable fault detection feature in the SEL-751 Feeder Protection Relay; Arc Sense technology (AST); and new asset monitoring features in the SEL-710-5 Motor Protection Relay.
This recorded webinar provides information on the comprehensive methods for controlled closing and opening of breakers, transformer configuration considerations, and controlled switching devices (CSDs) and introduces the SEL-352 Breaker Failure Relay.
This webinar focuses on the SEL Unified Threat Management (UTM) Firewall, a state-of-the-art firewall and router purpose-built for substation and industrial environments. During the webinar, you will learn about the UTM firewall capabilities, such as tracking the state of connections, dynamic routing, traffic shaping, and hardware failover to increase cybersecurity.
This technical presentation provides information on NERC PRC-027 compliance, applicability. and solutions that help you be ready to meet NERC audits.
This recorded webinar provides information about the SEL-700BT. It covers the features of the SEL-700BT; how fast, safe, and reliable motor bus transfer helps avoid expensive shutdowns and improves process plants’ economics; application of the SEL-700BT for main-main and main-tie-main motor bus configurations; and more.
This technical presentation provides information on the thermal model used in the SEL-710 Motor Protection Relay. This webinar will help you understand the thermal model and learn how to set the thermal element using a motor datasheet.
For years, SEL has led the way in solving complex power system challenges using powerMAX power management technology. powerMAX prevents blackouts and keeps critical processes running with advanced high-speed protection and control technology.
This webinar focuses on the high-fidelity transient recording, traveling-wave-based fault locating, and continuous line monitoring capabilities available in the SEL-T401L Ultra-High-Speed Line Relay.
This technical presentation showcases distribution system events like conductor slaps, evolving faults, and incorrect phase tripping. We provide recommendations for best practices during testing, commissioning, and maintenance. We also provide troubleshooting tips and tools to use when things don’t go as planned.
SEL software-defined networking (SDN) is delivering real-world benefits for operational technology (OT) networks, such as substation LANs. In this webinar, we’ll share the results from utility deployments worldwide.
This recorded webinar provides information on the fundamentals of arc-flash hazards and an overview of standards and various methods of arc-flash mitigation. It also covers effective arc-flash hazard reduction, including in low-voltage motor control centers, with SEL-700 series relays, the SEL-849 Motor Management Relay, and motorMAX.
This webinar reviews the requirements and methods for implementing motor bus transfer protection, which transfers critical loads from a primary source to an auxiliary feeder during faults in the primary feeder line. During the webinar you will learn how to apply this solution using the new SEL-700BT Motor Bus Transfer Relay.
SEL can assist in the development of your cybersecurity strategy and implementation. Our experts have helped hundreds of utilities identify cybersecurity vulnerabilities and build strong cyber defenses for their operational technology (OT) systems. During the presentation, you will learn more about OT cybersecurity and how we can help you develop an America’s Water Infrastructure Act (AWIA) risk assessment and emergency plan.
This webinar focuses on how an SEL Time-Domain Link (TiDL) technology solution applies to four key factors to successfully modernize substations: protection, robustness, maintainability, and cybersecurity.
This recorded webinar focuses on SEL high-impedance fault (HIF) detection capabilities for different types of grounded and ungrounded distribution systems to detect downed conductors in high-risk wildfire areas.
This recorded webinar provides information on generator capability-based loss-of-field protection, universal differential protection, digital distance element implementation using coincidence timing, and zero settings out-of-step tripping and power-swing blocking.
This recorded webinar provides information on the power of deny-by-default multilayer packet inspection in your LAN and situational awareness advantages. We also cover how to achieve failover times of less than 100 µs and the new DIN-rail-mounted SEL-2742S Software-Defined Network Switch.
This technical presentation provides information on SEL’s powerful event analysis software tool, SEL-5601-2 synchroWAVe Event Software, and showcases how it can be used to quickly identify the source of power system problems as the presenter walks through two real-world events.
This recorded webinar discusses information about power quality concepts and its impact on power systems, features of the SEL-735 Power Quality and Revenue Meter, and integration of the SEL-735 for retrieval and visualization of metering data.
This webinar describes the challenges of running teleprotection over Multiprotocol Label Switching (MPLS) networks. You'll learn how the SEL ICON addresses many of the challenges with implementation results from three utilities.
This recorded webinar discusses information about the SEL transformer protection relay family, through-fault monitoring a default relay function, transformer thermal life, and tap control and monitoring solutions.
This webinar focuses on the SEL-735 Power Quality and Revenue Meter with a color touchscreen display. During the webinar, you will learn how the display simplifies meter setup, data access, troubleshooting, and testing. We will provide examples of how to set the PT/CT ratio and IP address and how to identify reverse CT polarity and incorrect phase rotation.
This recorded webinar discusses key features and advantages of SEL Real-Time Automation Controllers (RTACs), remote terminal unit (RTU) applications, digital fault recorder (DFR) applications, and general applications.
This webinar focuses on the SEL-400G Advanced Generation Protection System and how it can be applied to protect generators of all sizes and types, including hydro, pumped-storage hydro, steam turbine, and combustion gas turbine generators. During the webinar, you will learn about the SEL-400G relay’s two independent universal differential zones, independent frequency zones, pumped-storage logic, loss-of-field protection schemes, and more.
This technical presentation will provide information on how to use reliability data to create a replacement strategy for microprocessor-based relays. This will help you avoid common pain points associated with managing the replacement of microprocessor-based relays.
This recorded webinar provides information on SEL solutions for wide-are protection and control applications, including power system stability classification, rotator angle stability, voltage stability, frequency stability, dynamic system studies, and case studies.
This recorded technical presentation provides information on the different methods used by SEL relays to track down faults on transmission lines, the pros and cons of each method, how to choose the best method based on application, and how to manually calculate the fault location in SEL-5601-2 synchroWAVe Event Software. This will help reduce the outage time and revenue loss after a fault.
This recorded technical presentation provides information on power quality concepts, touchscreen features, and user benefits. Improving power quality compliance and troubleshooting capabilities will improve the safety, reliability, and efficiency of your power system.
This recorded technical presentation provides information on directional overcurrent elements, mho distance elements, and pilot protection, including DCB, POTT, and line current differential.
In this webinar, we focus on the SEL-2411P Pump Automation Controller, the hardened, SCADA-ready solution from SEL that is designed specifically to address lift station challenges. During the webinar, you will learn how the SEL-2411P can assist you in increasing operational reliability, establish robust SCADA connectivity, simplify installation, improve field visibility, and reduce operational costs.
This recorded technical presentation covers the basics of acSELerator QuickSet SEL-5030 Software, an introduction to SELogic control equations, how to program an SEL relay, and how to retrieve and analyze event records.
This recorded technical presentation provides information on SEL Fast Message, DNP3, Modbus, and peer-to-peer protocols. This presentation provides a basic introduction to communications for participants not familiar with various protocols specifically for the electric power industry.
This recorded technical presentation provides information on common serial, fiber optics, Ethernet, and communications architectures. This presentation provides a basic introduction to communications for participants not familiar with various physical and logical communications standards commonly used in the electric power industry.
This recorded technical presentation provides information on how to use custom calculations in SEL-5601-2 synchroWAVe Event Software to help analyze relay event reports.
Join us for a recorded technical presentation where you will learn about a basic SEL Real-Time Automation Controller (RTAC) setup for a substation, including the initial setup out of the box; acSELerator RTAC SEL-5033 Software project setup; and downloading and testing.
This recorded technical presentation provides information on establishing an electronic security perimeter, implementing secure remote access, and applying tamper detection for devices in remote cabinets. The SEL-3620 Ethernet Security Gateway is a deny-by-default firewall, router, and password management device. The SEL-3620 is a smaller version for use in recloser cabinets with sensors to detect physical tampering.
This recorded webinar focuses on the SEL-RPM Redundant Power Module, which uses source diversity to improve control power reliability. During the webinar, you will learn about the importance of improving the reliability of your control power system, investigate six different typical power source configurations and how to add redundancy to these applications, and how the ride-through capability of the SEL-RPM allows for breaker tripping and event recording.
This recorded technical presentation provides information on engineering a better network, increasing performance over traditional Ethernet networks, and strengthening the cybersecurity of substation and industrial critical networks. Software-defined networking (SDN) allows engineers to define which devices communicate and how they communicate. With predefined failover paths, SDN increases performance over traditional Ethernet networks.
Breakout sessions from the Virtual SEL Technical Seminar.
This recorded webinar focuses on recent ultra-high-speed protection and traveling-wave fault location field experience using the SEL-T400L Time-Domain Line Protection. It also provides an overview of the relay’s new continuous line-monitoring feature for detecting incipient events and the SEL-T401L Ultra-High-Speed Line Relay, which is scheduled to release later this year.
This recorded webinar provides information on two new SEL solutions to automate data collection for NERC CIP-007-6 R1 reporting. The first solution is an audit utility for the SEL Real-Time Automation Controller (RTAC) and the second is the SEL Flow Auditor application for an SEL software-defined networking (SDN) LAN.
Now there’s an easier way to upgrade to more accurate current-based capacitor bank control. This webinar focuses on the new SEL-734W and SEL-8340 Capacitor Bank Control and Wireless Current Sensor solution, a simpler, safer, and lower-cost solution for advanced capacitor bank applications.
This webinar provides insights into and a demonstration of SEL Grid Configurator, a new tool that will replace acSELerator QuickSet SEL-5030 Software.
This webinar provides insights on how to develop secure supply chain management plans for compliance with NERC CIP-013. SEL cybersecurity experts share our strategies, processes, and best practices to support your efforts.
This webinar shares best practices on designing and implementing a converged information technology (IT)/operational technology (OT) utility communications network. Central Lincoln PUD and SEL share a case study on how Central Lincoln PUD successfully implemented a converged IT/OT network migration strategy that addresses their future needs, improves operational efficiency, and delivers better latency performance for protection.
This webinar offers information on two strategies for reducing wildfire risk—enhanced system protection and system hardening.
This webinar demonstrates how you can create and customize your own reports using energy and power quality metering data from SEL meters. During the webinar, you will learn how to retrieve and store SEL-735 Power Quality and Revenue Meter data with acSELerator Team SEL-5045 Software, how to exchange data between Team and Microsoft Power BI using the acSELerator Database API, and how to create an energy invoice using Microsoft Power BI.
This webinar provides insights on how to baseline your operation, build cyber defense, and streamline ongoing management. SEL and Dragos share a utility case study about a joint solution that addressed key cybersecurity challenges.
This webinar focuses on SEL solutions that mitigate hazardous arc-flash energy levels by as much as 90 percent and protect your personnel, equipment, and processes. During the webinar, you will learn about SEL’s proven arc-flash mitigation approaches, including results from several industrial and utility installations.
This webinar focuses on improving distribution reliability through a combination of automated protection and control schemes. During the webinar, you’ll learn about load transfer schemes, loop sectionalizing schemes, and centralized automatic restoration solutions.
This webinar focuses on the new SEL-651R Advanced Recloser Control point of common coupling (PCC) capability for distributed energy resources. During the webinar, you’ll learn about how a PCC works, IEEE 1547-2018, SEL fast islanding detection, and the advantages of the SEL-651R solution.
In this webinar discover some of the more surprising, lesser-known, and strange-looking waveforms captured while monitoring high-voltage transmission lines.
Learn how you can use SEL’s modern digital recloser controls to solve protection challenges that have historically been treated as acceptable anomalies.
This webinar chronicles Consumers Energy’s experience implementing an innovative solution based on the SEL ICON to migrate to digital leased lines and maintain the performance of protection circuits. The solution runs over a telecom carrier network based on Ciena's Carrier Ethernet technology.
This webinar will focus on securing power systems and electrical substations. Our portfolio of services and solutions makes substation operation systems secure and reliable and helps you achieve NERC CIP compliance.
In the past, power systems were dominated by linear loads and power generation sources. Today, this simple situation no longer exists and power systems include an increasing number of nonlinear loads and sources.
This webinar focuses on SEL’s 15-plus years of experience providing microgrid solutions. We share the success story of our first microgrid project—a solution in the oil and gas industry in 2002—and how we have expanded our solutions in the utility sector with remedial action schemes and other complex systems.
For years, many utilities have managed two communications networks: one based on time-division multiplexing (TDM) and tuned for the demanding requirements of operational technology (OT) applications and a second for information technology (IT). With the advent of high-bandwidth packet-based technologies, such as Multiprotocol Label Switching (MPLS) and Carrier Ethernet, there is a push to move toward a converged network model to increase the efficiency of assets.
In this webinar, Dr. Bogdan Kasztenny will discuss the challenge of deciding to reclose or not reclose on hybrid transmission lines. A new solution that uses fast and accurate fault locating allows autoreclosing cancel logic to be applied if the fault is on the underground cable portion of the line.
This webinar examines several benefits of implementing distribution network automation using fault location, isolation, and service restoration (FLISR). Distribution automation is examined for permanent faults, open-phase conductors, loss of source, substation events, and more.
This webinar will discuss a new point-to-point digital secondary system solution that was designed with simplicity in mind—Time-Domain Link (TiDL) technology. Learn how a TiDL system works, how easy it is to deploy, and how troubleshooting is simplified.
With many utility IT departments driving their network infrastructure towards packet-based solutions, it has created the challenge of how to engineer Ethernet-based pilot channels to provide the determinism and latency required for protection. This webinar presents a technology approach for guaranteeing deterministic performance over Ethernet-based wide-area networks (WANs).
The amount of data that today's digital relays, recloser controls, and other power system devices collect is astounding. It is a daunting challenge to sift through the data to make sense of the trends, patterns, and behaviors. The key to big data is knowing how to organize it so that it becomes an advantage, rather than a hindrance.
This webinar will examine several common bus configurations, present appropriate protection schemes for each configuration, and analyze the protection scheme complexity, advantages, and disadvantages.
Organize, visualize, and optimize energy usage with data analysis tools. Apply easy-to-use system-level software reports to quickly identify trends and opportunities for improvement, enabling operators to take actions that decrease energy costs.
We will discuss applications of negative-sequence differential protection for lines and transformers, negative-sequence directional elements for turn-to-turn faults in reactors and stators, and protection principles for generator turn-to-turn faults.
The topics discussed will include the following: 1. Load-Shedding Systems 2. Generation-Shedding and Runback Systems 3. Remedial Action Systems
In this webinar, the presenter will review time-domain line protection elements and illustrate their operation performance using real-world faults and digital simulations.
The webinar will: - Explain the principles of traffic engineering and how primary and failover paths can be predetermined to guarantee less than 100 µs failover times. - Show how the deny-by-default architecture of SDN enables far more secure networks.
In this webinar, you will learn about the benefits of having fast and reliable arc-flash protection, as well as the pros and cons of different arc-flash detection methodologies.
In this webinar, the presenter will review a number of time-domain protection techniques, including directional elements, direct-tripping underreaching elements, and differential elements, that significantly speed up line protection.
In this webinar, we will address: • Bridging the gap between second, millisecond, and microsecond accuracies • Maintaining time accuracy by implementing best practices • Adding precise-time redundancy and mitigating GPS vulnerabilities.
The following list contains the topics that will be covered during the webinar: • NERC CIP-007-5 • NERC PRC-005-2 • RTAC Configuration
This webinar provides an overview of TWs and TW fault location capabilities in the SEL-411L and presents real-world field experiences using the SEL-411L.
In this webinar, you will learn about the benefits of having fast and reliable arc-flash protection, as well as the pros and cons of different arc-flash detection methodologies.