Ingrese el término de búsqueda, el número MOT del producto (búsqueda inversa o búsqueda de pieza) o el número de dibujo.
This application guide explains how to use Microsoft Power BI and the acSELerator Database API to create interactive energy bills by using a set of prebuilt templates. This guide also explains the path of data from a variety of devices to the report and demonstrates how to build reports.
The SEL-451 Protection, Automation, and Bay Control System has extensive logic and protection features, allowing it to be used for many applications. This application guide describes how to implement a motor bus transfer scheme in the SEL-451 for a two-source configuration.
This application guide provides an example for setting the custom Modbus user map in the SEL-734 Advanced Metering System and SEL-735 Power Quality and Revenue Meter. It also includes a unique application example using a real-time automation controller (RTAC) with the FileIO Library to programmatically read a text file containing the custom user map and write the user map to the meter via Modbus.
This application guide shows how to provide arc-flash protection to a motor control center (MCC) by transferring the output of the time-overlight® element in an SEL-849 Motor Management Relay to an SEL-751A Feeder Protection Relay using IEC 61850 GOOSE.
This application guide provides an example of how to configure SEL-735 intermediate or advanced meters for the use of multiple load profile recorders with the Itron MV-90® xi meter reading software. In some cases, it is advantageous to expand beyond just one billing recorder and collect data from another selected LDP recorder within an SEL-735 Power Quality and Revenue Meter.
This application guide provides typical recommendations for installing arc-flash protection using an SEL-751 or SEL-751A to improve safety and enhance protection.
This application guide demonstrates a step-by-step procedure to download motor start reports from SEL motor protection relays and view them on a personal computer.
This application guide describes how to approximate trigonometric functions and square roots using SELogic control equations in SEL-700 series relays.
Application Guide - The SEL-735 Power Quality and Revenue Meter can accumulate pulses from gas, water, steam, or any other pulse output flow meters and store data to internal load profile (LDP) recorders. The acSELerator Team® SEL-5045 Software can then poll and download these data for storage and reporting. This application guide describes how to use SELogic® control equations to program the accumulation functions in the SEL-735 and how to configure an LDP recorder to display and store accumulated data.
This application guide describes how to apply logic available in the SEL-735 Power Quality and Revenue Meter to detect and take action for harmonic currents exceeding those specified in IEEE 1547.
Ordenar por