Schweitzer Engineering Laboratories

Newsroom

Jul 30, 2025

SEL enhances the performance and digital input capacity of the SEL-2240 Axion

PULLMAN, Washington—Schweitzer Engineering Laboratories (SEL), a global leader in power system protection, automation and control solutions, announces two new modules for the SEL-2240 Axion.

The first addition is the SEL-2241-2 Real-Time Automation Controller (RTAC) Module, which delivers over five times the processing power of the prior-generation RTAC module. This matches the performance of the popular SEL-3350 computing platform, but in a smaller, modular form factor. As an all-in-one intelligent electronic device, the higher processing power makes common functions like bay control, power system monitoring and digital fault recording more responsive as single- or multiple-use applications.

The second addition is the SEL-2244-4 Digital Input Module, which brings 33 percent more digital input capacity than the previous-generation digital input module. This increased capacity allows customers to streamline their system monitoring infrastructure and easily replace multiple high-I/O legacy remote terminal units or bay controllers with minimal wiring changes. To learn more about enhancements to the Axion, visit selinc.com/mktg/do-more-with-the-sel-2240-axion-rtac.

Back to Newsroom 
Featured Stories

Press Release

Two SEL Leaders Honored by the Manufacturing Institute

Technical

SEL and Puget Sound Energy Collaborate With Customers for Community Microgrid

Press Release

SEL Begins Work on New Electronic Device Manufacturing Facility in Moscow, Idaho

  • SEL Executive Vice President Elected Chair of the Board of Directors of ESCA
  • SEL Releases New Transformer Controller With LTC Control

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow