Schweitzer Engineering Laboratories

Newsroom

Sep 14, 2023

One Energy Enterprises’ Digital Substation in Findlay, Ohio, Energized and Operational

T&D World
The substation incorporates Schweitzer’s TiDL system, Hitachi Energy’s 30 MVA transformer and high-voltage circuit breakers.One Energy Enterprises’ fully digital, plug-and-play, transmission-voltage substation in Findlay, Ohio, has completed energization with testing and is operational commercially.The substation planned to power a Megawatt Hub was built as proof of concept for the company’s new, fully digital station architecture.“Traditional substations are not secure; they can fail during inevitable severe weather conditions, lack basic condition monitoring, and rely on thousands of small wires to send status and control signals back to the control building,” said One Energy CEO, Jereme Kent. “This is why we’ve designed our fully digital substations at One Energy to be secure, digital, resilient, embrace real-time condition monitoring, and survive every conceivable weather event.”One Energy selected Schweitzer Engineering Laboratories’ TiDL system, which helps connect a substation by fiber optics, thus ensuring physical security instead of opting for the IEC 61850-style digital architecture used in Europe. The TiDL merging unit can be factory installed, tested and commissioned in all major equipment, making field wiring manageable.To read the full article, click here.
Back to Newsroom 
Featured Stories

Technical

SEL Releases New Transformer Controller With LTC Control

Press Release

SEL President Appointed to the Federal Reserve Bank of San Francisco Economic Advisory Council

Press Release

SEL Announces New Vice President of Sales and Customer Service

  • Pullman School District Sale of Aquatic Center to SEL Finalized
  • SEL Names New Vice President of Sales and Customer Service

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow