Schweitzer Engineering Laboratories

Newsroom

Jun 25, 2021

Webinar: Finding Simplicity in the Complex World of Feeder Protection

Adding more features to a basic feeder protection relay can make it more complex—but it doesn’t have to. Join us July 14, 2021, for a webinar about the new SEL-851 Feeder Protection Relay, which offers comprehensive protection and advanced communications in a simple, compact package. During the webinar, you will learn how the relay protects low- and medium-voltage feeders, improves system visibility, increases safety and easily integrates into systems. You will also see an in-depth demonstration of the new SEL Grid Configurator software, which helps you quickly create, manage and deploy device settings. Visit the webinar webpage to learn more and register.
Back to Newsroom 
Featured Stories

Corporate

SEL Invests More Than $500 Million to Expand U.S. Manufacturing Capacity

Technical

SEL Releases Two New Solutions for High-Density Serial-to-Ethernet Communications

Corporate

SEL Expands Manufacturing Operations in West Lafayette

  • Manufacturer invests $150M in Post Falls
  • SEL Achieves IEC 62443-2-4 Certification, Strengthening Cybersecurity Assurance for Critical-Infrastructure Customers

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow