Schweitzer Engineering Laboratories

Newsroom

Apr 11, 2018

SEL Meter Exceeds Newest and Most Stringent ANSI 0.1 Accuracy Class

By complying with strict new metering standards, the SEL-735 Power Quality and Revenue Meter is helping utility operators ensure every kilowatt-hour is accounted for.

ANSI, the organization that sets the North American revenue metering standards, recently updated their standards to include a new accuracy class that requires higher metering accuracy and better performance, even under challenging nonsinusoidal system conditions. The SEL-735 exceeds these new, tougher requirements. 

Several megawatt-hours of energy pass through a metering installation each day. Installing accurate meters and instrument transformers ensures proper accounting of energy transactions and losses, leading to a fair return on investments for operators.

To ensure that meters provide reliable and highly accurate metering under all power system conditions, ANSI revised their C12.20-2015 standard to include six additional tests. The revisions include a new 0.1 Accuracy Class with more stringent accuracy requirements than the previous 0.2 Accuracy Class. ANSI also expanded the accuracy class test conditions to include meter performance under real-world conditions, such as operation in the presence of nonlinear loads that cause harmonics in the system. 

The SEL-735 complies with the new ANSI 0.1 Accuracy Class requirements, including the performance requirements under nonsinusoidal conditions. The SEL-735 meter’s compliance shows that it accurately reports bidirectional energy, even in the presence of harmonics and distorted waveforms.

Learn more about the SEL-735 on the product page.

Back to Newsroom 
Featured Stories

SEL In The News

Rep. Dan Newhouse and Dr. Ed Schweitzer: It’s Vital to WA That Congress Reassert Control Over Trade

Press Release

SEL Announces 2025-2026 Scholarship Recipients

Corporate

SEL Receives Purdue Senior Design Partner of the Year Award

  • SEL Technical Experts Recognized for Contributions to Industry
  • SEL Raises Starting Hourly Wage to $20

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow