Schweitzer Engineering Laboratories

Newsroom

Aug 2, 2016

SEL Completes Successful On-Site Testing of First Substation Software-Defined Network

PULLMAN, Washington — Schweitzer Engineering Laboratories successfully completed on-site testing of its new software-defined networking (SDN) technology at the Ameren Illinois Technology Applications Center (TAC) in Champaign, Illinois, using their smart grid testbed.SDN is emerging as a superior solution for the needs of both operational technology (OT) and information technology (IT) networks. Through the OpenFlow specification, SEL is using SDN to enhance the performance, configuration and management of proactive OT and dynamic IT networks. By providing centralized traffic engineering, the SEL-2740S Software-Defined Network Switch and SEL-5056 SDN Flow Controller give IT and OT network engineers path- and packet-level control of their communications flows.With sub-100 µs healing times, deny-by-default security, a –40o to +85oC operating range, and OT-optimized designs, the SEL-2740S and SEL-5056 provide unique capabilities that will change the way Ethernet is used for mission-critical applications. Engineers from Ameren, Pacific Northwest National Laboratory (PNNL), University of Illinois and SEL met in late February at the Ameren facility to perform validation tests on the SEL-2740S and SEL-5056. The validation testing focused on three main areas: cybersecurity, performance testing and operational integration. The performance testing results exceeded expectations. With less than 100 µs healing times, link failures went unnoticed by applications. The event report collection saw zero packets dropped even when there was a link break during the report collection.  “We successfully executed all test steps in our test plan, and it went so smoothly we were able to finish early,” explains Rhett Smith, SEL senior product manager. “The performance increase over traditional Ethernet is amazing to measure, and the cybersecurity attributes of the whitelisted flows of communication made the Ameren network engineers excited about what is now possible.”SDN will enable non-service-affecting network maintenance, centralized visualization and change control that current Ethernet technology is unable to provide. During testing, other attributes were discovered that are not possible with traditional networking. This included the ability to use port mirroring for a single flow instead of the entire port payload and being able to send data packets to an intrusion detection system (IDS) for deep-packet inspection if they don’t match whitelist rules.  SDN is inherently more secure than traditional Ethernet because of its deny-by-default architecture that uses whitelist flow management. During the testing, the engineers focused significantly on the cybersecurity aspects of the SEL-2740S and SEL-5056. Threat modeling exercises showed that key management and secure communications were intact and well designed.The SEL-2740S is the industry’s first SDN-based switch that improves Ethernet performance in mission-critical applications. The SEL-2740S and SEL-5056 are scheduled to release later this year. For more information on the advantages of SDN for substation applications or to order an evaluation system, visit https://selinc.com/p238.SEL serves the power industry worldwide through the design, manufacture, supply and support of products and services for power system protection, monitoring, control, automation, communications and metering. For more than 30 years, SEL has provided industry-leading performance in products and services, local technical support, a 10-year worldwide warranty and a commitment to making electric power safer, more reliable and more economical.
Back to Newsroom 
Featured Stories

Press Release

Two SEL Leaders Honored by the Manufacturing Institute

Technical

SEL and Puget Sound Energy Collaborate With Customers for Community Microgrid

Press Release

SEL Begins Work on New Electronic Device Manufacturing Facility in Moscow, Idaho

  • SEL Executive Vice President Elected Chair of the Board of Directors of ESCA
  • SEL Releases New Transformer Controller With LTC Control

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow