Schweitzer Engineering Laboratories

Newsroom

May 28, 2015

Compact Industrial Computer With 10-Year Warranty Delivers High Performance and Durability

Made in the USA, the new SEL-3360S from Schweitzer Engineering Laboratories (SEL) features Intel Core i7 processors, –40° to +75°C operation, no vents and no moving parts.

PULLMAN, Wash. — Schweitzer Engineering Laboratories, Inc. (SEL) today announced the SEL-3360S Compact Industrial Computer. Designed for extreme environments and small spaces, the SEL-3360S features powerful Intel Core i7 dual- and quad-core processors. To ensure the highest reliability, SEL’s newest industrial computer supports two solid-state 2.5" SATA drives and RAID configurations and uses single-level cell NAND flash. Up to 16 GB of error-correcting code RAM provides ample memory for demanding applications.

The SEL-3360S operates reliably in environments ranging from –40° to +75°C (–40° to +167°F) with no fans or forced airflow. Built and tested to utility substation standards, the SEL-3360S will withstand up to 15 kV of electrostatic discharge, high electromagnetic interference and shock up to 15 g.

“We are excited to introduce the SEL-3360S Computer with an industry-leading 10-year warranty,” said Dave Whitehead, SEL vice president of research and development. “SEL provides this noquestions-asked warranty based on the high level of reliability that we build into all of our products we manufacture.”

Out-of-band remote management features, such as Intel Active Management Technology (AMT), provide high serviceability to the SEL-3360S. Users can perform diagnostics, install software or operating systems and even command a reboot remotely via a cryptographically secure interface. SEL’s Backup and Recovery Tool (BaRT), unique system monitor (SysMon) and independent embedded controller (watchdog) maximize system availability by alerting users of potential issues and minimizing operational outages should a system failure occur.

SEL designs, manufactures and tests every computer at its headquarters in Pullman, Washington. SEL backs its products with a 10-year, worldwide warranty. The SEL-3360S is cUL certified, has the CE mark (also referred to as the EC mark) and is SEL’s first RoHS-compliant computer product.

The SEL-3360S is available now for only $2,850. For more information on features, benefits and applications, visit http://www.selinc.com/p230.

SEL serves the power industry worldwide through the design, manufacture, supply and support of products and services for power system protection, monitoring, control, automation, communications and metering. For more than 30 years, SEL has provided industry-leading performance in products and services, local technical support, a 10-year worldwide warranty and a commitment to making electric power safer, more reliable and more economical. 

Back to Newsroom 
Featured Stories

SEL In The News

Rep. Dan Newhouse and Dr. Ed Schweitzer: It’s Vital to WA That Congress Reassert Control Over Trade

Press Release

SEL Announces 2025-2026 Scholarship Recipients

Corporate

SEL Receives Purdue Senior Design Partner of the Year Award

  • SEL Technical Experts Recognized for Contributions to Industry
  • SEL Raises Starting Hourly Wage to $20

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow