Schweitzer Engineering Laboratories

Newsroom

Jun 15, 2015

SEL Introduces Reliable and Secure Microgrid Control System

New high-speed SEL microgrid control solutions allow seamless integration of distributed energy resources (DERs) to maintain uninterrupted power to critical loads.PULLMAN, Wash. — Schweitzer Engineering Laboratories, Inc. (SEL) today announced the release of its new line of microgrid control system solutions. The microgrid control system builds on the proven design and capabilities of SEL’s powerMAX® Power Management and Control System and makes use of SEL’s decades of experience in power system protection and control.At the heart of SEL’s solution is a powerful microgrid controller that is able to respond to external data, such as real-time pricing signals and fast-changing system dynamics. This capability enables the microgrid controller to optimize the system configuration based on the system user’s priorities and real-time data. Priorities can be assigned to various user-defined scenarios, like economic dispatch, carbon footprint minimization, renewable integration and system resiliency. The fast, deterministic controller can operate in as little as half a cycle, allowing it to reliably balance load with available generation.“Microgrids have low inertia, which means they need relay-speed SEL microgrid controllers,” said Bob Morris, SEL vice president of national operations. “SEL microgrid solutions combine dependable computing and communications to provide high-performance microgrid control, including adaptive relaying, synchrophasors, and cybersecurity.”SEL’s microgrid control system solutions use SEL’s robust layered cybersecurity hierarchy. This hardened security approach ensures that all data remains secure, allowing the system to operate continuously without threat of interruptions.Each microgrid system is unique and depends on variables such as the type of distributed energy resources, system owner operation priorities, project drivers and utility interconnection requirements. The SEL microgrid controller is both flexible and customizable to ensure interoperability with all system components and drivers. SEL is also capable of providing front-end engineering and design for microgrid preproject planning purposes.For more information on features, benefits, and applications of SEL microgrid control system solutions, visit  www.selinc.com/p231. SEL serves the power industry worldwide through the design, manufacture, supply and support of products and services for power system protection, monitoring, control, automation, communications and metering. For more than 30 years, SEL has provided industry-leading performance in products and services, local technical support, a 10-year worldwide warranty and a commitment to making electric power safer, more reliable and more economical.
Back to Newsroom 
Featured Stories

Press Release

SEL Names New Vice President of Sales and Customer Service

Press Release

SEL Names New Vice President of Engineering Services

Corporate

SEL Founder Urges Civic Engagement and Civility at Pullman Chamber Luncheon

  • SEL supports ambitious grid modernization project in Central America
  • Employee Owners Do More Than Show Up — We Build Things Better

Contact Us

Corporate News

Kate Wilhite

+1.509.592.5109info@selinc.com
Follow